v01.01.14.x

New Features

  • Added support for profiling OpenCL kernels using hardware events and the AET Library. Refer Profiling.

Defect Fixes

  • [MCT-718] Fixed issues with platform - do not create the platform singleton just to delete it. This scenario occurred where OpenCL APIs are not invoked, but the OpenCL runtime in linked into the application.

Supported Evaluation Modules (EVMs)

Compiler Versions

This release requires the following compiler versions:

Compiler Version
ARM GCC 6.2.1 (arm-linux-gnueabi)
ARM GCC 4.9.3 (arm-none-eabi, for OpenCL over TI-RTOS)
C6000 8.1.3