Profiling¶
You can profile an OpenCL application as any other application with generic profiling tools such as “gprof”. Here we explain how to profile commands in the OpenCL command queue.
Additionally, you can profile hardware events such as L2 cache misses and pipeline stalls through the AET library. See the Profiling Hardware Events section for more information.
Host Side Profiling¶
To profile commands on the host side, you will need to specify “CL_QUEUE_PROFILING_ENABLE” property when creating the command queue. OpenCL runtime will then record the host-side timestamp in nano-seconds when the command is enqueued, is submitted, starts execution and finishes execution. User code can query these timestamps using “clGetEventProfilingInfo” API on the corresponding event that is returned at command enqueue time.
DSP Side Profiling¶
OpenCL runtime also records timestamps for predefined OpenCL activities on the DSP side and uses lightweight ULM (Usage and Load Monitor) to communicate those data back to host. These predefined activities include start and finish of a workgroup execution, and dsp cache coherency operations. On the host side, users will need to use dsptop utility to retrieve the information. You probably will need two windows/consoles and run your OpenCL application after dsptop is run, for example,
- In window 1, run
dsptop -l last - In window 2, launch your OpenCL application, wait for it to finish
- Back in window 1, type “q” to quit dsptop. dsptop should print out the information sent back from the DSP side.
Details about usage of dsptop can be found by running dsptop -h and by
this dsptop wikipage .
Profiling Hardware Events¶
Profiling hardware events is a useful capability provided through the CTools
AET library. Starting from TI OpenCL product v1.1.14, this capability is
integrated into the OpenCL runtime. See all the stall and memory events
in the AET Profiling Events section below. Events not prefixed
with AET_EVT_STALL_ or AET_EVT_MEM_ cannot be profiled.
To profile hardware events, there are three choices:
- Profile All Possible Events
- Profile a Select Few Events
- Manually Profile 1 or 2 Events
Profile All Events¶
To profile all hardware events, run the profiling script as follows:
/usr/share/ti/opencl/profiling/oclaet.sh [-g] oclapp
# e.g oclapp is ./vecadd
While the the executable is running, raw profiling data is recorded into
profiling/aetdata.txt relative to the current directory.
After the profiling script finishes, it runs a python
script that forms a json table, a html table, and optionally a plot of each
kernel’s profiling information if -g option is specified. Note that
genering plots may require installing additional python packages.
Profile Select Events¶
To profile selected hardware events, run the profiling script as follows:
/usr/share/ti/opencl/profiling/oclaet.sh oclapp event_type event_number [event_number ...]
# event_type: 1 for stall events, 2 for meeory events
# event_number is the event offset from AET_GEM_STALL_EVT_START, if
# profiling stall cycles, or from AET_GEM_MEM_EVT_START, if profiling
# memory events. At each script run, you can only profile one or more
# events of the same type.
Manually Profile 1 or 2 Events¶
To manually profile 1 stall event, or 1 to 2 memory events, simply set the environment variables described in Environment Variables, as follows.
TI_OCL_EVENT_TYPE=1 TI_OCL_EVENT_NUMBER1=13 TI_OCL_STALL_CYCLE_THRESHOLD=0 ./vecadd
TI_OCL_EVENT_TYPE=2 TI_OCL_EVENT_NUMBER1=11 TI_OCL_EVENT_NUMBER1=12 ./vecadd
Note that profiling data is appended to profiling/aetdata.txt at each profiling run. If a fresh profiling is needed, remove profiling/aetdata.txt before profiling run.
Analyzing Profiling Data¶
If you manually profile, you will have to run the python script to obtain the JSON file or html table.
python /usr/share/ti/opencl/profiling/oclaet.py -t -g profiling/aetdata.txt
The -t flag and -g flags tell the script to produce an html table and matplot plot of profiling data, respectively. If neither of these flags are specified, then only the json file of raw counter data will be formed. This json is easier to read than the raw data dump in profiling/aetdata.txt. The current format for raw data is:
EVENT_TYPE # the event type
EVENT_NUMBER1 # the first event number (offset from base AET event)
EVENT_NUMBER2 # the second event number (offset from base AET event)
STALL_CYCLE_THRESHOLD # the stall cycle threshold
Core number # number of core
Counter0_Value # hardware counter 0 value: memory event 1
Counter1_Value # hardware counter 1 value: memory event 2 or stall event
~~~~End Core # End of core data for Core number
... # MORE CORE DATA CAN FOLLOW THIS
EVENT_TYPE
EVENT_NUMBER1
EVENT_NUMBER2
STALL_CYCLE_THRESHOLD
Core number
Counter0_Value
Counter1_Value
~~~~End Core
VectorAdd # Kernel Name
---End Kernel # Ends Kernel Data
Profiling Data Plotting Requirements¶
Plotting profiling data with python script requires matplotlib, pandas, and seaborn python packages to be installed. If they are not already installed on your system, you can follow the instructions below.
which pip
# install pip if it is not already on your system
wget https://bootstrap.pypa.io/get-pip.py
python get-pip.py
pip install matplotlib
pip install pandas
pip install seaborn
AET Profiling Events¶
- AET_EVT_MEM_L1D_RH_SRAM_A (AET_GEM_MEM_EVT_START + 0)
- L1D Read Hit SRAM A
- AET_EVT_MEM_L1D_RH_SRAM_B (AET_GEM_MEM_EVT_START + 1)
- L1D Read Hit SRAM B
- AET_EVT_MEM_L1D_RH_CACHE_A (AET_GEM_MEM_EVT_START + 2)
- L1D Read Hit Cache A
- AET_EVT_MEM_L1D_RH_CACHE_B (AET_GEM_MEM_EVT_START + 3)
- L1D Read Hit Cache B
- AET_EVT_MEM_L1D_WH_BUF_NOT_FULL_A (AET_GEM_MEM_EVT_START + 4)
- L1D Write Hit, Tag Buffer Not Full A
- AET_EVT_MEM_L1D_WH_BUF_NOT_FULL_B (AET_GEM_MEM_EVT_START + 5)
- L1D Write Hit, Tag Buffer Not Full B
- AET_EVT_MEM_L1D_WH_BUF_FULL_A (AET_GEM_MEM_EVT_START + 6)
- L1D Write Hit, Tag Buffer Full A
- AET_EVT_MEM_L1D_WH_BUF_FULL_B (AET_GEM_MEM_EVT_START + 7)
- L1D Write Hit, Tag Buffer Full B
- AET_EVT_MEM_L1D_RM_HITS_L2_SRAM_A (AET_GEM_MEM_EVT_START + 8)
- L1D Read Miss, Hits L2 SRAM A
- AET_EVT_MEM_L1D_RM_HITS_L2_SRAM_B (AET_GEM_MEM_EVT_START + 9)
- L1D Read Miss, Hits L2 SRAM B
- AET_EVT_MEM_L1D_RM_HITS_L2_CACHE_A (AET_GEM_MEM_EVT_START + 10)
- L1D Read Miss, Hits L2 Cache A
- AET_EVT_MEM_L1D_RM_HITS_L2_CACHE_B (AET_GEM_MEM_EVT_START + 11)
- L1D Read Miss, Hits L2 Cache B
- AET_EVT_MEM_L1D_RM_HITS_EXT_CABLE_A (AET_GEM_MEM_EVT_START + 12)
- L1D Read Miss, Hits External, Cacheable A
- AET_EVT_MEM_L1D_RM_HITS_EXT_CABLE_B (AET_GEM_MEM_EVT_START + 13)
- L1D Read Miss, Hits External, Cacheable B
- AET_EVT_MEM_L1D_RM_HITS_EXT_NON_CABLE_A (AET_GEM_MEM_EVT_START + 14)
- L1D Read Miss, Hits External, Non Cacheable A
- AET_EVT_MEM_L1D_RM_HITS_EXT_NON_CABLE_B (AET_GEM_MEM_EVT_START + 15)
- L1D Read Miss, Hits External, Non Cacheable B
- AET_EVT_MEM_L1D_WM_WRT_BUF_NOT_FULL_A (AET_GEM_MEM_EVT_START + 16)
- L1D Write Miss, Write Buffer Not Full A
- AET_EVT_MEM_L1D_WM_WRT_BUF_NOT_FULL_B (AET_GEM_MEM_EVT_START + 17)
- L1D Write Miss, Write Buffer Not Full B
- AET_EVT_MEM_L1D_WM_WRT_BUF_FULL_A (AET_GEM_MEM_EVT_START + 18)
- L1D Write Miss, Write Buffer Full A
- AET_EVT_MEM_L1D_WM_WRT_BUF_FULL_B (AET_GEM_MEM_EVT_START + 19)
- L1D Write Miss, Write Buffer Full B
- AET_EVT_MEM_L1D_WM_TAG_VIC_WRT_BUF_FLUSH_A (AET_GEM_MEM_EVT_START + 20)
- L1D Write Miss, Tag/Victim/Write Buffer Flush A
- AET_EVT_MEM_L1D_WM_TAG_VIC_WRT_BUF_FLUSH_B (AET_GEM_MEM_EVT_START + 21)
- L1D Write Miss, Tag/Victim/Write Buffer Flush B
- AET_EVT_MEM_CPU_CPU_BANK_CONFLICT (AET_GEM_MEM_EVT_START + 22)
- CPU - CPU Bank Conflict
- AET_EVT_MEM_CPU_SNOOP_CONFLICT (AET_GEM_MEM_EVT_START + 23)
- CPU - Snoop/Coherence Conflict (A or B)
- AET_EVT_MEM_CPU_IDMA_EDMA_BANK_CONFLICT (AET_GEM_MEM_EVT_START + 24)
- CPU - iDMA/EDMA Bank Conflict (A or B)
- AET_EVT_MEM_L1P_RH_SRAM (AET_GEM_MEM_EVT_START + 25)
- L1P Read Hit SRAM
- AET_EVT_MEM_L1P_RH_CACHE (AET_GEM_MEM_EVT_START + 26)
- L1P Read Hit Cache
- AET_EVT_MEM_L1P_RM_HITS_L2_SRAM (AET_GEM_MEM_EVT_START + 27)
- L1P Read Miss, Hits L2 SRAM
- AET_EVT_MEM_L1P_RM_HITS_L2_CACHE (AET_GEM_MEM_EVT_START + 28)
- L1P Read Miss, Hits L2 Cache
- AET_EVT_MEM_L1P_RM_HITS_EXT_CABLE (AET_GEM_MEM_EVT_START + 29)
- L1P Read Miss, Hits External Cacheable
- AET_EVT_STALL_CPU_PIPELINE (AET_GEM_STALL_EVT_START + 0)
- CPU Stall Cycles
- AET_EVT_STALL_CROSS_PATH (AET_GEM_STALL_EVT_START + 1)
- Stall Due to a Cross path
- AET_EVT_STALL_BRANCH_TO_SPAN_EXEC_PKT (AET_GEM_STALL_EVT_START + 2)
- Stall due to a branch to an execute packet that spans two fetch packets
- AET_EVT_STALL_EXT_FUNC_IFACE (AET_GEM_STALL_EVT_START + 3)
- Stall due to an External Functional Interface
- AET_EVT_STALL_MVC (AET_GEM_STALL_EVT_START + 4)
- Stall Conditions: 1) AMR write followed by addressing mode instruction and src2 register is affected by AMR Values 2) Read of emulation registers in the ECM
- AET_EVT_STALL_L1P_OTHER (AET_GEM_STALL_EVT_START + 5)
- Any other stall not prwviously listed
- AET_EVT_STALL_L1P_WAIT_STATE (AET_GEM_STALL_EVT_START + 6)
- Stall due to Wait states in L1P Memory
- AET_EVT_STALL_L1P_MISS (AET_GEM_STALL_EVT_START + 8)
- Execute Packed held off due to a Cache Miss
- AET_EVT_STALL_L1D_OTHER (AET_GEM_STALL_EVT_START + 10)
- Any other L1D Stall not previosuly listed
- AET_EVT_STALL_L1D_BANK_CONFLICT (AET_GEM_STALL_EVT_START + 11)
- Stall on a memory bank conflict between A and B
- AET_EVT_STALL_L1D_DMA_CONFLICT (AET_GEM_STALL_EVT_START + 12)
- Stall while CPU access is held off by a DMA Access
- AET_EVT_STALL_L1D_WRITE_BUFFER_FULL (AET_GEM_STALL_EVT_START + 13)
- Stall on a write miss on A or B while the Write Buffer is Full
- AET_EVT_STALL_L1D_TAG_UD_BUF_FULL (AET_GEM_STALL_EVT_START + 14)
- Stall on a Write Hit with a tag update on either A or B while the tag update buffer is full
- AET_EVT_STALL_L1D_LINE_FILL_B (AET_GEM_STALL_EVT_START + 15)
- Stall on a read miss on B while the read miss data is being fetched from the lower memory level
- AET_EVT_STALL_L1D_LINE_FILL_A (AET_GEM_STALL_EVT_START + 16)
- Stall on a read miss on A while the read miss data is being fetched from the lower memory level
- AET_EVT_STALL_L1D_WRT_BUF_FLUSH (AET_GEM_STALL_EVT_START + 17)
- Stall on a read Miss on Either A or B while the Write Buffer is being flushed
- AET_EVT_STALL_L1D_VICTIM_BUF_FLUSH (AET_GEM_STALL_EVT_START + 18)
- Stall on a read miss on either A or B while the Victim Buffer is being flushed
- AET_EVT_STALL_L1D_TAG_UD_BUF_FLUSH (AET_GEM_STALL_EVT_START + 20)
- Stall on a read miss on either A or B while the Tag Update Buffer is being flushed
- AET_EVT_STALL_L1D_SNOOP_CONFLICT (AET_GEM_STALL_EVT_START + 21)
- Stall while a CPU access is held off by a Snoop access
- AET_EVT_STALL_L1D_COH_OP_CONFLICT (AET_GEM_STALL_EVT_START + 22)
- Stall while a CPU access is held off by a block cache coherence operation access