v01.01.11.x¶
Platforms supported¶
- AM572 EVM (Linux and RTOS)
- AM571x
- 66AK2H EVM
- 66AK2L EVM
- 66AK2E EVM
- 66AK2G EVM
Release Notes¶
- Support use of exit/abort in C code called from OpenCL C kernels
Defect Fixes¶
- [MCT-499] Destruction of the Platform singleton causes a crash in a subsequent clReleaseProgram() during teardown of ViennaCL OCL examples
- [MCT-648] C++ I/O broken for OpenCL RTOS examples with 4Q BIOS
- [MCT-649] OOT being reported as IOT on K2E
Compiler Versions¶
This release requires the following compiler versions:
Compiler | Version |
---|---|
ARM GCC | 5.3.1 (arm-linux-gnueabi) |
ARM GCC | 4.9.3 (arm-none-eabi, for OpenCL over TI-RTOS) |
C6000 | 8.1.0 |