v01.01.10.x¶
Platforms supported¶
- AM572 EVM (Linux and RTOS)
- AM571x
- 66AK2H EVM
- 66AK2L EVM
- 66AK2E EVM
- 66AK2G EVM
Release Notes¶
- Added support for AM571x
- AM57x: Add DSP performance monitoring support for OpenCL applications
Defect Fixes¶
- [MCT-566] - C66 intrinsics not available in OpenCL C
- [MCT-571] - dsptop does not work on AM57 with DSP suspend/resume enabled
- [MCT-536] - clocl creates .dsp_h file even if link to build .out file fails
- [MCT-516] - OpenCL-RTOS: Exit ARM and DSP programs on completion
- [MCT-572] - Defect in OpenCL CMEM error message regarding number of CMEM blocks required
- [MCT-575] - OpenCL-RTOS: clocl shipped with RTOS does not find the correct version of libstdc++.so.6
- [MCT-593] - MessageQ error results in debugss error messages on subsequent run
- [MCT-594] - OpenCL matmpy intermittent DSP1 crash due to EdmaMgr issues w/ suspend/resume
- [MCT-597] - Race condition in OpenCL cleanup code.
Compiler Versions¶
This release requires the following compiler versions:
| Compiler | Version |
|---|---|
| ARM GCC | 5.3.1 (arm-linux-gnueabi) |
| ARM GCC | 4.9.3 (arm-none-eabi, for OpenCL over TI-RTOS) |
| C6000 | 8.1.0 |