![]() |
![]() |
TI-RTOS Drivers
tidrivers_tivac_2_16_00_08
|
UART driver implementation for a Tiva UART controller thay uses DMA.
============================================================================
The UART header file should be included in an application as follows:
Refer to UART.h for a complete description of APIs & example of use.
#include <stdint.h>
#include <stdbool.h>
#include <ti/drivers/UART.h>
#include <ti/sysbios/knl/Semaphore.h>
#include <ti/sysbios/family/arm/m3/Hwi.h>
Go to the source code of this file.
Data Structures | |
struct | UARTTivaDMA_HWAttrs |
UARTTivaDMA Hardware attributes. More... | |
struct | UARTTivaDMA_Object |
UARTTivaDMA Object. More... | |
Macros | |
#define | ti_sysbios_family_arm_m3_Hwi__nolocalnames |
Typedefs | |
typedef struct UARTTivaDMA_HWAttrs | UARTTivaDMA_HWAttrs |
UARTTivaDMA Hardware attributes. More... | |
typedef struct UARTTivaDMA_Object | UARTTivaDMA_Object |
UARTTivaDMA Object. More... | |
typedef struct UARTTivaDMA_Object * | UARTTivaDMA_Handle |
Variables | |
const UART_FxnTable | UARTTivaDMA_fxnTable |
#define ti_sysbios_family_arm_m3_Hwi__nolocalnames |
typedef struct UARTTivaDMA_HWAttrs UARTTivaDMA_HWAttrs |
UARTTivaDMA Hardware attributes.
The fields, with the exception of intPriority, are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For TivaWare these definitions are found in:
intPriority is the UART peripheral's interrupt priority, as defined by the underlying OS. It is passed unmodified to the underlying OS's interrupt handler creation code, so you need to refer to the OS documentation for usage. For example, for SYS/BIOS applications, refer to the ti.sysbios.family.arm.m3.Hwi documentation for SYS/BIOS usage of interrupt priorities. If the driver uses the ti.drivers.ports interface instead of making OS calls directly, then the HwiP port handles the interrupt priority in an OS specific way. In the case of the SYS/BIOS port, intPriority is passed unmodified to Hwi_create().
A sample structure is shown below:
typedef struct UARTTivaDMA_Object UARTTivaDMA_Object |
UARTTivaDMA Object.
The application must not access any member variables of this structure!
typedef struct UARTTivaDMA_Object * UARTTivaDMA_Handle |
const UART_FxnTable UARTTivaDMA_fxnTable |