49 #ifndef ti_drivers_uart_UARTTivaDMA__include
50 #define ti_drivers_uart_UARTTivaDMA__include
60 #include <ti/sysbios/knl/Semaphore.h>
61 #define ti_sysbios_family_arm_m3_Hwi__nolocalnames
62 #include <ti/sysbios/family/arm/m3/Hwi.h>
177 ti_sysbios_family_arm_m3_Hwi_Struct
hwi;
183 #undef ti_sysbios_family_arm_m3_Hwi__nolocalnames
uint32_t txChannelIndex
Definition: UARTTivaDMA.h:144
size_t writeCount
Definition: UARTTivaDMA.h:168
Semaphore_Struct writeSem
Definition: UARTTivaDMA.h:178
struct UARTTivaDMA_Object UARTTivaDMA_Object
UARTTivaDMA Object.
UARTTivaDMA Object.
Definition: UARTTivaDMA.h:152
struct UARTTivaDMA_HWAttrs UARTTivaDMA_HWAttrs
UARTTivaDMA Hardware attributes.
UART_Callback readCallback
Definition: UARTTivaDMA.h:159
Semaphore_Struct readSem
Definition: UARTTivaDMA.h:179
The definition of a UART function table that contains the required set of functions to control a spec...
Definition: UART.h:514
unsigned int baseAddr
Definition: UARTTivaDMA.h:136
bool opened
Definition: UARTTivaDMA.h:154
unsigned int intPriority
Definition: UARTTivaDMA.h:140
UART_Mode
UART mode settings.
Definition: UART.h:308
unsigned int readTimeout
Definition: UARTTivaDMA.h:157
UART_DataMode
UART data mode settings.
Definition: UART.h:356
UART_ReturnMode
UART return mode settings.
Definition: UART.h:341
UART_Mode writeMode
Definition: UARTTivaDMA.h:156
size_t writeSize
Definition: UARTTivaDMA.h:169
UART_Echo
UART echo settings.
Definition: UART.h:374
void * readBuf
Definition: UARTTivaDMA.h:172
UART_DataMode writeDataMode
Definition: UARTTivaDMA.h:163
UARTTivaDMA Hardware attributes.
Definition: UARTTivaDMA.h:134
ti_sysbios_family_arm_m3_Hwi_Struct hwi
Definition: UARTTivaDMA.h:177
unsigned int intNum
Definition: UARTTivaDMA.h:138
UART_Echo readEcho
Definition: UARTTivaDMA.h:164
struct UARTTivaDMA_Object * UARTTivaDMA_Handle
UART_Callback writeCallback
Definition: UARTTivaDMA.h:160
const void * writeBuf
Definition: UARTTivaDMA.h:167
UART_ReturnMode readReturnMode
Definition: UARTTivaDMA.h:161
UART_DataMode readDataMode
Definition: UARTTivaDMA.h:162
void(* UART_Callback)(UART_Handle, void *buf, size_t count)
The definition of a callback function used by the UART driver when used in UART_MODE_CALLBACK The cal...
Definition: UART.h:301
unsigned int writeTimeout
Definition: UARTTivaDMA.h:158
size_t readCount
Definition: UARTTivaDMA.h:173
uint32_t rxChannelIndex
Definition: UARTTivaDMA.h:142
size_t readSize
Definition: UARTTivaDMA.h:174
const UART_FxnTable UARTTivaDMA_fxnTable
UART_Mode readMode
Definition: UARTTivaDMA.h:155