Linker options control linking operations. They can be placed on the command line or in a command file. Linker options must be preceded by a hyphen (-). Options can be separated from arguments (if they have them) by an optional space.
| Option | Alias | Description | Section |
|---|---|---|---|
| --run_linker | -z | Enables linking | Section 8.3 |
| --output_file | -o | Names the executable output module. The default filename is a.out. | Section 8.4.24 |
| --map_file | -m | Produces a map or listing of the input and output sections, including holes, and places the listing in filename | Section 8.4.19 |
| --stack_size | -stack | Sets C system stack size to sizewords and defines a global symbol that specifies the stack size. Default = 1K words | Section 8.4.30 |
| --heap_size | -heap | Sets heap size (for the dynamic memory allocation in C) to sizewords and defines a global symbol that specifies the heap size. Default = 1K words | Section 8.4.15 |
| Option | Alias | Description | Section |
|---|---|---|---|
| --library | -l | Names an archive library or link command filename as linker input | Section 8.4.17 |
| --disable_auto_rts | Disables the automatic selection of a run-time-support library | Section 8.4.8 | |
| --priority | -priority | Satisfies unresolved references by the first library that contains a definition for that symbol | Section 8.4.17.3 |
| --reread_libs | -x | Forces rereading of libraries, which resolves back references | Section 8.4.17.3 |
| --search_path | -i | Alters library-search algorithms to look in a directory named with pathname before looking in the default location. This option must appear before the --library option. | Section 8.4.17.1 |
| Option | Alias | Description | Section |
|---|---|---|---|
| --define | Predefines name as a preprocessor macro. | Section 8.4.11 | |
| --undefine | Removes the preprocessor macro name. | Section 8.4.11 | |
| --disable_pp | Disables preprocessing for command files | Section 8.4.11 |
| Option | Alias | Description | Section |
|---|---|---|---|
| --diag_error | Categorizes the diagnostic identified by num as an error | Section 8.4.7 | |
| --diag_remark | Categorizes the diagnostic identified by num as a remark | Section 8.4.7 | |
| --diag_suppress | Suppresses the diagnostic identified by num | Section 8.4.7 | |
| --diag_warning | Categorizes the diagnostic identified by num as a warning | Section 8.4.7 | |
| --display_error_number | Displays a diagnostic's identifiers along with its text | Section 8.4.7 | |
| --emit_references:file[=file] | Emits a file containing section information. The information includes section size, symbols defined, and references to symbols. | Section 8.4.7 | |
| --emit_warnings_as_errors | -pdew | Treats warnings as errors | Section 8.4.7 |
| --issue_remarks | Issues remarks (nonserious warnings) | Section 8.4.7 | |
| --no_demangle | Disables demangling of symbol names in diagnostics | Section 8.4.21 | |
| --no_warnings | Suppresses warning diagnostics (errors are still issued) | Section 8.4.7 | |
| --set_error_limit | Sets the error limit to num. The linker abandons linking after this number of errors. (The default is 100.) | Section 8.4.7 | |
| --verbose_diagnostics | Provides verbose diagnostics that display the original source with line-wrap | Section 8.4.7 | |
| --warn_sections | -w | Displays a message when an undefined output section is created | Section 8.4.34 |
| Option | Alias | Description | Section |
|---|---|---|---|
| --absolute_exe | -a | Produces an absolute, executable module. This is the default; if neither --absolute_exe nor --relocatable is specified, the linker acts as if --absolute_exe were specified. | Section 8.4.3.1 |
| --ecc={ on | off } | Enable linker-generated Error Correcting Codes (ECC). The default is off. | Section 8.4.12
Section 8.5.10 |
|
| --ecc:data_error | Inject the specified errors into the output file for testing | Section 8.4.12
Section 8.5.10 |
|
| --ecc:ecc_error | Inject the specified errors into the Error Correcting Code (ECC) for testing | Section 8.4.12
Section 8.5.10 |
|
| --mapfile_contents | Controls the information that appears in the map file. | Section 8.4.20 | |
| --relocatable | -r | Produces a nonexecutable, relocatable output module | Section 8.4.3.2 |
| --rom | -r | Create a ROM object | |
| --run_abs | -abs | Produces an absolute listing file | Section 8.4.28 |
| --xml_link_info | Generates a well-formed XML file containing detailed information about the result of a link | Section 8.4.35 |
| Option | Alias | Description | Section |
|---|---|---|---|
| --entry_point | -e | Defines a global symbol that specifies the primary entry point for the output module | Section 8.4.13 |
| --globalize | Changes the symbol linkage to global for symbols that match pattern | Section 8.4.18 | |
| --hide | Hides global symbols that match pattern | Section 8.4.16 | |
| --localize | Changes the symbol linkage to local for symbols that match pattern | Section 8.4.18 | |
| --make_global | -g | Makes symbol global (overrides -h) | Section 8.4.18.1 |
| --make_static | -h | Makes all global symbols static | Section 8.4.18.1 |
| --no_sym_merge | -b | Disables merge of symbolic debugging information in COFF object files | Section 8.4.22 |
| --no_symtable | -s | Strips symbol table information and line number entries from the output module | Section 8.4.23 |
| --retain | Retains a list of sections that otherwise would be discarded. (EABI only) | Section 8.4.27 | |
| --scan_libraries | -scanlibs | Scans all libraries for duplicate symbol definitions | Section 8.4.29 |
| --symbol_map | Maps symbol references to a symbol definition of a different name | Section 8.4.32 | |
| --undef_sym | -u | Places an unresolved external symbol into the output module's symbol table | Section 8.4.33 |
| --unhide | Reveals (un-hides) global symbols that match pattern | Section 8.4.16 |
| Option | Alias | Description | Section |
|---|---|---|---|
| --arg_size | --args | Allocates memory to be used by the loader to pass arguments | Section 8.4.4 |
| --fill_value | -f | Sets default fill values for holes within output sections; fill_value is a 32-bit constant | Section 8.4.14 |
| --ram_model | -cr | Initializes variables at load time | Section 8.4.26 |
| --rom_model | -c | Autoinitializes variables at run time | Section 8.4.26 |
| Option | Alias | Description | Section |
|---|---|---|---|
| --cinit_compression [=compression_kind] | Specifies the type of compression to apply to the C auto initialization data. The default compression_kind if this option is used with no kind specified is lzss for Lempel-Ziv-Storer-Szymanski compression. Alternately, specify --cinit_compression=rle to use Run Length Encoded compression, which generally provides less efficient compression. (EABI only) | Section 8.4.5 | |
| --compress_dwarf | Aggressively reduces the size of DWARF information from input object files. (EABI only) | Section 8.4.6 | |
| --copy_compression [=compression_kind] | Compresses data copied by linker copy tables (EABI only) | Section 8.4.5 | |
| --unused_section_elimination | Eliminates sections that are not needed in the executable module; on by default. (EABI only) | Section 8.4.10 | |
| --keep_asm | Retain any post-link files (.pl) and .absolute listing files (.abs) generated by the −plink option. This allows you to view any changes the post-link optimizer makes. (Requires use of -plink) | Note (1) | |
| --no_postlink_across_calls | -nf | Disable post-link optimizations across functions. (Requires use of -plink) | Note (1) |
| --plink_advice_only | Annotates assembly code with comments if changes cannot be made safely due to pipeline considerations, such as when float support or VCU support is enabled. (Requires use of -plink) | Note (1) | |
| --postlink_exclude | -ex | Exclude files from post-link pass. (Requires use of -plink) | Note (1) |
| --postlink_opt | -plink | Post-link optimizations. (Only after --run_linker or -z) | Note (1) |
| Option | Alias | Description | Section |
|---|---|---|---|
| --disable_clink | -j | Disables conditional linking of COFF object modules. (COFF only) | Section 8.4.9 |
| --linker_help | -help | Displays information about syntax and available options | – |
| --preferred_order | Prioritizes placement of functions | Section 8.4.25 | |
| --strict_compatibility | Performs more conservative and rigorous compatibility checking of input object files | Section 8.4.31 | |
| --zero_init | Controls preinitialization of uninitialized variables. Default is on.Always off if --ram_model is used. (EABI only) | Section 8.4.36 |