Retain Discarded Sections (--retain Option)

NOTE

The --retain option is used only with EABI mode. It is ignored when linking in COFF mode.

When --unused_section_elimination is on, the ELF linker does not include a section in the final link if it is not needed in the executable to resolve references. The --retain option tells the linker to retain a list of sections that would otherwise not be retained. This option accepts the wildcards '*' and '?'. When wildcards are used, the argument should be in quotes. The syntax for this option is:

--retain=sym_or_scn_spec

The --retain option take one of the following forms: