Alternate Host malloc/free Extension for Zero Copy OpenCL Kernels¶
The TI OpenCL implementation adds 4 new host functions
-
void *
__malloc_ddr(size_t size)¶
-
void
__free_ddr(void *p)¶
-
void *
__malloc_msmc(size_t size)¶
-
void
__free_msmc(void *p)¶
These new APIs in the TI OpenCL implementation are not specified as part of OpenCL specification, but are TI extensions that are roughly modeled after OpenCL 2.0 specified functions clSVMAlloc and clSVMFree. They are not the same as those functions and therefore will not inherit those names in order to avoid confusion.
The __malloc_ddr/__free_ddr APIs allocate and free memory in the global address space in off-chip DDR memory. The __malloc_msmc/__free_msmc APIs allocate and free memory in the global address space in on-chip MSMC memory.
The rationale for these memory allocation extensions is to allow OpenCL APIs to be hidden in lower-level implementation routines so that top level algorithmic code can remain free from OpenCL mechanics. This abstraction of OpenCL APIs is possible without these extensions, but would typically require data copy from Linux managed memory to OpenCL managed memory. These extensions were provided to allow the top level algorithmic code to originate data allocation in OpenCL managed memory, thus eliminated the need for data copy and improving performance.
Without these new APIs the host application and lower level function might look like:
main()
{
float *p = (float*) malloc(size);
// populate p
fftw(p, size);
// consume modified p
free(p);
}
void fftw(float *v1, size_t size)
{
Buffer buffer v1Buf (context, CL_MEM_USE_HOST_PTR | CL_MEM_READ_WRITE, size, v1);
fftw_kernel.setArg(0, v1Buf);
fftw_kernel.setArg(1, size);
Event ev;
Q.enqueueTask(fftw_kernel, 0, &ev);
ev.wait();
...
}
The issue with the above code is that the enqueue of the fftw_kernel would entail a copy of the Linux heap based underlying memory store in the OpenCL buffer to a copy allocated from CMEM. It would also entail a copy back after the enqueue of the kernel. Since the SoC contains shared memory between the ARM and the DSP, it would be preferable to have a zero copy setup. This would be impossible with a Linux heap based malloc pointer.
With the new functions, the above code might look like
main()
{
float *p = __malloc_ddr(size);
// populate p
fftw(p, size);
// consume modified p
__free_ddr(p);
}
void fftw(float *v1, size_t size)
{
Buffer buffer v1Buf (context, CL_MEM_USE_HOST_PTR | CL_MEM_READ_WRITE, size, v1);
fftw_kernel.setArg(0, v1Buf);
fftw_kernel.setArg(1, size);
Event ev;
Q.enqueueTask(fftw_kernel, 0, &ev);
ev.wait();
...
}
In this version, the user simply replaced malloc/free with __malloc_ddr/__free_ddr and otherwise the user’s code remains the same.
The low level fftw function is not modified, but since the incoming pointer v1 now points to OpenCL managed CMEM memory, the OpenCL implementation no longer needs to copy the data. It may still perform cache coherency operations surrounding the kernel enqueue.
A nice benefit to the above code setup is that the low level function fftw works with malloc memory or __malloc_ddr memory. This is good for cases when the low level functions may be part of a 3rd party library. The use of __malloc_ddr is not required for correctness and therefore the user of fftw can then choose whether they want to modify their source to get the additional performance boost resulting from zero copy.
OpenCL subbuffers created from OpenCL buffers defined with CL_MEM_USE_HOST_PTR and a supplied pointer originating from __malloc_ddr, will also benefit from the underlying subbuffer memory residing in CMEM.
Caution
OpenCL buffers can also be created with CL_MEM_USE_HOST_PTR and a supplied pointer in the middle of a __malloc_ddr/__malloc_msmc allocated region. However, when doing so, extra caution should be taken not to create overlapping buffers, as it is undefined behavior when they are accessed by the same kernel and at least one of them is write access. If such undefined scenario is absolutely intended, user needs to pass “-a” option to the kernel compiler, telling the compiler that kernel arguments could alias each other. “-a” should be specified in the clBuildProgram API call for online compilation and on the clocl command line for offline compilation. Even so, it is still user’s responsibility to ensure correct parallel execution semantics, for example, when there are multiple workgroups.
Important
Since the ARM CPU is a 32 bit architecture, Linux will only support 4GB of virtual memory at any given time, therefore the amount of memory available to __malloc_ddr or __malloc_msmc will be limited in size to a limit below 4GB. This is in contrast to defining an OpenCL buffer in the host application that is only limited by the maximum block available in any CMEM heap. These can exceed 4GB in length. This can occur because the allocation of the buffer does not imply a map into the virtual memory space. That would occur independently with the mapBuffer commands (which would be limited in size). A malloc on the other hand implies a readiness to use the returned pointer and thus any memory returned by clMalloc would be auto mapped into the virtual address space.
Important
Obviously, creating a buffer using a __malloc_ddr/__malloc_msmc pointer will require size specified at buffer creation time to be less than or equal to the size of the allocated memory using __malloc_ddr/__malloc_msmc.
Error
Calling __free_ddr() or __free_msmc() on memory that is underlying an OpenCL Buffer while the buffer is still in use is undefined behavior.
Memory Alignment¶
Similar to global buffers and local buffers, memory allocated by
__malloc_ddr and __malloc_msmc are always aligned at 128-byte boundary.