TI-RTOS Drivers
tidrivers_tivac_2_16_00_08
|
Macros | |
#define | SPI_STATUS_SUCCESS 0 |
Successful status code returned by SPI_control(). More... | |
#define | SPI_STATUS_ERROR -1 |
Generic error status code returned by SPI_control(). More... | |
#define | SPI_STATUS_UNDEFINEDCMD -2 |
An error status code returned by SPI_control() for undefined command codes. More... | |
SPI_STATUS_* macros are general status codes returned by SPI_control()
SPITivaDMA_STATUS_* macros are command codes only defined in the SPITivaDMA.h driver implementation and need to:
#define SPI_STATUS_SUCCESS 0 |
Successful status code returned by SPI_control().
SPI_control() returns SPI_STATUS_SUCCESS if the control code was executed successfully.
#define SPI_STATUS_ERROR -1 |
Generic error status code returned by SPI_control().
SPI_control() returns SPI_STATUS_ERROR if the control code was not executed successfully.
#define SPI_STATUS_UNDEFINEDCMD -2 |
An error status code returned by SPI_control() for undefined command codes.
SPI_control() returns SPI_STATUS_UNDEFINEDCMD if the control code is not recognized by the driver implementation.