102 #ifndef ti_driver_pwm_PWMTiva__include
103 #define ti_driver_pwm_PWMTiva__include
138 #define PWMTiva_CMD_CHANGE_GEN_PERIOD PWM_CMD_RESERVED + 0
142 #define PWMTiva_CHANGE_GEN_PERIOD PWMTiva_CMD_CHANGE_GEN_PERIOD
146 #define PWMTiva_NUM_PWM_PERIPHERALS 2
149 #define PWMTiva_NUM_PWM_GENERATORS 4
const PWM_FxnTable PWMTiva_fxnTable
PWMTiva_Status * pwmStatus
Definition: PWMTiva.h:196
struct PWMTiva_Status PWMTiva_Status
PWMTiva_Status.
struct PWMTiva_HWAttrs PWMTiva_HWAttrs
PWMTiva Hardware attributes.
uint32_t pwmGenOpts
Definition: PWMTiva.h:175
uint8_t dutyMode
Definition: PWMTiva.h:199
uint8_t prescalar
Definition: PWMTiva.h:186
The definition of a PWM function table that contains the required set of functions to control a speci...
Definition: PWM.h:349
uint16_t genPeriods[PWMTiva_NUM_PWM_GENERATORS]
Definition: PWMTiva.h:184
uint32_t baseAddr
Definition: PWMTiva.h:173
uint32_t pwmOutput
Definition: PWMTiva.h:174
struct PWMTiva_Object PWMTiva_Object
PWMTiva Object.
#define PWMTiva_NUM_PWM_GENERATORS
Definition: PWMTiva.h:149
PWMTiva Object.
Definition: PWMTiva.h:195
uint16_t pwmDuty
Definition: PWMTiva.h:197
uint8_t pwmOutputBit
Definition: PWMTiva.h:198
PWMTiva Hardware attributes.
Definition: PWMTiva.h:172
uint8_t activeOutputs
Definition: PWMTiva.h:187
PWMTiva_Status.
Definition: PWMTiva.h:183
uint8_t cyclesPerMicroSec
Definition: PWMTiva.h:185