85 #ifndef ti_driver_pwm_PWMTimerTiva__include
86 #define ti_driver_pwm_PWMTimerTiva__include
121 #define PWMTimerTiva_CMD_CHANGE_PERIOD PWM_CMD_RESERVED + 0
125 #define PWMTimerTiva_CHANGE_PERIOD PWMTimerTiva_CMD_CHANGE_PERIOD
PWMTimerTiva Object.
Definition: PWMTimerTiva.h:163
uint32_t period
Definition: PWMTimerTiva.h:164
struct PWMTimerTiva_HWAttrs PWMTimerTiva_HWAttrs
PWMTimerCC3200 Hardware attributes.
PWMTimerCC3200 Hardware attributes.
Definition: PWMTimerTiva.h:153
The definition of a PWM function table that contains the required set of functions to control a speci...
Definition: PWM.h:349
uint8_t cyclesPerMicroSec
Definition: PWMTimerTiva.h:167
uint32_t duty
Definition: PWMTimerTiva.h:165
uint16_t timer
Definition: PWMTimerTiva.h:155
struct PWMTimerTiva_Object PWMTimerTiva_Object
PWMTimerTiva Object.
const PWM_FxnTable PWMTimerTiva_fxnTable
uint8_t dutyMode
Definition: PWMTimerTiva.h:166
uint32_t baseAddr
Definition: PWMTimerTiva.h:154