TI-RTOS for SimpleLink Wireless MCUs  2.14.02.22
Data Fields
UDMACC26XX_HWAttrs Struct Reference

UDMACC26XX hardware attributes. More...

#include <UDMACC26XX.h>

Data Fields

uint32_t baseAddr
 
Power_Resource powerMngrId
 
uint8_t intNum
 
uint8_t intPriority
 UDMACC26XX error interrupt priority. More...
 

Detailed Description

UDMACC26XX hardware attributes.

Field Documentation

uint32_t UDMACC26XX_HWAttrs::baseAddr
Power_Resource UDMACC26XX_HWAttrs::powerMngrId

UDMACC26XX Peripheral's power manager ID

uint8_t UDMACC26XX_HWAttrs::intNum

UDMACC26XX error interrupt number

uint8_t UDMACC26XX_HWAttrs::intPriority

UDMACC26XX error interrupt priority.

The CC26xx uses three of the priority bits, meaning ~0 has the same effect as (7 << 5). (7 << 5) will apply the lowest priority. (0 << 5) will apply the highest priority.


The documentation for this struct was generated from the following file:
Copyright 2015, Texas Instruments Incorporated