IPC API  3.30.00.09
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Data Structures | Macros | Typedefs | Enumerations | Functions
IpcPower.h File Reference

Detailed Description

============================================================================


Go to the source code of this file.

Data Structures

struct  IpcPower_WugenEvtMask
 Type representing OMAP's WUGEN_MEVT[0|1] registers. More...
 

Macros

#define IpcPower_S_SUCCESS   (0)
 Operation is successful. More...
 
#define IpcPower_E_FAIL   (-1)
 Operation is not successful. More...
 
#define IpcPower_E_MEMORY   (-2)
 Operation resulted in memory failure. More...
 

Typedefs

typedef enum IpcPower_Event IpcPower_Event
 Event types for power management callbacks. More...
 
typedef Void(* IpcPower_CallbackFuncPtr )(Int event, Ptr data)
 Power Event Callback function type definition. More...
 
typedef struct
IpcPower_WugenEvtMask 
IpcPower_WugenEvtMask
 Type representing OMAP's WUGEN_MEVT[0|1] registers. More...
 

Enumerations

enum  IpcPower_Event {
  IpcPower_Event_SUSPEND = 0,
  IpcPower_Event_RESUME = 1
}
 Event types for power management callbacks. More...
 

Functions

Void IpcPower_init ()
 Initialize the IpcPower module. More...
 
Void IpcPower_exit ()
 Finalize the IpcPower module. More...
 
Void IpcPower_suspend ()
 Initiate the suspend procedure. More...
 
Void IpcPower_wakeLock ()
 Disable the deep sleep mode in the core. More...
 
Void IpcPower_wakeUnlock ()
 Enable the core to go to deep sleep mode. More...
 
UInt IpcPower_hibernateLock ()
 Disable the core to go to suspend / hibernate. More...
 
UInt IpcPower_hibernateUnlock ()
 Enable the core to go to suspend / hibernate. More...
 
Bool IpcPower_canHibernate ()
 Return TRUE if hibernation is allowed. More...
 
Int IpcPower_registerCallback (Int event, IpcPower_CallbackFuncPtr fxn, Ptr data)
 Register callback function for a Power event. More...
 
Int IpcPower_unregisterCallback (Int event, IpcPower_CallbackFuncPtr fxn)
 Unregister callback function for a Power event. More...
 
Void IpcPower_getWugenEvtMask (IpcPower_WugenEvtMask *mask)
 Retrieve current WUGEN mask used for suspend. More...
 
Void IpcPower_setWugenEvtMask (IpcPower_WugenEvtMask *mask)
 Set WUGEN mask used for suspend. More...
 

Macro Definition Documentation

#define IpcPower_S_SUCCESS   (0)

Operation is successful.

#define IpcPower_E_FAIL   (-1)

Operation is not successful.

#define IpcPower_E_MEMORY   (-2)

Operation resulted in memory failure.

Typedef Documentation

Event types for power management callbacks.

typedef Void(* IpcPower_CallbackFuncPtr)(Int event, Ptr data)

Power Event Callback function type definition.

Type representing OMAP's WUGEN_MEVT[0|1] registers.

For APIs IpcPower_getWugenEvtMask() and IpcPower_setWugenEvtMask()

Enumeration Type Documentation

Event types for power management callbacks.

Enumerator
IpcPower_Event_SUSPEND 
IpcPower_Event_RESUME 

Callback event for Power suspend

Function Documentation

Void IpcPower_init ( )

Initialize the IpcPower module.

See Also
IpcPower_exit
Void IpcPower_exit ( )

Finalize the IpcPower module.

See Also
IpcPower_init
Void IpcPower_suspend ( )

Initiate the suspend procedure.

Void IpcPower_wakeLock ( )

Disable the deep sleep mode in the core.

See Also
IpcPower_wakeUnlock
Void IpcPower_wakeUnlock ( )

Enable the core to go to deep sleep mode.

See Also
IpcPower_wakeLock
UInt IpcPower_hibernateLock ( )

Disable the core to go to suspend / hibernate.

See Also
IpcPower_hibernateUnlock, IpcPower_canHibernate
UInt IpcPower_hibernateUnlock ( )

Enable the core to go to suspend / hibernate.

See Also
IpcPower_hibernateLock, IpcPower_canHibernate
Bool IpcPower_canHibernate ( )

Return TRUE if hibernation is allowed.

See Also
IpcPower_hibernateLock, IpcPower_hibernateUnlock
Int IpcPower_registerCallback ( Int  event,
IpcPower_CallbackFuncPtr  fxn,
Ptr  data 
)

Register callback function for a Power event.

Parameters
[in]eventPower Management callback event type.
[in]fxnFunction being registered.
[in]dataData to be passed as argument to function.

Returns SUCCESS or FAIL

See Also
IpcPower_registerCallback
Int IpcPower_unregisterCallback ( Int  event,
IpcPower_CallbackFuncPtr  fxn 
)

Unregister callback function for a Power event.

Parameters
[in]eventPower Management callback event type.
[in]fxnFunction being unregistered.

Returns SUCCESS or FAIL

See Also
IpcPower_unregisterCallback
Void IpcPower_getWugenEvtMask ( IpcPower_WugenEvtMask mask)

Retrieve current WUGEN mask used for suspend.

Parameters
[in]maskPointer to structure for holding WUGEN event mask
See Also
IpcPower_suspend, IpcPower_setWugenEvtMask
Void IpcPower_setWugenEvtMask ( IpcPower_WugenEvtMask mask)

Set WUGEN mask used for suspend.

The values in the passed structure are copied into the internal WUGEN event mask. To achieve an ORing of certain bits in the mask, first retrieve the current mask with IpcPower_getWugenEvtMask() and then OR in the bits you want to enable.

Parameters
[in]maskPointer to WUGEN event mask structure
See Also
IpcPower_suspend, IpcPower_getWugenEvtMask
Copyright 2014, Texas Instruments Incorporated