![]() |
![]() |
|
TI-RTOS Drivers
tidrivers_cc32xx_2_16_01_13
|
|
Macros | |
| #define | PWM_STATUS_SUCCESS 0 |
| Successful status code returned by PWM_control(). More... | |
| #define | PWM_STATUS_ERROR -1 |
| Generic error status code returned by PWM_control(). More... | |
| #define | PWM_STATUS_UNDEFINEDCMD -2 |
| An error status code returned by PWM_control() for undefined command codes. More... | |
PWM_STATUS_* macros are general status codes returned by PWM_control()
PWMTimerCC3200_STATUS_* macros are command codes only defined in the PWMTimerCC3200.h driver implementation and need to:
| #define PWM_STATUS_SUCCESS 0 |
Successful status code returned by PWM_control().
PWM_control() returns PWM_STATUS_SUCCESS if the control code was executed successfully.
| #define PWM_STATUS_ERROR -1 |
Generic error status code returned by PWM_control().
PWM_control() returns PWM_STATUS_ERROR if the control code was not executed successfully.
| #define PWM_STATUS_UNDEFINEDCMD -2 |
An error status code returned by PWM_control() for undefined command codes.
PWM_control() returns PWM_STATUS_UNDEFINEDCMD if the control code is not recognized by the driver implementation.