![]() |
![]() |
|
TI-RTOS Drivers
tidrivers_c2000_2_16_01_13
|
| CCamera_Config | Camera Global configuration |
| CCamera_FxnTable | The definition of a Camera function table that contains the required set of functions to control a specific Camera driver implementation |
| CCamera_Params | Camera Parameters |
| CClockP_FreqHz | Frequency-in-hertz struct |
| CClockP_Params | Basic ClockP Parameters |
| CDIR | |
| Cdiskio_fxns | |
| CEMAC_Config | EMAC Global configuration |
| CEMAC_FxnTable | EMAC Function table structure |
| CEMACTiva_HWAttrs | EMACTiva Hardware attributes |
| CEMACTiva_Object | EMACTiva Object |
| CFATFS | |
| CFIL | |
| CFILINFO | |
| CGPIOTiva_Config | GPIO device specific driver configuration structure |
| CHwiP_Params | Basic HwiP Parameters |
| CI2C_Config | I2C Global configuration |
| CI2C_FxnTable | The definition of a I2C function table that contains the required set of functions to control a specific I2C driver implementation |
| CI2C_Params | I2C Parameters |
| CI2C_Transaction | I2C transaction |
| CI2CTiva_HWAttrs | I2CTiva Hardware attributes |
| CI2CTiva_Object | I2CTiva Object |
| CI2S_BufDesc | I2S buffer descriptor for issue/reclaim mode |
| CI2S_Config | I2S Global configuration |
| CI2S_FxnTable | The definition of a I2S function table that contains the required set of functions to control a specific I2S driver implementation |
| CI2S_Params | Basic I2S Parameters |
| CList_Elem | |
| CList_List | |
| CMutexP_Params | Basic MutexP Parameters |
| CNVS_Attrs | NVS attributes |
| CNVS_Config | NVS Global configuration |
| CNVS_FxnTable | The definition of an NVS function table that contains the required set of functions to control a specific NVS driver implementation |
| CNVS_Params | NVS Parameters |
| CPIN_State_s | Underlying data structure for type PIN_State |
| CPower_NotifyObj | Power notify object structure |
| CPWM_Config | PWM Global configuration |
| CPWM_FxnTable | The definition of a PWM function table that contains the required set of functions to control a specific PWM driver implementation |
| CPWM_Params | PWM Parameters |
| CRingBuf_Object | |
| CSDSPI_Config | SDSPI Global configuration |
| CSDSPI_FxnTable | The definition of a SDSPI function table that contains the required set of functions to control a specific SDSPI driver implementation |
| CSDSPI_Params | SDSPI Parameters |
| CSDSPITiva_HWAttrs | SDSPITiva Hardware attributes |
| CSDSPITiva_Object | SDSPITiva Object |
| CSemaphoreP_Params | Basic SemaphoreP Parameters |
| CSPI_Config | SPI Global configuration |
| CSPI_FxnTable | The definition of a SPI function table that contains the required set of functions to control a specific SPI driver implementation |
| CSPI_Params | SPI Parameters |
| CSPI_Transaction | A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat frames are sent and received from the buffers pointed to txBuf and rxBuf. The arg variable is an user-definable argument which gets passed to the SPI_CallbackFxn when the SPI driver is in SPI_MODE_CALLBACK |
| CSPITivaDMA_HWAttrs | SPITivaDMA Hardware attributes |
| CSPITivaDMA_Object | SPITivaDMA Object |
| CUART_Config | UART Global configuration |
| CUART_FxnTable | The definition of a UART function table that contains the required set of functions to control a specific UART driver implementation |
| CUART_Params | UART Parameters |
| CUARTTiva_FxnSet | Complement set of read functions to be used by the UART ISR and UARTTiva_read(). Internal use only |
| CUARTTiva_HWAttrs | UARTTiva Hardware attributes |
| CUARTTiva_Object | UARTTiva Object |
| CUSBMSCHFatFs_Config | USBMSCHFatFs Global configuration |
| CUSBMSCHFatFs_FxnTable | The definition of a USBMSCHFatFs function table that contains the required set of functions to control a specific USBMSCHFatFs driver implementation |
| CUSBMSCHFatFs_Params | USBMSCHFatFs Parameters |
| CUSBMSCHFatFsTiva_HWAttrs | USBMSCHFatFsTiva Hardware attributes |
| CUSBMSCHFatFsTiva_Object | USBMSCHFatFsTiva Object |
| CWatchdog_Config | Watchdog Global configuration |
| CWatchdog_FxnTable | The definition of a Watchdog function table that contains the required set of functions to control a specific Watchdog driver implementation |
| CWatchdog_Params | Watchdog Parameters |
| CWatchdogTiva_HWAttrs | Watchdog hardware attributes for Tiva |
| CWatchdogTiva_Object | Watchdog Object for Tiva |
| CWiFi_Config | WiFi Global configuration |
| CWiFi_FxnTable | The definition of a WiFi function table that contains the required set of functions to control a specific WiFi driver implementation |
| CWiFi_Params | WiFi Parameters |