![]() |
![]() |
|
TI-RTOS Drivers
tidrivers_c2000_2_16_00_08
|
|
Macros | |
| #define | WiFi_STATUS_SUCCESS 0 |
| Successful status code returned by WiFi_control(). More... | |
| #define | WiFi_STATUS_ERROR -1 |
| Generic error status code returned by WiFi_control(). More... | |
| #define | WiFi_STATUS_UNDEFINEDCMD -2 |
| An error status code returned by WiFi_control() for undefined command codes. More... | |
WiFi_STATUS_* macros are general status codes returned by WiFi_control()
| #define WiFi_STATUS_SUCCESS 0 |
Successful status code returned by WiFi_control().
WiFi_control() returns WiFi_STATUS_SUCCESS if the control code was executed successfully.
| #define WiFi_STATUS_ERROR -1 |
Generic error status code returned by WiFi_control().
WiFi_control() returns WiFi_STATUS_ERROR if the control code was not executed successfully.
| #define WiFi_STATUS_UNDEFINEDCMD -2 |
An error status code returned by WiFi_control() for undefined command codes.
WiFi_control() returns WiFi_STATUS_UNDEFINEDCMD if the control code is not recognized by the driver implementation.