Functions | |
| void | trimDevice (void) |
| Performs the necessary trim of the device which is not done in boot code. More... | |
| void trimDevice | ( | void | ) |
Performs the necessary trim of the device which is not done in boot code.
This function should only execute coming from ROM boot. The current implementation does not take soft reset into account. However, it does no damage to execute it again. It only consumes time.
Definition at line 199 of file setup.c.