Functions | |
| static bool | FlashsafeSMPHTryAcquire (void) |
| Aquire the flash semaphore. More... | |
| static void | FlashsafeSMPHRelease (void) |
| Release the flash semaphore. More... | |
| uint32_t | FlashsafeSizeGet (void) |
| Get the size of the flash. More... | |
| uint32_t | FlashsafeSectorSizeGet (void) |
| Get size of a flash sector in no of bytes. More... | |
| uint32_t | FlashsafePowerModeSet (uint32_t ui32PowerMode, uint32_t ui32BankGracePeriode, uint32_t ui32PumpGracePeriode) |
| Set power mode. More... | |
| uint32_t | FlashsafePowerModeGet (void) |
| Get current configured power mode. More... | |
| uint32_t | FlashsafeProtectionSet (uint32_t ui32SectorAddress, uint32_t ui32ProtectMode) |
| Set sector protection. More... | |
| uint32_t | FlashsafeProtectionGet (uint32_t ui32SectorAddress) |
| Get sector protection. More... | |
| uint32_t | FlashsafeProtectionSave (uint32_t ui32SectorAddress) |
| Save sector protection to make it permanent. More... | |
| uint32_t | FlashsafeCheckFsmForError (void) |
| Checks if the Flashsafe state machine has detected an error. More... | |
| uint32_t | FlashsafeCheckFsmForReady (void) |
| Checks if the Flash state machine is ready. More... | |
| uint32_t | FlashsafeIntRegister (void(*pfnHandler)(void)) |
| Registers an interrupt handler for the flash interrupt. More... | |
| uint32_t | FlashsafeIntUnregister (void) |
| Unregisters the interrupt handler for the flash interrupt. More... | |
| uint32_t | FlashsafeIntEnable (uint32_t ui32IntFlags) |
| Enables flash controller interrupt sources. More... | |
| uint32_t | FlashsafeIntDisable (uint32_t ui32IntFlags) |
| Disables individual flash controller interrupt sources. More... | |
| uint32_t | FlashsafeIntStatus (void) |
| Gets the current interrupt status. More... | |
| uint32_t | FlashsafeIntClear (uint32_t ui32IntFlags) |
| Clears flash controller interrupt source. More... | |
| uint32_t | FlashsafeSectorErase (uint32_t ui32SectorAddress) |
| Erase a flash sector. More... | |
| uint32_t | FlashsafeProgram (uint8_t *pui8DataBuffer, uint32_t ui32Address, uint32_t ui32Count) |
| Programs unprotected main bank flash sectors. More... | |
| uint32_t | FlashsafeDisableSectorsForWrite (void) |
| Disables all sectors for erase and programming on the active bank. More... | |
| uint32_t FlashsafeCheckFsmForError | ( | void | ) |
Checks if the Flashsafe state machine has detected an error.
This function returns the status of the Flashsafe State Machine indicating if an error is detected or not. Primary use is to check if an Erase or Program operation has failed.
Definition at line 243 of file flashsafe.c.
| uint32_t FlashsafeCheckFsmForReady | ( | void | ) |
Checks if the Flash state machine is ready.
This function returns the status of the Flash State Machine indicating if it is ready to accept a new command or not. Primary use is to check if an Erase or Program operation has finished.
Definition at line 261 of file flashsafe.c.
| uint32_t FlashsafeDisableSectorsForWrite | ( | void | ) |
Disables all sectors for erase and programming on the active bank.
This function disables all sectors for erase and programming on the active bank and enables the Idle Reading Power reduction mode if no low power mode is configured. Furthermore, an additional level of protection from erase is enabled.
Definition at line 457 of file flashsafe.c.

| uint32_t FlashsafeIntClear | ( | uint32_t | ui32IntFlags | ) |
Clears flash controller interrupt source.
The flash controller interrupt source is cleared, so that it no longer assert. This must be done in the interrupt handler to keep it from being called again immediately upon exit.
| ui32IntFlags | is the bit mask of the interrupt sources to be cleared. Can be any of:
|
Definition at line 385 of file flashsafe.c.

| uint32_t FlashsafeIntDisable | ( | uint32_t | ui32IntFlags | ) |
Disables individual flash controller interrupt sources.
This function disables the flash controller interrupt sources.
| ui32IntFlags | is the bit mask of the interrupt sources to be disabled. The parameter is the bitwise OR of any of the following:
|
Definition at line 354 of file flashsafe.c.

| uint32_t FlashsafeIntEnable | ( | uint32_t | ui32IntFlags | ) |
Enables flash controller interrupt sources.
This function enables the flash controller interrupt sources.
| ui32IntFlags | is the bit mask of the interrupt sources to be enabled. The parameter is the bitwise OR of any of the following:
|
Definition at line 333 of file flashsafe.c.

| uint32_t FlashsafeIntRegister | ( | void(*)(void) | pfnHandler | ) |
Registers an interrupt handler for the flash interrupt.
This function does the actual registering of the interrupt handler. This function enables the global interrupt in the interrupt controller; specific FLASH interrupts must be enabled via FlashsafeIntEnable(). It is the interrupt handler's responsibility to clear the interrupt source.
| pfnHandler | is a pointer to the function to be called when the flash interrupt occurs. |
Definition at line 279 of file flashsafe.c.

| uint32_t FlashsafeIntStatus | ( | void | ) |
Gets the current interrupt status.
This function returns the interrupt status for the Flash.
Definition at line 374 of file flashsafe.c.

| uint32_t FlashsafeIntUnregister | ( | void | ) |
Unregisters the interrupt handler for the flash interrupt.
This function does the actual unregistering of the interrupt handler. It clears the handler to be called when a FLASH interrupt occurs. This function also masks off the interrupt in the interrupt controller so that the interrupt handler no longer is called.
Definition at line 306 of file flashsafe.c.

| uint32_t FlashsafePowerModeGet | ( | void | ) |
Get current configured power mode.
This function will return the current configured power mode.
Definition at line 144 of file flashsafe.c.

| uint32_t FlashsafePowerModeSet | ( | uint32_t | ui32PowerMode, |
| uint32_t | ui32BankGracePeriode, | ||
| uint32_t | ui32PumpGracePeriode | ||
| ) |
Set power mode.
This function will set the specified power mode.
Any access to the bank causes a reload of the specified bank grace periode input value into the bank down counter. After the last access to the flash bank, the down counter delays from 0 to 255 prescaled HCLK clock cycles before putting the bank into one of the fallback power modes as determined by ui32PowerMode. This value must be greater than 1 when the fallback mode is not FLASH_PWR_ACTIVE_MODE.
Note: The prescaled clock used for the down counter is a clock divided by 16 from input HCLK. The ui32BankGracePeriode parameter is ignored if ui32PowerMode is equal to FLASH_PWR_ACTIVE_MODE. Any access to flash memory causes the pump grace periode down counter to reload with value of ui32PumpGracePeriode. After the bank has gone to sleep, the down counter delays this number of prescaled HCLK clock cycles before entering one of the charge pump fallback power modes as determined by ui32PowerMode. The prescaled clock used for the pump grace periode down counter is a clock divided by 16 from input HCLK. This parameter is ignored if ui32PowerMode is equal to FLASH_PWR_ACTIVE_MODE.
In current flash module design the SW application has to call the FlashsafePowerModeSet() funtion with the FLASH_PWR_ACTIVE_MODE input parameter value if the flash modules comes out of any of the two low power modes, in in order to reestablish the factory configured idle reading power reduction mode.
Changing the power mode of the flash module must be a part within a device power mode transition requiring configuration of multiple modules. Refer to documents describing the device power modes.
| ui32PowerMode | is the wanted power mode. The defined power modes are: |
| ui32BankGracePeriode | is the starting count value for the bank grace periode down counter. |
| ui32PumpGracePeriode | is the starting count value for the pump grace periode down counter. |
Definition at line 115 of file flashsafe.c.

| uint32_t FlashsafeProgram | ( | uint8_t * | pui8DataBuffer, |
| uint32_t | ui32Address, | ||
| uint32_t | ui32Count | ||
| ) |
Programs unprotected main bank flash sectors.
This function will program a sequence of bytes into the on-chip flash. Programming each location consists of the result of an AND operation of the new data and the existing data; in other words bits that contain 1 can remain 1 or be changed to 0, but bits that are 0 cannot be changed to 1. Therefore, a byte can be programmed multiple times as long as these rules are followed; if a program operation attempts to change a 0 bit to a 1 bit, that bit will not have its value changed.
This function will not return until the data has been programmed or an programming error has occurred.
The pui8DataBuffer pointer can not point to flash.
| pui8DataBuffer | is a pointer to the data to be programmed. |
| ui32Address | is the starting address in flash to be programmed. |
| ui32Count | is the number of bytes to be programmed. |
Definition at line 431 of file flashsafe.c.

| uint32_t FlashsafeProtectionGet | ( | uint32_t | ui32SectorAddress | ) |
Get sector protection.
This return the protection mode for the specified flash bank sector.
| ui32SectorAddress | is the start address of the desired sector. |
Definition at line 189 of file flashsafe.c.

| uint32_t FlashsafeProtectionSave | ( | uint32_t | ui32SectorAddress | ) |
Save sector protection to make it permanent.
This function will save the the current protection mode for the specified flash bank sector. A write protected sector will become permanent write protected!! A device reset will not change the write protection!
| ui32SectorAddress | is the start address of the sector to be protected. |
Definition at line 216 of file flashsafe.c.

| uint32_t FlashsafeProtectionSet | ( | uint32_t | ui32SectorAddress, |
| uint32_t | ui32ProtectMode | ||
| ) |
Set sector protection.
This function will set the specified protection on specified flash bank sector. A sector can either have no protection or have write protection which guards for both program and erase of that sector. Sector protection can only be changed from FLASH_NO_PROTECT to FLASH_WRITE_PROTECT!
| ui32SectorAddress | is the start address of the sector to protect. |
| ui32ProtectMode | is the enumerated sector protection mode. The defined sector protection modes are: |
Definition at line 164 of file flashsafe.c.

| uint32_t FlashsafeSectorErase | ( | uint32_t | ui32SectorAddress | ) |
Erase a flash sector.
This function will erase the specified flash sector. The function will not return until the flash sector has been erased or an error condition occurred. If flash top sector is erased the function will program the the device security data bytes with default values. The device security data located in the customer configuration area of the flash top sector, must have valid values at all times. These values affects the configuration of the device during boot.
| ui32SectorAddress | is the starting address in flash of the sector to be erased. |
Definition at line 403 of file flashsafe.c.

| uint32_t FlashsafeSectorSizeGet | ( | void | ) |
Get size of a flash sector in no of bytes.
This function will return the size of a flash sector in number of bytes.
Definition at line 104 of file flashsafe.c.
Referenced by FlashsafeProtectionGet(), FlashsafeProtectionSave(), FlashsafeProtectionSet(), and FlashsafeSectorErase().

| uint32_t FlashsafeSizeGet | ( | void | ) |
Get the size of the flash.
This function returns the size of the flash main bank in number of bytes.
Definition at line 93 of file flashsafe.c.
Referenced by FlashsafeProgram(), FlashsafeProtectionGet(), FlashsafeProtectionSave(), FlashsafeProtectionSet(), and FlashsafeSectorErase().

|
inlinestatic |
Release the flash semaphore.
Definition at line 189 of file flashsafe.h.
Referenced by FlashsafeDisableSectorsForWrite(), FlashsafeIntClear(), FlashsafeIntDisable(), FlashsafeIntEnable(), FlashsafeIntRegister(), FlashsafeIntUnregister(), FlashsafePowerModeGet(), FlashsafePowerModeSet(), FlashsafeProgram(), FlashsafeProtectionGet(), FlashsafeProtectionSave(), FlashsafeProtectionSet(), and FlashsafeSectorErase().

|
inlinestatic |
Aquire the flash semaphore.
Definition at line 176 of file flashsafe.h.
Referenced by FlashsafeDisableSectorsForWrite(), FlashsafeIntClear(), FlashsafeIntDisable(), FlashsafeIntEnable(), FlashsafeIntRegister(), FlashsafeIntUnregister(), FlashsafePowerModeGet(), FlashsafePowerModeSet(), FlashsafeProgram(), FlashsafeProtectionGet(), FlashsafeProtectionSave(), FlashsafeProtectionSet(), and FlashsafeSectorErase().

| #define FAPI_STATUS_FSM_BUSY 0x00000001 |
Definition at line 126 of file flashsafe.h.
| #define FAPI_STATUS_FSM_ERROR 0x00000004 |
Definition at line 130 of file flashsafe.h.
| #define FAPI_STATUS_FSM_READY 0x00000002 |
Definition at line 127 of file flashsafe.h.
| #define FAPI_STATUS_INCORRECT_DATABUFFER_LENGTH 0x00000003 |
Definition at line 128 of file flashsafe.h.
| #define FAPI_STATUS_SUCCESS 0x00000000 |
Definition at line 125 of file flashsafe.h.
| #define FLASH_INT_FSM_DONE 0x00400000 |
Definition at line 138 of file flashsafe.h.
| #define FLASH_INT_RV 0x00010000 |
Definition at line 139 of file flashsafe.h.
| #define FLASH_NO_PROTECT 0x00000000 |
Definition at line 156 of file flashsafe.h.
| #define FLASH_PWR_ACTIVE_MODE 0x00000000 |
Definition at line 146 of file flashsafe.h.
| #define FLASH_PWR_DEEP_STDBY_MODE 0x00000002 |
Definition at line 148 of file flashsafe.h.
| #define FLASH_PWR_OFF_MODE 0x00000001 |
Definition at line 147 of file flashsafe.h.
| #define FLASH_WRITE_PROTECT 0x00000001 |
Definition at line 157 of file flashsafe.h.
| #define FLASHSAFE_ACCESS_DENIED 0x000000ff |
Definition at line 116 of file flashsafe.h.
Referenced by FlashsafeDisableSectorsForWrite(), FlashsafeIntClear(), FlashsafeIntDisable(), FlashsafeIntEnable(), FlashsafeIntRegister(), FlashsafeIntUnregister(), FlashsafePowerModeGet(), FlashsafePowerModeSet(), FlashsafeProgram(), FlashsafeProtectionGet(), FlashsafeProtectionSave(), FlashsafeProtectionSet(), and FlashsafeSectorErase().
| #define FLASHSAFE_ACCESS_OK 0x000000ee |
Definition at line 117 of file flashsafe.h.
Referenced by FlashsafeDisableSectorsForWrite(), FlashsafeIntClear(), FlashsafeIntDisable(), FlashsafeIntEnable(), FlashsafeIntRegister(), FlashsafeIntUnregister(), FlashsafePowerModeSet(), and FlashsafeProtectionSet().
| #define FSM_REG_WRT_DISABLE 2 |
Definition at line 166 of file flashsafe.h.
| #define FSM_REG_WRT_ENABLE 5 |
Definition at line 165 of file flashsafe.h.
| #define SMPH_ALLOC_FLASH 1 |
Definition at line 118 of file flashsafe.h.
Referenced by FlashsafeSMPHRelease(), and FlashsafeSMPHTryAcquire().