![]() |
![]() |
|
TI-RTOS for SimpleLink Wireless MCUs
2.14.01.20
|
| CCamera_Config | Camera Global configuration |
| CCamera_FxnTable | The definition of a Camera function table that contains the required set of functions to control a specific Camera driver implementation |
| CCamera_Params | Camera Parameters |
| CCameraCC3200DMA_HWAttrs | CameraCC3200DMA Hardware attributes |
| CCameraCC3200DMA_Object | CameraCC3200DMA Object |
| CClockP_FreqHz | Frequency-in-hertz struct |
| CClockP_Params | Basic ClockP Parameters |
| CCryptoCC26XX_AESCCM_Transaction | CryptoCC26XX AES-CCM Transaction |
| CCryptoCC26XX_AESECB_Transaction | CryptoCC26XX AES-ECB Transaction |
| CCryptoCC26XX_Config | CryptoCC26XX Global Configuration |
| CCryptoCC26XX_HWAttrs | CryptoCC26XX Hardware Attributes |
| CCryptoCC26XX_Object | CryptoCC26XX Object |
| CCryptoCC26XX_Params | CryptoCC26XX Parameters |
| CCryptoCC26XX_Transaction | CryptoCC26XX Transaction |
| CGPIOCC3200_Config | GPIO device specific driver configuration structure |
| CGPIOMSP430_Config | GPIO device specific driver configuration structure |
| CGPIOMSP432_Config | GPIO device specific driver configuration structure |
| CGPIOTiva_Config | GPIO device specific driver configuration structure |
| CHwiP_Params | Basic HwiP Parameters |
| CI2C_Config | I2C Global configuration |
| CI2C_FxnTable | The definition of a I2C function table that contains the required set of functions to control a specific I2C driver implementation |
| CI2C_Params | I2C Parameters |
| CI2C_Transaction | I2C transaction |
| CI2CCC26XX_HWAttrs | I2CCC26XX Hardware attributes |
| CI2CCC26XX_I2CPinCfg | I2CCC26XX Pin Configuration |
| CI2CCC26XX_Object | I2CCC26XX Object |
| CI2CCC3200_HWAttrs | I2CCC3200 Hardware attributes |
| CI2CCC3200_Object | I2CCC3200 Object |
| CI2CEUSCIB_HWAttrs | I2CEUSCIB Hardware attributes |
| CI2CEUSCIB_Object | I2CEUSCIB Object |
| CI2CMSP432_HWAttrs | I2CMSP432 Hardware attributes These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP430Ware these definitions are found in: |
| CI2CMSP432_Object | I2CMSP432 Object |
| CI2CTiva_HWAttrs | I2CTiva Hardware attributes |
| CI2CTiva_Object | I2CTiva Object |
| CI2CUSCIB_HWAttrs | I2CUSCIB Hardware attributes |
| CI2CUSCIB_Object | I2CUSCIB Object |
| CI2S_BufDesc | I2S buffer descriptor for issue/reclaim mode |
| CI2S_Config | I2S Global configuration |
| CI2S_FxnTable | The definition of a I2S function table that contains the required set of functions to control a specific I2S driver implementation |
| CI2S_Params | Basic I2S Parameters |
| CI2SCC3200DMA_HWAttrs | I2SCC3200DMA Hardware attributes |
| CI2SCC3200DMA_Object | I2SCC3200DMA Object |
| CI2SCC3200DMA_SerialPinConfig | CC3200 Serial Pin Configuration |
| CI2SCC3200DMA_SerialPinParams | CC3200 specific I2S Parameters |
| CI2SCC3200DMA_SerialPinVars | I2SCC3200DMA Serial pin variables |
| CLCD_Buffer | LCD_Buffer used to store data to be printed on the LCD display |
| CLCD_Command | Format of LCD commands used by the LCD controller |
| CLCD_Config | The LCD_Config structure contains a set of pointers used to characterize the LCD driver implementation |
| CLCD_HWAttrs | LCD Hardware attributes |
| CLCD_Object | LCD Object |
| CLCD_Params | LCD Parameters are used to with the LCD_open() call. Default values for these parameters are set using LCD_Params_init() |
| CMutexP_Params | Basic MutexP Parameters |
| CPIN_State_s | Underlying data structure for type PIN_State |
| CPower_NotifyObj | Power notify object structure |
| CPowerCC3200_Config | Power global configuration |
| CPowerCC3200_MCURegisters | MCU core registers that need to be save on entering LPDS |
| CPowerCC3200_ModuleState | Internal module state |
| CPowerCC3200_NVICRegisters | NVIC registers that need to be save on entering LPDS |
| CPowerCC3200_SaveRegisters | Struct of context registers to save on entering LPDS |
| CPowerCC3200_Wakeup | For wakeup from LPDS or shutdown configuration |
| CPowerMSP432_Config | Power global configuration (MSP432-specific) |
| CPowerMSP432_Freqs | Structure holding device frequencies (in Hz) |
| CPWM_Config | PWM Global configuration |
| CPWM_FxnTable | The definition of a PWM function table that contains the required set of functions to control a specific PWM driver implementation |
| CPWM_Params | PWM Parameters |
| CPWMTimerCC3200_HWAttrs | PWMTimerCC3200 Hardware attributes |
| CPWMTimerCC3200_Object | PWMTimerCC3200 Object |
| CPWMTimerMSP432_HWAttrs | PWMTimerMSP432 Hardware attributes |
| CPWMTimerMSP432_Object | PWMTimerMSP432 Object |
| CPWMTimerMSP432_Status | PWMTimerMSP432_Status |
| CPWMTimerTiva_HWAttrs | PWMTimerCC3200 Hardware attributes |
| CPWMTimerTiva_Object | PWMTimerTiva Object |
| CPWMTiva_HWAttrs | PWMTiva Hardware attributes |
| CPWMTiva_Object | PWMTiva Object |
| CPWMTiva_Status | PWMTiva_Status |
| CRF_Mode | Struct defining operating mode of RF driver |
| CRF_Object | Struct used to store RF client state and configuration Pointer to an RF_Object is used as handles (RF_Handle) in interactions with the RF driver |
| CRF_Params | RF parameter struct RF parameters are used with the RF_open() and RF_Params_init() call |
| CRF_RadioSetup | Union of the different flavors of RADIO_SETUP commands |
| CSDSPI_Config | SDSPI Global configuration |
| CSDSPI_FxnTable | The definition of a SDSPI function table that contains the required set of functions to control a specific SDSPI driver implementation |
| CSDSPI_Params | SDSPI Parameters |
| CSDSPICC3200_HWAttrs | SDSPICC3200 Hardware attributes |
| CSDSPICC3200_Object | SDSPICC3200 Object |
| CSDSPIEUSCIA_HWAttrs | SDSPIEUSCIA Hardware attributes |
| CSDSPIEUSCIA_Object | SDSPIEUSCIA Object |
| CSDSPIEUSCIB_HWAttrs | SDSPIEUSCIB Hardware attributes |
| CSDSPIEUSCIB_Object | SDSPIEUSCIB Object |
| CSDSPIMSP432_HWAttrs | SDSPIMSP432 Hardware attributes |
| CSDSPIMSP432_Object | SDSPIMSP432 Object |
| CSDSPITiva_HWAttrs | SDSPITiva Hardware attributes |
| CSDSPITiva_Object | SDSPITiva Object |
| CSDSPIUSCIA_HWAttrs | SDSPIUSCIA Hardware attributes |
| CSDSPIUSCIA_Object | SDSPIUSCIA Object |
| CSDSPIUSCIB_HWAttrs | SDSPIUSCIB Hardware attributes |
| CSDSPIUSCIB_Object | SDSPIUSCIB Object |
| CSemaphoreP_Params | Basic SemaphoreP Parameters |
| CSPI_Config | SPI Global configuration |
| CSPI_FxnTable | The definition of a SPI function table that contains the required set of functions to control a specific SPI driver implementation |
| CSPI_Params | SPI Parameters |
| CSPI_Transaction | A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat frames are sent and received from the buffers pointed to txBuf and rxBuf. The arg variable is an user-definable argument which gets passed to the SPI_CallbackFxn when the SPI driver is in SPI_MODE_CALLBACK |
| CSPICC26XX_HWAttrs | SPICC26XXDMA Hardware attributes |
| CSPICC26XX_Object | SPICC26XXDMA Object |
| CSPICC3200DMA_HWAttrs | SPICC3200DMA Hardware attributes |
| CSPICC3200DMA_Object | SPICC3200DMA Object |
| CSPIEUSCIADMA_HWAttrs | SPIEUSCIADMA Hardware attributes |
| CSPIEUSCIADMA_Object | SPIEUSCIADMA Object |
| CSPIEUSCIBDMA_HWAttrs | SPIEUSCIBDMA Hardware attributes |
| CSPIEUSCIBDMA_Object | SPIEUSCIBDMA Object |
| CSPIMSP432DMA_HWAttrs | SPIMSP432DMA Hardware attributes These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP430Ware these definitions are found in: |
| CSPIMSP432DMA_Object | SPIMSP432DMA Object |
| CSPITivaDMA_HWAttrs | SPITivaDMA Hardware attributes |
| CSPITivaDMA_Object | SPITivaDMA Object |
| CSPIUSCIADMA_HWAttrs | SPIUSCIADMA Hardware attributes |
| CSPIUSCIADMA_Object | SPIUSCIADMA Object |
| CSPIUSCIBDMA_HWAttrs | SPIUSCIBDMA Hardware attributes |
| CSPIUSCIBDMA_Object | SPIUSCIBDMA Object |
| CUART_Config | UART Global configuration |
| CUART_FxnTable | The definition of a UART function table that contains the required set of functions to control a specific UART driver implementation |
| CUART_Params | UART Parameters |
| CUARTCC26XX_HWAttrs | UARTCC26XX Hardware attributes |
| CUARTCC26XX_Object | UARTCC26XX Object |
| CUARTCC3200_FxnSet | Complement set of read functions to be used by the UART ISR and UARTCC3200_read(). Internal use only |
| CUARTCC3200_HWAttrs | UARTCC3200 Hardware attributes |
| CUARTCC3200_Object | UARTCC3200 Object |
| CUARTCC3200DMA_HWAttrs | UARTCC3200DMA Hardware attributes |
| CUARTCC3200DMA_Object | UARTCC3200DMA Object |
| CUARTEUSCIA_BaudrateConfig | UARTEUSCIA Baudrate configuration |
| CUARTEUSCIA_HWAttrs | UARTEUSCIA Hardware attributes |
| CUARTEUSCIA_Object | UARTEUSCIA Object |
| CUARTMSP432_BaudrateConfig | UARTMSP432 Baudrate configuration |
| CUARTMSP432_FxnSet | Complement set of read functions to be used by the UART ISR and UARTMSP432_read(). Internal use only |
| CUARTMSP432_HWAttrs | UARTMSP432 Hardware attributes |
| CUARTMSP432_Object | UARTMSP432 Object |
| CUARTTiva_FxnSet | Complement set of read functions to be used by the UART ISR and UARTTiva_read(). Internal use only |
| CUARTTiva_HWAttrs | UARTTiva Hardware attributes |
| CUARTTiva_Object | UARTTiva Object |
| CUARTTivaDMA_HWAttrs | UARTTivaDMA Hardware attributes |
| CUARTTivaDMA_Object | UARTTivaDMA Object |
| CUARTUSCIA_BaudrateConfig | UARTUSCIA Baudrate configuration |
| CUARTUSCIA_HWAttrs | UARTUSCIA Hardware attributes |
| CUARTUSCIA_Object | UARTUSCIA Object |
| CUDMACC26XX_Config | UDMACC26XX Global configuration |
| CUDMACC26XX_HWAttrs | UDMACC26XX hardware attributes |
| CUDMACC26XX_Object | UDMACC26XX object |
| CWatchdog_Config | Watchdog Global configuration |
| CWatchdog_FxnTable | The definition of a Watchdog function table that contains the required set of functions to control a specific Watchdog driver implementation |
| CWatchdog_Params | Watchdog Parameters |
| CWatchdogCC26XX_HWAttrs | Watchdog hardware attributes for CC26XX |
| CWatchdogCC26XX_Object | Watchdog Object for CC26XX |
| CWatchdogCC3200_HWAttrs | Watchdog hardware attributes for CC3200 |
| CWatchdogCC3200_Object | Watchdog Object for CC3200 |
| CWatchdogMSP430_HWAttrs | Watchdog hardware attributes for MSP430 |
| CWatchdogMSP430_Object | Watchdog Object for MSP430 |
| CWatchdogMSP432_HWAttrs | Watchdog hardware attributes for MSP432 These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP432Ware these definitions are found in: |
| CWatchdogMSP432_Object | Watchdog Object for MSP432 |
| CWatchdogTiva_HWAttrs | Watchdog hardware attributes for Tiva |
| CWatchdogTiva_Object | Watchdog Object for Tiva |