![]() |
![]() |
| _Memory.h [code] | Memory manager interface definitions |
| _MemoryDefs.h [code] | Definitions for Memory module |
| _MemoryOS.h [code] | Memory abstraction APIs for local memory allocation |
| Cache.h [code] | Defines Cache API interface |
| Cfg.h [code] | Configuration Helper Utilities |
| Dev.h [code] | Defines Dev API interface |
| FrameQ.h [code] | Defines for interfaces for FrameQ module |
| FrameQ_ShMem.h [code] | Header file for FrameQ on SharedMemory interface |
| FrameQBufMgr.h [code] | Defines for interfaces for FrameQBufMgr module |
| FrameQBufMgr_ShMem.h [code] | Header file for FrameQBufMgr ShMem |
| FrameQBufMgrDefs.h [code] | Defines configurable elements for FrameQBufMgr module |
| FrameQDefs.h [code] | Defines configurable elements for FrameQ module |
| Gate.h [code] | Critical section support |
| GateMonitor.h [code] | Header file for Gate based on Monitor |
| GateMP.h [code] | Multiple processor gate that provides local and remote context protection |
| GateMutex.h [code] | Gate based on Mutex |
| GateProcess.h [code] | Process level gate |
| GateSem.h [code] | Header file for Gate based on Semaphore |
| GateSpinlock.h [code] | Gate based on Spinlock |
| HeapBufMP.h [code] | Multi-processor fixed-size buffer heap implementation |
| HeapMemMP.h [code] | Multi-processor variable size buffer heap implementation |
| HeapMultiBufMP.h [code] | Multiple fixed size buffer heap implementation |
| HeapQueueMgr.h [code] | Multi-processor fixed-size buffer heap using hardware queues |
| IGateProvider.h [code] | Interface implemented by all gate providers |
| IHeap.h [code] | Defines Heap based memory allocator |
| Ipc.h [code] | Ipc Manager |
| IpcHost.h [code] | This file contains APIs and defines that are used by applications only on the host-side of the device |
| IpcMemMgr.h [code] | IPC Memory Manager |
| List.h [code] | Creates a doubly linked list. It works as utils for other modules |
| ListMP.h [code] | Multiple processor shared memory list |
| Memory.h [code] | Memory manager interface definitions |
| MemoryDefs.h [code] | Definitions for Memory module |
| MemoryOS.h [code] | Memory abstraction APIs for local memory allocation |
| MessageQ.h [code] | MessageQ Manager |
| MultiProc.h [code] | Processor ID Manager |
| NameServer.h [code] | NameServer Manager |
| Notify.h [code] | Notification manager for IPC |
| OsalPrint.h [code] | Kernel utils Print interface definitions |
| OsalSemaphore.h [code] | Kernel utils Semaphore interface definitions |
| ProcMgr.h [code] | The Processor Manager on a master processor provides control functionality for a slave device |
| RingIO.h [code] | This will have definitions for interfaces and structures for RingIO module |
| RingIOShm.h [code] | RingIOShm shared memory based physical transport for communication with the remote processor |
| SharedRegion.h [code] | Shared memory manager and address translator |
| Std.h [code] | This will have definitions of standard data types for platform abstraction |
| String.h [code] | Defines for String manipulation library |
| SysLink.h [code] | This module contains common definitions, types, structures and functions used by SysLink |
| SyslinkMemMgr.h [code] | Header file implementing Memory manager. It is a wrapper implementation to support Shared memory allocation using heap address translations using shared region or Tiler buffer allocation using tiler buffer manager and address translations |
| Trace.h [code] | Kernel Trace enabling/disabling/application interface |