![]() |
![]() |
This module contains common definitions, types, structures and functions used by SysLink.
Go to the source code of this file.
Functions | |
| Void | SysLink_setup (Void) |
| Function to initialize SysLink. | |
| Void | SysLink_destroy (Void) |
| Function to finalize SysLink. | |
Variables | |
| String | SysLink_params |
| Config params override strings. | |
Function to initialize SysLink.
This function must be called in every user process before making calls to any other SysLink APIs.
Function to finalize SysLink.
This function must be called in every user process at the end after all usage of SysLink in that process is complete.
Config params override strings.
This string is a list of semi-colon-delimited "assignments" that can be set by users prior to the initial call to SysLink_setup() to affect system behavior.
Example assignments include:
SL_PARAMS environment variable to set this string's value.SL_PARAMS) prior to running slaveloader.