![]() |
![]() |
|
IPC API
3.40.01.08
|
| ▼ ti | |
| ▼ grcm | |
| RcmClient.h | Remote Command Message Client Module. An RcmClient is used for sending messages to an RcmServer for processing |
| RcmServer.h | Remote Command Message Server Module. An RcmServer processes inbound messages received from an RcmClient |
| RcmTypes.h | Remote Command Message Types |
| ▼ ipc | |
| ▼ ipcmgr | |
| IpcMgr.h | Ipc Manager |
| ▼ mm | |
| MmRpc.h | Multi-Media derived Remote Procedure Call |
| MmServiceMgr.h | Multi-Media Service Manager |
| MmType.h | Specific types to support the MmRpc and MmServiceMgr modules |
| ▼ tests | |
| gatempapp_rsc_table_vayu_dsp.h | |
| GateMPAppCommon.h | |
| Mx.h | Example of a host-side module which uses MmRpc to invoke functions on a remote processor |
| MxServer.h | Example of a slave-side module which implements the Mx module functions. The functions in MxServer are invoked remotely by the Mx module running on the host processor |
| power_rsc_table_vayu_dsp.h | |
| GateMP.h | Multiple processor gate that provides local and remote context protection |
| HeapBufMP.h | Multi-processor fixed-size buffer heap implementation |
| HeapMemMP.h | Multi-processor variable size buffer heap implementation |
| HeapMultiBufMP.h | Multiple fixed size buffer heap implementation |
| Ipc.h | Ipc Manager |
| ListMP.h | Multiple processor shared memory list |
| MessageQ.h | MessageQ Manager |
| MultiProc.h | Processor ID Manager |
| NameServer.h | NameServer Manager |
| Notify.h | Notification manager for IPC |
| SharedRegion.h | Shared memory manager and address translator |
| ▼ pm | |
| _IpcPower.h | |
| IpcPower.h |