SharedRegion.h File Reference
Detailed Description
Shared memory manager and address translator.
===========================================================================
The SharedRegion module is designed to be used in a multi-processor environment in which memory regions are shared and accessed across different processors. The module itself does not use any shared memory, because all module state is stored locally. SharedRegion APIs use the system gate for thread protection.
This module creates and stores a local shared memory region table. The table contains the processor's view for every shared region in the system. The table must not contain any overlapping regions. Each processor's view of a particular shared memory region is determined by the region id. In cases where a processor cannot access a certain shared memory region, that shared memory region should be left invalid for that processor. Note: The number of entries must be the same on all processors.
Each shared region contains the following:
- base - The base address
- len - The length
- name - The name of the region
- isValid - Whether the region is valid
- ownerProcId - The id of the processor which owns the region
- cacheEnable - Whether the region is cacheable
- cacheLineSize - The cache line size
- createHeap - Whether a heap is created for the region.
A region is added using the SharedRegion_setEntry API. The length of a region must be the same across all processors. The owner of the region can be specified. If specified, the owner manages the shared region. It creates a HeapMemMP instance which spans the full size of the region. The other processors open the same HeapMemMP instance.
After a shared region is valid, SharedRegion APIs can be used to convert pointers between the local processor's address space and the SharedRegion- pointer (SRPtr) address space. These APIs include SharedRegion_getId, SharedRegion_getSRPtr and SharedRegion_getPtr. An example is shown below:
============================================================================
Go to the source code of this file.
Define Documentation
| #define SharedRegion_S_BUSY 2 |
The resource is still in use.
| #define SharedRegion_S_ALREADYSETUP 1 |
The module has been already setup.
| #define SharedRegion_S_SUCCESS 0 |
| #define SharedRegion_E_FAIL -1 |
| #define SharedRegion_E_INVALIDARG -2 |
Argument passed to function is invalid.
| #define SharedRegion_E_MEMORY -3 |
Operation resulted in memory failure.
| #define SharedRegion_E_ALREADYEXISTS -4 |
The specified entity already exists.
| #define SharedRegion_E_NOTFOUND -5 |
Unable to find the specified entity.
| #define SharedRegion_E_TIMEOUT -6 |
| #define SharedRegion_E_INVALIDSTATE -7 |
Module is not initialized.
| #define SharedRegion_E_OSFAILURE -8 |
A failure occurred in an OS-specific call.
| #define SharedRegion_E_RESOURCE -9 |
Specified resource is not available.
| #define SharedRegion_E_RESTART -10 |
Operation was interrupted. Please restart the operation.
| #define SharedRegion_INVALIDREGIONID (0xFFFF) |
| #define SharedRegion_DEFAULTOWNERID (UInt16)(~0) |
Default owner processor id.
Typedef Documentation
SharedRegion pointer type.
Function Documentation
| Int SharedRegion_clearEntry |
( |
UInt16 |
regionId |
) |
|
Initializes the entry fields.
- Parameters:
-
| entry | pointer to a SharedRegion entry |
- See also:
- SharedRegion_setEntry
| SizeT SharedRegion_getCacheLineSize |
( |
UInt16 |
regionId |
) |
|
Gets the entry information for the specified region id.
- Parameters:
-
| regionId | the region id |
| entry | pointer to return region information |
- Returns:
- Status
- See also:
- SharedRegion_setEntry
| Ptr SharedRegion_getHeap |
( |
UInt16 |
regionId |
) |
|
Gets the heap associated with the specified region id.
- Parameters:
-
- Returns:
- Handle of the heap, NULL if the region has no heap
| UInt16 SharedRegion_getId |
( |
Ptr |
addr |
) |
|
Gets the region id for the specified address.
- Parameters:
-
- Returns:
- region id
| UInt16 SharedRegion_getIdByName |
( |
String |
name |
) |
|
Gets the id of a region, given its name.
- Parameters:
-
- Returns:
- region id
| UInt16 SharedRegion_getNumRegions |
( |
Void |
|
) |
|
Gets the number of regions.
- Returns:
- number of regions
Calculate the local pointer from the shared region pointer.
- Parameters:
-
| srptr | SharedRegion pointer |
- Returns:
- local pointer
- See also:
- SharedRegion_getPtr
Calculate the shared region pointer given local address and id.
- Parameters:
-
| addr | the local address |
| regionId | region id |
- Returns:
- SharedRegion pointer
- See also:
- SharedRegion_getPtr
| Bool SharedRegion_isCacheEnabled |
( |
UInt16 |
regionId |
) |
|
whether cache enable was specified
- Parameters:
-
- Returns:
- 'TRUE' if cache enable specified, otherwise 'FALSE'
Sets the entry at the specified region id.
- Parameters:
-
| regionId | region id |
| entry | pointer to set region information. |
- Returns:
- Status
| Bool SharedRegion_translateEnabled |
( |
Void |
|
) |
|
Whether address translation is enabled.
- Returns:
- 'TRUE' if translate is enabled otherwise 'FALSE'
Returns the SharedRegion_SRPtr value that maps to NULL.
- Returns:
- Value in SRPtr-space that maps to NULL in Ptr-space