![]() |
![]() |
Remote Command Message Server Module. An RcmServer processes inbound messages received from an RcmClient. More...
Functions | |
| Int | RcmServer_addSymbol (RcmServer_Handle handle, String name, RcmServer_MsgFxn addr, UInt32 *index) |
| Add a symbol to the server's function table. | |
| Int | RcmServer_construct (RcmServer_Struct *structPtr, String name, const RcmServer_Params *params) |
| Initialize a new instance object inside the provided structure. | |
| Int | RcmServer_create (String name, RcmServer_Params *params, RcmServer_Handle *handle) |
| Create an RcmServer instance. | |
| Int | RcmServer_delete (RcmServer_Handle *handlePtr) |
| Delete an RcmServer instance. | |
| Int | RcmServer_destruct (RcmServer_Struct *structPtr) |
| Finalize the instance object inside the provided structure. | |
| Void | RcmServer_exit (Void) |
| Finalize the RcmServer module. | |
| Void | RcmServer_init (Void) |
| Initialize the RcmServer module. | |
| Void | RcmServer_Params_init (RcmServer_Params *params) |
| Initialize the instance create params structure. | |
| Int | RcmServer_removeSymbol (RcmServer_Handle handle, String name) |
| Remove a symbol and from the server's function table. | |
| Int | RcmServer_start (RcmServer_Handle handle) |
| Start the server. | |
Defines | |
| #define | RcmServer_S_SUCCESS (0) |
| Success return code. | |
| #define | RcmServer_E_FAIL (-1) |
| General failure return code. | |
| #define | RcmServer_E_NOMEMORY (-2) |
| The was insufficient memory left on the heap. | |
| #define | RcmServer_E_SYMBOLNOTFOUND (-3) |
| The given symbol was not found in the server's symbol table. | |
| #define | RcmServer_E_SYMBOLSTATIC (-4) |
| The given symbols is in the static table, it cannot be removed. | |
| #define | RcmServer_E_SYMBOLTABLEFULL (-5) |
| The server's symbol table is full. | |
Data Structures | |
| struct | RcmServer_FxnDesc |
| Function descriptor. More... | |
| struct | RcmServer_FxnDescAry |
| Function descriptor array. More... | |
| struct | RcmServer_ThreadPoolDesc |
| Worker pool descriptor. More... | |
| struct | RcmServer_ThreadPoolDescAry |
| Worker pool descriptor array. More... | |
| struct | RcmServer_Params |
| RcmServer Instance create parameters. More... | |
| struct | RcmServer_Struct |
| Opaque client structure large enough to hold an instance object. More... | |
Typedefs | |
| typedef Int32(* | RcmServer_MsgFxn )(UInt32, UInt32 *) |
| Remote function type. | |
| typedef struct RcmServer_Object_tag * | RcmServer_Handle |
| RcmServer instance object handle. | |
Remote Command Message Server Module. An RcmServer processes inbound messages received from an RcmClient.
The RcmServer module is used to create an server instance. RcmClients send their messages to only one RcmServer instance for processing. The server instance can be created with a function dispatch table and additional tables can be added as requested by the clients.
Diagnostics
Diags_INFO - full detail log events Diags_USER1 - message processing
| Int RcmServer_addSymbol | ( | RcmServer_Handle | handle, |
| String | name, | ||
| RcmServer_MsgFxn | addr, | ||
| UInt32 * | index | ||
| ) |
Add a symbol to the server's function table.
This function adds a new symbol to the server's function table. This is useful for supporting Dynamic Load Libraries (DLLs).
| [in] | handle | Handle to an instance object. |
| [in] | name | The function's name. |
| [in] | addr | The function's address in the server's address space. |
| [out] | index | The function's index value to be used in the RcmClient_Message.fxnIdx field. |
| RcmClient_S_SUCCESS | |
| RcmServer_E_NOMEMORY | |
| RcmServer_E_SYMBOLTABLEFULL |
| Int RcmServer_construct | ( | RcmServer_Struct * | structPtr, |
| String | name, | ||
| const RcmServer_Params * | params | ||
| ) |
Initialize a new instance object inside the provided structure.
This function is the same as RcmServer_create() except that it does not allocate memory for the instance object. The instance object is constructed inside the provided structure. Call RcmServer_destruct() to finalize a constructed instance object.
| [in] | structPtr | A pointer to an allocated structure. |
| [in] | name | The name of the server. The RcmClient will locate a server instance using this name. It must be unique to the system. |
| [in] | params | The create params used to customize the instance object. |
| RcmClient_S_SUCCESS | |
| RcmServer_E_FAIL | |
| RcmServer_E_NOMEMORY |
| Int RcmServer_create | ( | String | name, |
| RcmServer_Params * | params, | ||
| RcmServer_Handle * | handle | ||
| ) |
Create an RcmServer instance.
A server instance is used to execute functions on behalf of an RcmClient instance. There can be multiple server instances on any given CPU. The servers typically reside on a remote CPU from the RcmClient instance.
| [in] | name | The name of the server. The RcmClient will locate a server instance using this name. It must be unique to the system. |
| [in] | params | The create params used to customize the instance object. |
| [out] | handle | An opaque handle to the created instance object. |
| RcmClient_S_SUCCESS | |
| RcmServer_E_FAIL | |
| RcmServer_E_NOMEMORY |
| Int RcmServer_delete | ( | RcmServer_Handle * | handlePtr ) |
Delete an RcmServer instance.
| [in,out] | handlePtr | Handle to the instance object to delete. |
| Int RcmServer_destruct | ( | RcmServer_Struct * | structPtr ) |
Finalize the instance object inside the provided structure.
| [in] | structPtr | A pointer to the structure containing the instance object to finalize. |
| Void RcmServer_exit | ( | Void | ) |
Finalize the RcmServer module.
This function is used to finalize the RcmServer module. Any resources acquired by RcmServer_init() will be released. Do not call any RcmServer functions after calling RcmServer_exit().
This function must be serialized by the caller.
| Void RcmServer_init | ( | Void | ) |
Initialize the RcmServer module.
This function is used to initialize the RcmServer module. Call this function before calling any other RcmServer function.
This function must be serialized by the caller
| Void RcmServer_Params_init | ( | RcmServer_Params * | params ) |
Initialize the instance create params structure.
| Int RcmServer_removeSymbol | ( | RcmServer_Handle | handle, |
| String | name | ||
| ) |
Remove a symbol and from the server's function table.
Useful when unloading a DLL from the server.
| [in] | handle | Handle to an instance object. |
| [in] | name | The function's name. |
| RcmClient_S_SUCCESS | |
| RcmServer_E_SYMBOLNOTFOUND | |
| RcmServer_E_SYMBOLSTATIC |
| Int RcmServer_start | ( | RcmServer_Handle | handle ) |
Start the server.
The server is created in stop mode. It will not start processing messages until it has been started.
| [in] | handle | Handle to an instance object. |
| RcmClient_S_SUCCESS | |
| RcmServer_E_FAIL |
| #define RcmServer_S_SUCCESS (0) |
Success return code.
| #define RcmServer_E_FAIL (-1) |
General failure return code.
| #define RcmServer_E_NOMEMORY (-2) |
The was insufficient memory left on the heap.
| #define RcmServer_E_SYMBOLNOTFOUND (-3) |
The given symbol was not found in the server's symbol table.
This error could occur if the symbol spelling is incorrect or if the RcmServer is still loading its symbol table.
| #define RcmServer_E_SYMBOLSTATIC (-4) |
The given symbols is in the static table, it cannot be removed.
All symbols installed at instance create time are added to the static symbol table. They cannot be removed. The statis symbol table must remain intact for the lifespan of the server instance.
| #define RcmServer_E_SYMBOLTABLEFULL (-5) |
The server's symbol table is full.
The symbol table is full. You must remove some symbols before any new symbols can be added.
| typedef Int32(* RcmServer_MsgFxn)(UInt32, UInt32 *) |
Remote function type.
All functions executed by the RcmServer must be of this type. Typically, these functions are simply wrappers to the vendor function. The server invokes this remote function by passing in the RcmClient_Message.dataSize field and the address of the RcmClient_Message.data array.
RcmServer_MsgFxn fxn = ...; RcmClient_Message *msg = ...; msg->result = (*fxn)(msg->dataSize, msg->data);
| typedef struct RcmServer_Object_tag* RcmServer_Handle |
RcmServer instance object handle.