|
|
TI-Drivers is a software component that includes device drivers for the assorted peripherals on a given device (i.e., UART, SPI, I2C, etc.).
These device drivers are also included in the TI-RTOS product. They are provided here as a separate component so that they can be used as a stand-alone library in non-TI-RTOS environments. To avoid duplication, TI-RTOS includes this versioned component in the tirtos/products directory.
The following documentation is provided with this release.
NOTE: Please view the Device Specific driver implementations as they may contain or exclude certain features that are defined in the top level interfaces.
License and manifest.
Release notes from previous releases are also available in the release notes archive directory.
TIDRIVERS JIRA Identifier | Summary |
---|---|
TIDRIVERS-523 | use PCM_getPowerState instead of PCM_getPowerMode in PowerMSP432.c |
TIDRIVERS-504 | RingBuf_peek can return non-atomic data |
TIDRIVERS-473 | I2CMSP432 driver needs rework of set/release of Power constraints |
TIDRIVERS-456 | Concurrent read/write access to UART not possible |
TIDRIVERS-450 | Consider marking “.vtable” section as NOLOAD for Tiva/MSP432 devices to ease small .bin file generation |
TIDRIVERS-433 | Implement Watchdog_convertMsToTicks() API on all platforms |
TIDRIVERS-430 | Use FORCE_LPM_ENTRY for MSP432 transistions to DEEPSLEEP and SHUTDOWN |
TIDRIVERS-424 | API documentation of UART.h does not highlight the necessity of cancelling asynchronous operations |
TIDRIVERS-422 | Add pin parking support during LPM3+ (ti.drivers.power.PowerMSP432) |
TIDRIVERS-419 | Add a Power_setPolicy() API |
TIDRIVERS-408 | FatFS is missing utils directory in ti.mw.fatfs |
TIDRIVERS-367 | ADC driver (single version) implementation and ADC14MSP432 implementation |
TIDRIVERS-360 | Add Power_disablePolicy() |
TIDRIVERS-356 | Add a DMA driver for MSP432 |
TIDRIVERS-309 | Remove GPIOMSP432 workaround |
TIDRIVERS-176 | MSP430’s I2CEUSCIB driver is not initializing all the EUSCI_B_I2C_initMasterParam fields |
TIDRIVERS-124 | For MSP432 add a lighter-weight sleep policy that is enabled by default |
TIDRIVERS-114 | Add an ADC driver into TI-RTOS |
Supported Operating Systems:
This release requires the following software components and tools versions to successfully function:
This release was validated using the following components:
None
Please check the TI-RTOS Support Wiki for issues found after this product was released.
All releases have 4 digits (M.mm.pp.bb). This includes GA and pre-releases (engineering, alpha/EA, beta, etc.). Pre-releases are denoted with a suffix (e.g. 6.30.00.00-eng or 6.30.00.10-beta).
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and bb is an unrestricted set of digits used as an incrementing build counter.
To support multiple side-by-side installations of the product, the product version is encoded in the top level directory.
Subsequent releases of patch upgrades will be identified by the patch number. Typically, these patches only include critical bug fixes.
Last updated: June 22, 2016 Build Ver: 2.20.00.08