![]() |
![]() |
#include <ip6if.h>
Data Fields | |
UINT32 | InReceives |
Total number of packets received. | |
UINT32 | InHdrErrors |
Packets dropped because of header errors. | |
UINT32 | InMcastPkts |
Number of multicast packets received. | |
UINT32 | InTruncatedPkts |
Number of truncated packets received. | |
UINT32 | InForwErrors |
Number of packets dropped because we had to forward. | |
UINT32 | InExtnHdrErrors |
Packets dropped because extension header parse failed. | |
UINT32 | InReasmReqds |
Number of fragments awaiting reassembly. | |
UINT32 | InReasmFails |
Number of fragment reassembly failures/timeouts. | |
UINT32 | InReasmOKs |
Number of successful reassemblies. | |
UINT32 | InUnknownProtos |
Packets dropped because the L4 Proto was not supported. | |
UINT32 | InDelivers |
Packets successfully delivered to host stack. | |
UINT32 | OutRequests |
Total number of packets transmit requests from host stack. | |
UINT32 | OutNoRoutes |
Packets dropped because of no route to destination. | |
UINT32 | OutFragReqds |
Number of Packets on Tx path that need to be fragmented in order to be transmitted successfully. | |
UINT32 | OutFragFails |
Number of Packets on Tx path that need to be fragmented but couldnt be fragmented because of some error. | |
UINT32 | OutFragOKs |
Number of Packets on Tx path that were fragmented successfully. | |
UINT32 | OutFragCreates |
Number of Packets generated on Tx path due to fragmentation. | |
UINT32 | OutMcastPkts |
Number of Multicast packets sent out by the host IPv6 stack. | |
UINT32 | OutDiscards |
Number of packets discarded because of errors on Tx path. | |
UINT32 | OutTransmits |
Number of packets successfully transmitted by the host IPv6 stack. |
This structure is used to hold various packet stats for receive and transmit paths of the core IPv6 module. The stats maintained in this structure are defined as per IP MIBs defined in RFC 4293.