![]() |
![]() |
Functions | |
int | Sock6PcbAttach (HANDLE hSock) |
int | Sock6PcbDetach (HANDLE hSock) |
int | Sock6PcbBind (HANDLE hSock, IP6N LIP, uint LPort) |
int | Sock6PcbConnect (HANDLE hSock, IP6N FIP, uint FPort) |
HANDLE | Sock6PcbResolveChain (HANDLE hSock, uint SockProt, uint Prot, IP6N LIP, uint LPort, IP6N FIP, uint FPort) |
HANDLE | Sock6PcbResolve (uint SockProt, IP6N LIP, uint LPort, IP6N FIP, uint FPort, uint Match) |
void | Sock6PcbRtChange (HANDLE hRt6) |
void | Sock6PcbCleanup () |
void | Sock6CleanPcb (uint SockProt, IP6N IPAddress) |
void Sock6CleanPcb | ( | uint | SockProt, | |
IP6N | IPAddress | |||
) |
Description
The function cycles through all the socket entries for the specified protocol family and closes any socket which matches the IP Address specified. The function was added to ensure that when an IP address is modified then any sockets which are using the OLD IP Address should be closed.
This is for *internal* NDK Stack Usage.
[in] | SockProt | Socket Family |
[in] | IPAddress | OLD IP Address to which a socket might be bound to and which needs to be cleaned. |
Not | Applicable |
int Sock6PcbAttach | ( | HANDLE | hSock | ) |
Description
The function attaches the SOCKET to the appropriate list.
[in] | hSock | The pointer to the socket which we will attach to the corresponding list. |
Success | - 0 | |
Error | - Non Zero |
int Sock6PcbBind | ( | HANDLE | hSock, | |
IP6N | LIP, | |||
uint | LPort | |||
) |
Description
The function binds the socket to the specific Local IP and Port.
[in] | hSock | Handle to the socket which is to be bound. |
[in] | LIP | Local IPv6 Address to which the socket is to bound. |
[in] | LPort | Local Port to which the socket is to be bound. |
Success | - 0 | |
Error | - Non Zero |
void Sock6PcbCleanup | ( | ) |
Description
The function aborts all closing sockets in the IPv6 socket family.
Not | Applicable. |
int Sock6PcbConnect | ( | HANDLE | hSock, | |
IP6N | FIP, | |||
uint | FPort | |||
) |
Description
The function sets the Foreign IP And Port in the SOCKET to the ones passed in this API. The function ensures there is no duplication present.
[in] | hSock | Socket Handle to be configured with the IP and Port. |
[in] | FIP | Foreign IP Address |
[in] | FPort | Foreign Port |
Success | - 0 | |
Error | - Non Zero |
int Sock6PcbDetach | ( | HANDLE | hSock | ) |
Description
The function detaches the SOCKET from the appropriate list.
[in] | hSock | The pointer to the socket which we will detach from the corresponding list. |
Success | - 0 | |
Error | - Non Zero |
HANDLE Sock6PcbResolve | ( | uint | SockProt, | |
IP6N | LIP, | |||
uint | LPort, | |||
IP6N | FIP, | |||
uint | FPort, | |||
uint | Match | |||
) |
Description
The function finds a socket matching the criteria given.
[in] | SockProt | The Socket Protocol Family. |
[in] | LIP | The Local IPv6 Address |
[in] | LPort | The Local Port |
[in] | FIP | The Foreign IPv6 Address |
[in] | FPort | The Foreign Port |
[in] | Match | The type of resolution which is being sought.
|
Handle | to Socket Matching the search criteria. |
HANDLE Sock6PcbResolveChain | ( | HANDLE | hSock, | |
uint | SockProt, | |||
uint | Prot, | |||
IP6N | LIP, | |||
uint | LPort, | |||
IP6N | FIP, | |||
uint | FPort | |||
) |
Description
The function finds a socket matching the criteria given. The function unlike the SockPcbResolve can be used to start searches from various points in the list.
[in] | hSock | The socket handle from where the search will start. A value of 0 here indicates that the search is started from the begining of the list. |
[in] | SockProt | The Socket Protocol Family. |
[in] | Prot | The Protocol family |
[in] | LIP | The Local IPv6 Address |
[in] | LPort | The Local Port |
[in] | FIP | The Foreign IPv6 Address |
[in] | FPort | The Foreign Port |
Handle | to Socket Matching the search criteria. |
void Sock6PcbRtChange | ( | HANDLE | hRt6 | ) |
Description
The function is called from the ROUTE6 Module to indicate that there has been a change in the IPv6 ROUTING Table. The function invalidates all sockets which have cached this route This will ensure that subsequent packets being transmitted via these sockets relook the routing table for the correct match.
[in] | hRt6 | Handle to the V6 routing entry which has expired. |
Not | Applicable |