![]() |
![]() |
Functions | |
| HANDLE | SB6New (INT32 Max, INT32 Min, uint Mode) |
| void | SB6Free (HANDLE h) |
| void | SB6Flush (HANDLE h, uint fFree) |
| INT32 | SB6Read (HANDLE h, INT32 Size, INT32 Off, UINT8 *pbDst, PSA_IN6 pPeer, UINT8 flagPeek) |
| INT32 | SB6Write (HANDLE h, INT32 Size, void *pData, PBM_Pkt *pPkt) |
| INT32 | SB6SetMax (HANDLE h, INT32 Max) |
| void SB6Flush | ( | HANDLE | h, | |
| uint | fFree | |||
| ) |
Description
The function is called to flush out all data in the socket buffers. The function is similar to SB6Free except it does not clean out the SOCKET Buffer object itself.
| [in] | h | Handle to the socket buffer object |
| [in] | fFree | Flag which indicates how to handle internal SB memory. When set to 1 the function will clean up the internal memory and when passed as 0; the internal memory block will be retained |
| Not | Applicable. |
| void SB6Free | ( | HANDLE | h | ) |
Description
The function is called to cleanup the socket buffer object for V6.
| [in] | h | Handle to the socket buffer object which is to be cleaned up. |
| Not | Applicable. |
| HANDLE SB6New | ( | INT32 | Max, | |
| INT32 | Min, | |||
| uint | Mode | |||
| ) |
Description
The function is called to create a new socket buffer for the IPv6 socket layer.
| [in] | Max | Sets the Maximum Buffer size. |
| [in] | Min | Sets the Minimum Buffer size |
| [in] | Mode | This defines the mode in which the Socket Buffer will operate. Valid values for these are as follows:-
|
| Success | - 0 | |
| Error | - Non Zero |
| INT32 SB6Read | ( | HANDLE | h, | |
| INT32 | Size, | |||
| INT32 | Off, | |||
| UINT8 * | pbDst, | |||
| PSA_IN6 | pPeer, | |||
| UINT8 | flagPeek | |||
| ) |
Description
The function is called to read data from the Socket Buffer object.
| [in] | h | Handle to the socket buffer object |
| [in] | Size | Size of the Buffer in which data has to be copied. |
| [in] | Off | Offset |
| [in] | pbDst | Pointer to the destination where the data has to be copied to. |
| [in] | pPeer | Pointer to the peer information record; where information about the peer is recorded. |
| [in] | flagPeek | Flag which indicates if the function was just called to PEEK or READ. In PEEK i.e. flagPeek = 0 the pointers in the SOCKET buffer object are not updated. |
| Error | - 0 | |
| Success | - Number of bytes read and copied into the supplied buffer. |
| INT32 SB6SetMax | ( | HANDLE | h, | |
| INT32 | Max | |||
| ) |
Description
The function sets the max bytes held in the socket buffer.
| [in] | h | Handle to the socket buffer object |
| [in] | Max | New MAXIMUM Size |
| Success | - Returns the same value as 'Max' | |
| Error | - Returns the original value i.e. '!Max' |
| INT32 SB6Write | ( | HANDLE | h, | |
| INT32 | Size, | |||
| void * | pData, | |||
| PBM_Pkt * | pPkt | |||
| ) |
Description
The function is called to write data to the Socket Buffer object.
| [in] | h | Handle to the socket buffer object |
| [in] | Size | Size of the Buffer from where data has to be copied. |
| [in] | pData | Pointer to where the data payload starts. |
| [in] | pPkt | Pointer to received packet whose data payload is added to the socket buffer. |
| Error | - 0 | |
| Success | - Number of bytes copied into the socket buffer. |