TI-RTOS for SimpleLink Wireless MCUs  2.14.02.22
Data Fields
WatchdogMSP430_HWAttrs Struct Reference

Watchdog hardware attributes for MSP430. More...

#include <WatchdogMSP430.h>

Data Fields

uint32_t baseAddr
 
uint32_t sfrAddr
 
uint8_t clockSource
 
uint8_t clockDivider
 

Detailed Description

Watchdog hardware attributes for MSP430.

Field Documentation

uint32_t WatchdogMSP430_HWAttrs::baseAddr

Base address of Watchdog

uint32_t WatchdogMSP430_HWAttrs::sfrAddr

SFR base address for Watchdog enabled

uint8_t WatchdogMSP430_HWAttrs::clockSource

Clock source for Watchdog

uint8_t WatchdogMSP430_HWAttrs::clockDivider

Clock divider for Watchdog


The documentation for this struct was generated from the following file:
Copyright 2015, Texas Instruments Incorporated