TI-RTOS for SimpleLink Wireless MCUs  2.14.02.22
Data Fields
UARTMSP432_Object Struct Reference

UARTMSP432 Object. More...

#include <UARTMSP432.h>

Collaboration diagram for UARTMSP432_Object:
Collaboration graph
[legend]

Data Fields

struct {
   bool   opened:1
 
   UART_Mode   readMode:1
 
   UART_Mode   writeMode:1
 
   UART_DataMode   readDataMode:1
 
   UART_DataMode   writeDataMode:1
 
   UART_ReturnMode   readReturnMode:1
 
   UART_Echo   readEcho:1
 
   bool   writeCR:1
 
   bool   bufTimeout:1
 
   bool   callCallback:1
 
   bool   drainByISR:1
 
   bool   rxEnabled:1
 
   bool   txEnabled:1
 
state
 
HwiP_Handle hwiHandle
 
ClockP_Handle timeoutClk
 
uint32_t baudRate
 
UART_STOP stopBits
 
UART_PAR parityType
 
RingBuf_Object ringBuffer
 
UARTMSP432_FxnSet readFxns
 
unsigned char * readBuf
 
size_t readSize
 
size_t readCount
 
SemaphoreP_Handle readSem
 
unsigned int readTimeout
 
UART_Callback readCallback
 
const unsigned char * writeBuf
 
size_t writeSize
 
size_t writeCount
 
SemaphoreP_Handle writeSem
 
unsigned int writeTimeout
 
UART_Callback writeCallback
 
unsigned int writeEmptyClkTimeout
 
Power_NotifyObj perfChangeNotify
 
uint32_t perfConstraintMask
 

Detailed Description

UARTMSP432 Object.

The application must not access any member variables of this structure!

Field Documentation

bool UARTMSP432_Object::opened
UART_Mode UARTMSP432_Object::readMode
UART_Mode UARTMSP432_Object::writeMode
UART_DataMode UARTMSP432_Object::readDataMode
UART_DataMode UARTMSP432_Object::writeDataMode
UART_ReturnMode UARTMSP432_Object::readReturnMode
UART_Echo UARTMSP432_Object::readEcho
bool UARTMSP432_Object::writeCR
bool UARTMSP432_Object::bufTimeout
bool UARTMSP432_Object::callCallback
bool UARTMSP432_Object::drainByISR
bool UARTMSP432_Object::rxEnabled
bool UARTMSP432_Object::txEnabled
struct { ... } UARTMSP432_Object::state
HwiP_Handle UARTMSP432_Object::hwiHandle
ClockP_Handle UARTMSP432_Object::timeoutClk
uint32_t UARTMSP432_Object::baudRate
UART_STOP UARTMSP432_Object::stopBits
UART_PAR UARTMSP432_Object::parityType
RingBuf_Object UARTMSP432_Object::ringBuffer
UARTMSP432_FxnSet UARTMSP432_Object::readFxns
unsigned char* UARTMSP432_Object::readBuf
size_t UARTMSP432_Object::readSize
size_t UARTMSP432_Object::readCount
SemaphoreP_Handle UARTMSP432_Object::readSem
unsigned int UARTMSP432_Object::readTimeout
UART_Callback UARTMSP432_Object::readCallback
const unsigned char* UARTMSP432_Object::writeBuf
size_t UARTMSP432_Object::writeSize
size_t UARTMSP432_Object::writeCount
SemaphoreP_Handle UARTMSP432_Object::writeSem
unsigned int UARTMSP432_Object::writeTimeout
UART_Callback UARTMSP432_Object::writeCallback
unsigned int UARTMSP432_Object::writeEmptyClkTimeout
Power_NotifyObj UARTMSP432_Object::perfChangeNotify
uint32_t UARTMSP432_Object::perfConstraintMask

The documentation for this struct was generated from the following file:
Copyright 2015, Texas Instruments Incorporated