TI-RTOS for SimpleLink Wireless MCUs  2.14.02.22
Data Fields
PowerMSP432_Freqs Struct Reference

Structure holding device frequencies (in Hz) More...

#include <PowerMSP432.h>

Data Fields

unsigned int MCLK
 
unsigned int HSMCLK
 
unsigned int SMCLK
 
unsigned int ACLK
 

Detailed Description

Structure holding device frequencies (in Hz)

Field Documentation

unsigned int PowerMSP432_Freqs::MCLK
unsigned int PowerMSP432_Freqs::HSMCLK
unsigned int PowerMSP432_Freqs::SMCLK
unsigned int PowerMSP432_Freqs::ACLK

The documentation for this struct was generated from the following file:
Copyright 2015, Texas Instruments Incorporated