TI-RTOS for SimpleLink Wireless MCUs  2.14.02.22
Data Fields
I2CEUSCIB_HWAttrs Struct Reference

I2CEUSCIB Hardware attributes. More...

#include <I2CEUSCIB.h>

Data Fields

uint32_t baseAddr
 
uint8_t clockSource
 

Detailed Description

I2CEUSCIB Hardware attributes.

These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP430Ware these definitions are found in:

A sample structure is shown below:

const I2CEUSCIB_HWAttrs i2cUSCIBHWAttrs[] = {
{
.baseAddr = EUSCI_B0_BASE,
.clockSource = EUSCI_B_SPI_CLOCKSOURCE_SMCLK
},
{
.baseAddr = EUSCI_B1_BASE,
.clockSource = EUSCI_B_SPI_CLOCKSOURCE_SMCLK
},
};

Field Documentation

uint32_t I2CEUSCIB_HWAttrs::baseAddr

EUSCI_B_I2C Peripheral's base address

uint8_t I2CEUSCIB_HWAttrs::clockSource

EUSCI_B_I2C Clock source


The documentation for this struct was generated from the following file:
Copyright 2015, Texas Instruments Incorporated