TI-RTOS for SimpleLink Wireless MCUs  2.14.02.22
Data Fields
HwiP_Params Struct Reference

Basic HwiP Parameters. More...

#include <HwiP.h>

Data Fields

char * name
 
uintptr_t arg
 
uint32_t priority
 

Detailed Description

Basic HwiP Parameters.

Structure that contains the parameters passed into HwiP_create when creating a HwiP instance. The HwiP_Params_init function should be used to initialize the fields to default values before the application sets the fields manually. The HwiP default parameters are noted in HwiP_Params_init.

Field Documentation

char* HwiP_Params::name

Name of the clock instance. Memory must persist for the life of the clock instance. This can be used for debugging purposes, or set to NULL if not needed.

uintptr_t HwiP_Params::arg

Argument passed into the Hwi function.

uint32_t HwiP_Params::priority

Device specific priority.


The documentation for this struct was generated from the following file:
Copyright 2015, Texas Instruments Incorporated