TI-RTOS for SimpleLink Wireless MCUs  2.14.02.22
Data Structures | Typedefs | Enumerations | Variables
SDSPIUSCIA.h File Reference

Detailed Description

SDSPI driver implementation for a USCI SPI peripheral used with the SDSPI driver.

============================================================================

The SDSPI header file should be included in an application as follows:

This SDSPI driver implementation is designed to operate on a USCI SPI controller in a simple polling method.


#include <stdint.h>
#include <ti/drivers/SDSPI.h>
#include <ti/sysbios/fatfs/ff.h>
#include <ti/sysbios/fatfs/diskio.h>
Include dependency graph for SDSPIUSCIA.h:

Go to the source code of this file.

Data Structures

struct  SDSPIUSCIA_HWAttrs
 SDSPIUSCIA Hardware attributes. More...
 
struct  SDSPIUSCIA_Object
 SDSPIUSCIA Object. More...
 

Typedefs

typedef enum SDSPIUSCIA_CartType SDSPIUSCIA_CardType
 SD Card type inserted. More...
 
typedef struct SDSPIUSCIA_HWAttrs SDSPIUSCIA_HWAttrs
 
typedef struct SDSPIUSCIA_Object SDSPIUSCIA_Object
 SDSPIUSCIA Object. More...
 
typedef struct SDSPIUSCIA_ObjectSDSPIUSCIA_Handle
 

Enumerations

enum  SDSPIUSCIA_CartType {
  NOCARD = 0,
  MMC = 1,
  SDSC = 2,
  SDHC = 3
}
 SD Card type inserted. More...
 

Variables

const SDSPI_FxnTable SDSPIUSCIA_fxnTable
 

Typedef Documentation

SD Card type inserted.

SDSPIUSCIA Object.

The application must not access any member variables of this structure!

Enumeration Type Documentation

SD Card type inserted.

Enumerator
NOCARD 

Unrecognized Card

MMC 

Multi-media Memory Card (MMC)

SDSC 

Standard SDCard (SDSC)

SDHC 

High Capacity SDCard (SDHC)

Variable Documentation

const SDSPI_FxnTable SDSPIUSCIA_fxnTable
Copyright 2015, Texas Instruments Incorporated