![]() |
![]() |
TI-RTOS for SimpleLink Wireless MCUs
2.14.02.22
|
I2S driver implementation for a CC3200 I2S controller.
============================================================================
The I2S header file should be included in an application as follows:
#include <stdint.h>
#include <stdbool.h>
#include <ti/drivers/I2S.h>
#include <ti/drivers/ports/HwiP.h>
#include <ti/drivers/ports/SemaphoreP.h>
#include <ti/drivers/utils/List.h>
Go to the source code of this file.
Data Structures | |
struct | I2SCC3200DMA_HWAttrs |
I2SCC3200DMA Hardware attributes. More... | |
struct | I2SCC3200DMA_SerialPinConfig |
CC3200 Serial Pin Configuration. More... | |
struct | I2SCC3200DMA_SerialPinParams |
CC3200 specific I2S Parameters. More... | |
struct | I2SCC3200DMA_SerialPinVars |
I2SCC3200DMA Serial pin variables. More... | |
struct | I2SCC3200DMA_Object |
I2SCC3200DMA Object. More... | |
Macros | |
#define | I2SCC3200DMA_SET_ZEROBUF_LEN I2S_CMD_RESERVED + 0 |
#define | I2SCC3200DMA_SET_EMPTYBUF_LEN I2S_CMD_RESERVED + 1 |
#define | I2SCC3200DMA_INDEX_INVALID 0xFF |
#define | I2SCC3200DMA_NUM_SERIAL_PINS 2 |
Typedefs | |
typedef enum I2SCC3200DMA_DataSize | I2SCC3200DMA_DataSize |
I2SCC3200DMA data size is used to determine how to configure the DMA data transfers. This field is to be only used internally. More... | |
typedef struct I2SCC3200DMA_HWAttrs | I2SCC3200DMA_HWAttrs |
I2SCC3200DMA Hardware attributes. More... | |
typedef struct I2SCC3200DMA_SerialPinConfig | I2SCC3200DMA_SerialPinConfig |
CC3200 Serial Pin Configuration. More... | |
typedef struct I2SCC3200DMA_SerialPinParams | I2SCC3200DMA_SerialPinParams |
CC3200 specific I2S Parameters. More... | |
typedef struct I2SCC3200DMA_SerialPinVars | I2SCC3200DMA_SerialPinVars |
I2SCC3200DMA Serial pin variables. More... | |
typedef struct I2SCC3200DMA_Object | I2SCC3200DMA_Object |
I2SCC3200DMA Object. More... | |
typedef struct I2SCC3200DMA_Object * | I2SCC3200DMA_Handle |
Enumerations | |
enum | I2SCC3200DMA_DataSize { I2SCC3200DMA_16bit = 0, I2SCC3200DMA_32bit = 1 } |
I2SCC3200DMA data size is used to determine how to configure the DMA data transfers. This field is to be only used internally. More... | |
Functions | |
void | I2SCC3200DMA_Params_init (I2SCC3200DMA_SerialPinParams *params) |
Function to initialize the I2S_Params struct to its defaults. More... | |
Variables | |
const I2S_FxnTable | I2SCC3200DMA_fxnTable |
unsigned short | I2SCC3200DMA_zeroBuffer [32] |
I2S_BufDesc | I2SCC3200DMA_zeroBufDesc |
unsigned char | I2SCC3200DMA_emptyBuffer [32] |
I2S_BufDesc | I2SCC3200DMA_emptyBufDesc |
#define I2SCC3200DMA_SET_ZEROBUF_LEN I2S_CMD_RESERVED + 0 |
#define I2SCC3200DMA_SET_EMPTYBUF_LEN I2S_CMD_RESERVED + 1 |
#define I2SCC3200DMA_INDEX_INVALID 0xFF |
#define I2SCC3200DMA_NUM_SERIAL_PINS 2 |
typedef enum I2SCC3200DMA_DataSize I2SCC3200DMA_DataSize |
I2SCC3200DMA data size is used to determine how to configure the DMA data transfers. This field is to be only used internally.
I2SCC3200DMA_16bit: txBuf and rxBuf are arrays of uint16_t elements I2SCC3200DMA_32bit: txBuf and rxBuf are arrays of uint32_t elements
typedef struct I2SCC3200DMA_HWAttrs I2SCC3200DMA_HWAttrs |
I2SCC3200DMA Hardware attributes.
These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For CC3200Ware these definitions are found in:
A sample structure is shown below:
typedef struct I2SCC3200DMA_SerialPinConfig I2SCC3200DMA_SerialPinConfig |
CC3200 Serial Pin Configuration.
typedef struct I2SCC3200DMA_SerialPinParams I2SCC3200DMA_SerialPinParams |
CC3200 specific I2S Parameters.
typedef struct I2SCC3200DMA_SerialPinVars I2SCC3200DMA_SerialPinVars |
I2SCC3200DMA Serial pin variables.
The application must not access any member variables of this structure!
typedef struct I2SCC3200DMA_Object I2SCC3200DMA_Object |
I2SCC3200DMA Object.
The application must not access any member variables of this structure!
typedef struct I2SCC3200DMA_Object * I2SCC3200DMA_Handle |
I2SCC3200DMA data size is used to determine how to configure the DMA data transfers. This field is to be only used internally.
I2SCC3200DMA_16bit: txBuf and rxBuf are arrays of uint16_t elements I2SCC3200DMA_32bit: txBuf and rxBuf are arrays of uint32_t elements
Enumerator | |
---|---|
I2SCC3200DMA_16bit | |
I2SCC3200DMA_32bit |
void I2SCC3200DMA_Params_init | ( | I2SCC3200DMA_SerialPinParams * | params | ) |
Function to initialize the I2S_Params struct to its defaults.
params->serialPinConfig[0].pinNumber = 0; params->serialPinConfig[0].pinMode = I2S_PINMODE_RX; params->serialPinConfig[0].inActiveConfig = I2S_SERCONFIG_INACT_LOW_LEVEL;
params->serialPinConfig[1].pinNumber = 1; params->serialPinConfig[1].pinMode = I2S_PINMODE_TX; params->serialPinConfig[1].inActiveConfig = I2S_SERCONFIG_INACT_LOW_LEVEL;
params | Parameter structure to initialize |
const I2S_FxnTable I2SCC3200DMA_fxnTable |
unsigned short I2SCC3200DMA_zeroBuffer[32] |
I2S_BufDesc I2SCC3200DMA_zeroBufDesc |
unsigned char I2SCC3200DMA_emptyBuffer[32] |
I2S_BufDesc I2SCC3200DMA_emptyBufDesc |