module ti.sysbios.family.arm.a15.smp.Core

Core Identification Module

C synopsis target-domain sourced in ti/sysbios/family/arm/a15/smp/Core.xdc
 
config Core_numCores  // module-wide

number of Cores in SMP environment

C synopsis target-domain
extern const UInt Core_numCores;
 
 
config Core_resetSection  // module-wide

Section to place the reset function

C synopsis target-domain
extern const String Core_resetSection;
 
DETAILS
This configuration parameter allows the app to specify a named output section that will contain the SYS/BIOS core reset function. The core reset function is different from _c_int00 and internally calls _c_int00.
If resetSection is null (or undefined) the reset function is placed in the target's default text section.
 
config Core_useSkernelCmd  // module-wide

Use sKernel command to wake-up cores on Keystone2 devices

C synopsis target-domain
extern const Bool Core_useSkernelCmd;
 
DETAILS
This config param only has an effect when building apps for Keystone2 devices. It is ignored for all other devices like OMAP5xxx, DRA7xx, etc.
If set to true, this config param will cause SYS/BIOS to use sKernel commands to wake-up cores. This param is true by default.
If debugging using CCS, a gel script can be used to wake-up all cores instead of using sKernel commands at runtime. This config param can be disabled in this case.
Note: If debugging using CCS and using a gel script to wake-up all cores, the application needs to be loaded on only one of the cores. Only the app symbols need to be loaded on all other cores.
 
Core_getId()  // module-wide

return the current core id

C synopsis target-domain
UInt Core_getId();
 
 
Core_hwiEnable()  // module-wide

Locally enable interrupts

C synopsis target-domain
macro UInt Core_hwiEnable();
 
RETURNS
opaque key for use by Hwi_restore() or Core_hwiRestore()
DETAILS
Core_hwiEnable locally enables hardware interrupts on the current Core and returns an opaque key indicating whether interrupts were enabled or disabled on entry to Core_hwiEnable().
The actual value of the key is target/device specific and is meant to be passed to Hwi_restore() or Core_hwiRestore().
 
Core_interruptCore()  // module-wide

Cause an interrupt on a particular core

C synopsis target-domain
Void Core_interruptCore(UInt coreId);
 
 
Core_lock()  // module-wide

acquire Inter-core lock

C synopsis target-domain
Void Core_lock();
 
CONSTRAINTS
This function should always be called with interrupts disabled.
 
Core_unlock()  // module-wide

release Inter-core lock

C synopsis target-domain
Void Core_unlock();
 
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId Core_Module_id();
// Get this module's unique id
 
Bool Core_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle Core_Module_heap();
// The heap from which this module allocates memory
 
Bool Core_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 Core_Module_getMask();
// Returns the diagnostics mask for this module
 
Void Core_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
 
Configuration settings sourced in ti/sysbios/family/arm/a15/smp/Core.xdc
var Core = xdc.useModule('ti.sysbios.family.arm.a15.smp.Core');
module-wide config parameters
 
 
 
config Core.numCores  // module-wide

number of Cores in SMP environment

Configuration settings
Core.numCores = UInt undefined;
 
C SYNOPSIS
 
config Core.resetSection  // module-wide

Section to place the reset function

Configuration settings
Core.resetSection = String null;
 
DETAILS
This configuration parameter allows the app to specify a named output section that will contain the SYS/BIOS core reset function. The core reset function is different from _c_int00 and internally calls _c_int00.
If resetSection is null (or undefined) the reset function is placed in the target's default text section.
C SYNOPSIS
 
config Core.useSkernelCmd  // module-wide

Use sKernel command to wake-up cores on Keystone2 devices

Configuration settings
Core.useSkernelCmd = Bool true;
 
DETAILS
This config param only has an effect when building apps for Keystone2 devices. It is ignored for all other devices like OMAP5xxx, DRA7xx, etc.
If set to true, this config param will cause SYS/BIOS to use sKernel commands to wake-up cores. This param is true by default.
If debugging using CCS, a gel script can be used to wake-up all cores instead of using sKernel commands at runtime. This config param can be disabled in this case.
Note: If debugging using CCS and using a gel script to wake-up all cores, the application needs to be loaded on only one of the cores. Only the app symbols need to be loaded on all other cores.
C SYNOPSIS
 
metaonly config Core.common$  // module-wide

Common module configuration parameters

Configuration settings
Core.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
generated on Thu, 08 Jan 2015 01:47:22 GMT