module ti.sysbios.family.arm.m3.Hwi

Cortex M3 Hardware Interrupt Manager

The Cortex M3's Nested Vectored Interrupt Controller (NVIC) supports 256 interrupts/exceptions. [ more ... ]
C synopsis target-domain sourced in ti/sysbios/family/arm/m3/Hwi.xdc
#include <ti/sysbios/family/arm/m3/Hwi.h>
Functions
Void
Void
Void
Void 
Void
Void 
Void 
Functions common to all IHwi modules
Void 
UInt 
UInt 
UInt 
UInt 
Ptr 
Void 
Void 
Void 
Void 
Void 
Functions common to all target instances
Functions common to all target modules
Typedefs
typedef struct
typedef struct
typedef Void 
typedef Void 
typedef Hwi_Object *
typedef struct
typedef UArg 
typedef enum
typedef struct
typedef struct
typedef struct
typedef struct
typedef Void 
Constants
extern const Assert_Id 
extern const UInt 
extern const Bool 
extern const Bool 
extern const Bool 
extern const Bool 
extern const Error_Id 
extern const Error_Id 
extern const Error_Id 
extern const Error_Id 
extern const Error_Id 
extern const Error_Id 
extern const Error_Id 
extern const Error_Id 
extern const Error_Id 
extern const Error_Id 
extern const Error_Id 
extern const Log_Event 
extern const Log_Event 
extern const Int 
extern const Int 
extern const UInt 
 
DETAILS
The Cortex M3's Nested Vectored Interrupt Controller (NVIC) supports 256 interrupts/exceptions.
SYS/BIOS Interrupt IDs or interrupt numbers correspond to an interrupt's position in the interrupt vector table.
ID 0 corresponds to vector 0 which is used by the NVIC to hold the initial (reset) stack pointer value.
IDs 1-14 are hardwired to exceptions.
ID 15 is the SysTick timer interrupt.
ID's 16-255 are mapped to the NVIC's user interrupts 0-239 which are tied to platform specific interrupt sources.
The M3 Hwi module supports "zero latency" interrupts. Interrupts configured with priority greater (in priority, lower in number) than disablePriority are NOT disabled by disable.
Zero latency interrupts are not handled by SYS/BIOS's interrupt dispatcher. Instead, they are vectored to directly. As such, and because they are not masked by disable, these interrupt handlers are severely restricted in terms of the SYS/BIOS APIs they can invoke and THREAD SAFETY MUST BE CAREFULLY CONSIDERED!
Due to the M3's native automatic stacking of saved-by-caller C context on the way to an ISR, zero latency interrupt handlers are implemented using regular C functions (ie no 'interrupt' keyword is required).
Zero latency interrupts are distinguished from regular dispatched interrupts at create time by their priority being greater than disablePriority.
Note that since zero latency interrupts don't use the dispatcher, the arg parameter is not functional.
RESTRICTIONS
When used within a dual M3 core (Ducati) arrangement, care must be taken when initializing this shared resource. The "Shared Resources" note provided in the ducati package discusses the management of the various hardware and software resources shared by the two M3 cores.
By default, core 0 places its runtime vector table at 0x400 and core 1 places its runtime vector table at 0x800. This placement is made automatically when the ti.sysbios.family.arm.ducati.Core module is used. This default behavior can be overridden by explicitly setting the Hwi.resetVectorAddress and Hwi.vectorTableAddress config parameters.

Calling Context

Function Hwi Swi Task Main Startup
clearInterrupt Y Y Y Y Y
create N N Y Y N
disable Y Y Y Y Y
disableInterrupt Y Y Y Y N
enable Y Y Y N N
enableInterrupt Y Y Y Y N
Params_init Y Y Y Y Y
restore Y Y Y Y Y
restoreInterrupt Y Y Y Y Y
construct N N Y Y N
delete N N Y Y N
destruct N N Y Y N
getHookContext Y Y Y Y N
setFunc Y Y Y Y N
setHookContext Y Y Y Y N
Definitions:
  • Hwi: API is callable from a Hwi thread.
  • Swi: API is callable from a Swi thread.
  • Task: API is callable from a Task thread.
  • Main: API is callable during any of these phases:
    • In your module startup after this module is started (e.g. Hwi_Module_startupDone() returns TRUE).
    • During xdc.runtime.Startup.lastFxns.
    • During main().
    • During BIOS.startupFxns.
  • Startup: API is callable during any of these phases:
    • During xdc.runtime.Startup.firstFxns.
    • In your module startup before this module is started (e.g. Hwi_Module_startupDone() returns FALSE).
enum Hwi_MaskingOption

Shorthand interrupt masking options

C synopsis target-domain
typedef enum Hwi_MaskingOption {
    Hwi_MaskingOption_NONE,
    // No interrupts are disabled
    Hwi_MaskingOption_ALL,
    // All interrupts are disabled
    Hwi_MaskingOption_SELF,
    // Only this interrupt is disabled
    Hwi_MaskingOption_BITMASK,
    // User supplies IER masks
    Hwi_MaskingOption_LOWER
    // All current and lower priority interrupts are disabled. Only a few targets/devices truly support this masking option. For those that don't, this setting is treated the same as MaskingOption_SELF
} Hwi_MaskingOption;
typedef Hwi_ExceptionHookFuncPtr

Exception hook function type definition

C synopsis target-domain
typedef Void (*Hwi_ExceptionHookFuncPtr)(Hwi_ExcContext*);
typedef Hwi_FuncPtr

Hwi create function type definition

C synopsis target-domain
typedef Void (*Hwi_FuncPtr)(UArg);
typedef Hwi_Irp

Interrupt Return Pointer. This is the address of the interrupted instruction

C synopsis target-domain
typedef UArg Hwi_Irp;
typedef Hwi_VectorFuncPtr

Hwi vector function type definition

C synopsis target-domain
typedef Void (*Hwi_VectorFuncPtr)(Void);
struct Hwi_CCR

NVIC Configuration Control Register (CCR)

C synopsis target-domain
typedef struct Hwi_CCR {
    Bits8 STKALIGN;
    // Auto stack alignment in exception
    Bits8 BFHFNMIGN;
    // All faults ignore BUS Faults
    Bits8 DIV_0_TRP;
    // Trap on divige be zero
    Bits8 UNALIGN_TRP;
    // Trap on all unaligned accesses
    Bits8 USERSETMPEND;
    // Allow user to trigger interrupts
    Bits8 NONEBASETHRDENA;
    // Allow entering thread mode anytime
} Hwi_CCR;
struct Hwi_ExcContext

Exception Context - Register contents at the time of an exception

C synopsis target-domain
typedef struct Hwi_ExcContext {
    BIOS_ThreadType threadType;
    Ptr threadHandle;
    Ptr threadStack;
    SizeT threadStackSize;
    Ptr r0;
    Ptr r1;
    Ptr r2;
    Ptr r3;
    Ptr r4;
    Ptr r5;
    Ptr r6;
    Ptr r7;
    Ptr r8;
    Ptr r9;
    Ptr r10;
    Ptr r11;
    Ptr r12;
    Ptr sp;
    Ptr lr;
    Ptr pc;
    Ptr psr;
    Ptr ICSR;
    Ptr MMFSR;
    Ptr BFSR;
    Ptr UFSR;
    Ptr HFSR;
    Ptr DFSR;
    Ptr MMAR;
    Ptr BFAR;
    Ptr AFSR;
} Hwi_ExcContext;
struct Hwi_HookSet

Hwi hook set type definition

C synopsis target-domain
typedef struct Hwi_HookSet {
    Void (*registerFxn)(Int);
    Void (*createFxn)(IHwi_Handle,Error_Block*);
    Void (*beginFxn)(IHwi_Handle);
    Void (*endFxn)(IHwi_Handle);
    Void (*deleteFxn)(IHwi_Handle);
} Hwi_HookSet;
DETAILS
The functions that make up a hookSet have certain restrictions. They cannot call any Hwi instance functions other than Hwi_getHookContext() and Hwi_setHookContext(). For all practical purposes, they should treat the Hwi_Handle passed to these functions as an opaque handle.
struct Hwi_NVIC

Nested Vectored Interrupt Controller

C synopsis target-domain
typedef struct Hwi_NVIC {
    UInt32 RES_00;
    // 0xE000E000 reserved
    UInt32 ICTR;
    // 0xE000E004 Interrupt Control Type
    UInt32 RES_08;
    // 0xE000E008 reserved
    UInt32 RES_0C;
    // 0xE000E00C reserved
    UInt32 STCSR;
    // 0xE000E010 SysTick Control & Status Register
    UInt32 STRVR;
    // 0xE000E014 SysTick Reload Value Register
    UInt32 STCVR;
    // 0xE000E018 SysTick Current Value Register
    UInt32 STCALIB;
    // 0xE000E01C SysTick Calibration Value Register
    UInt32 RES_20[56];
    // 0xE000E020-0xE000E0FC reserved
    UInt32 ISER[8];
    // 0xE000E100-0xE000E11C Interrupt Set Enable Registers
    UInt32 RES_120[24];
    // 0xE000E120-0xE000E17C reserved
    UInt32 ICER[8];
    // 0xE000E180-0xE000E19C Interrupt Clear Enable Registers
    UInt32 RES_1A0[24];
    // 0xE000E1A0-0xE000E1FC reserved
    UInt32 ISPR[8];
    // 0xE000E200-0xE000E21C Interrupt Set Pending Registers
    UInt32 RES_220[24];
    // 0xE000E220-0xE000E7C reserved
    UInt32 ICPR[8];
    // 0xE000E280-0xE000E29C Interrupt Clear Pending Registers
    UInt32 RES_2A0[24];
    // 0xE000E2A0-0xE000E2FC reserved
    UInt32 IABR[8];
    // 0xE000E300-0xE000E31C Interrupt Active Bit Registers
    UInt32 RES_320[56];
    // 0xE000E320-0xE000E3FC reserved
    UInt8 IPR[240];
    // 0xE000E400-0xE000E4EF Interrupt Priority Registers
    UInt32 RES_4F0[516];
    // 0xE000E4F0-0xE000ECFC reserved
    UInt32 CPUIDBR;
    // 0xE000ED00 CPUID Base Register
    UInt32 ICSR;
    // 0xE000ED04 Interrupt Control State Register
    UInt32 VTOR;
    // 0xE000ED08 Vector Table Offset Register
    UInt32 AIRCR;
    // 0xE000ED0C Application Interrupt/Reset Control Register
    UInt32 SCR;
    // 0xE000ED10 System Control Register
    UInt32 CCR;
    // 0xE000ED14 Configuration Control Register
    UInt8 SHPR[12];
    // 0xE000ED18 System Handlers 4-15 Priority Registers
    UInt32 SHCSR;
    // 0xE000ED24 System Handler Control & State Register
    UInt8 MMFSR;
    // 0xE000ED28 Memory Manage Fault Status Register
    UInt8 BFSR;
    // 0xE000ED29 Bus Fault Status Register
    UInt16 UFSR;
    // 0xE000ED2A Usage Fault Status Register
    UInt32 HFSR;
    // 0xE000ED2C Hard Fault Status Register
    UInt32 DFSR;
    // 0xE000ED30 Debug Fault Status Register
    UInt32 MMAR;
    // 0xE000ED34 Memory Manager Address Register
    UInt32 BFAR;
    // 0xE000ED38 Bus Fault Address Register
    UInt32 AFSR;
    // 0xE000ED3C Auxiliary Fault Status Register
    UInt32 PFR0;
    // 0xE000ED40 Processor Feature Register
    UInt32 PFR1;
    // 0xE000ED44 Processor Feature Register
    UInt32 DFR0;
    // 0xE000ED48 Debug Feature Register
    UInt32 AFR0;
    // 0xE000ED4C Auxiliary Feature Register
    UInt32 MMFR0;
    // 0xE000ED50 Memory Model Fault Register0
    UInt32 MMFR1;
    // 0xE000ED54 Memory Model Fault Register1
    UInt32 MMFR2;
    // 0xE000ED58 Memory Model Fault Register2
    UInt32 MMFR3;
    // 0xE000ED5C Memory Model Fault Register3
    UInt32 ISAR0;
    // 0xE000ED60 ISA Feature Register0
    UInt32 ISAR1;
    // 0xE000ED64 ISA Feature Register1
    UInt32 ISAR2;
    // 0xE000ED68 ISA Feature Register2
    UInt32 ISAR3;
    // 0xE000ED6C ISA Feature Register3
    UInt32 ISAR4;
    // 0xE000ED70 ISA Feature Register4
    UInt32 RES_D74[99];
    // 0xE000ED74-0xE000EEFC reserved
    UInt32 STI;
    // 0xE000EF00 Software Trigger Interrupt Register
    UInt32 PID4;
    // 0xE000EFD0 Peripheral ID Register4
    UInt32 PID5;
    // 0xE000EFD4 Peripheral ID Register5
    UInt32 PID6;
    // 0xE000EFD8 Peripheral ID Register6
    UInt32 PID7;
    // 0xE000EFDC Peripheral ID Register7
    UInt32 PID0;
    // 0xE000EFE0 Peripheral ID Register0
    UInt32 PID1;
    // 0xE000EFE4 Peripheral ID Register1
    UInt32 PID2;
    // 0xE000EFE8 Peripheral ID Register2
    UInt32 PID3;
    // 0xE000EFEC Peripheral ID Register3
    UInt32 CID0;
    // 0xE000EFF0 Component ID Register0
    UInt32 CID1;
    // 0xE000EFF4 Component ID Register1
    UInt32 CID2;
    // 0xE000EFF8 Component ID Register2
    UInt32 CID3;
    // 0xE000EFFC Component ID Register3
} Hwi_NVIC;
config Hwi_NUM_INTERRUPTS  // module-wide

The Cortex M3 NVIC supports up to 256 interrupts/exceptions

C synopsis target-domain
extern const Int Hwi_NUM_INTERRUPTS;
DETAILS
The actual number supported is device specific and provided by the catalog device specification.
config Hwi_NUM_PRIORITIES  // module-wide

The Cortex M3 NVIC supports up to 256 interrupt priorities

C synopsis target-domain
extern const Int Hwi_NUM_PRIORITIES;
DETAILS
The actual number supported is device specific and provided by the catalog device specification.
config Hwi_A_unsupportedMaskingOption  // module-wide

Assert when bad maskSetting parameter provided

C synopsis target-domain
extern const Assert_Id Hwi_A_unsupportedMaskingOption;
config Hwi_E_NMI  // module-wide

Error raised when NMI exception occurs

C synopsis target-domain
extern const Error_Id Hwi_E_NMI;
config Hwi_E_alreadyDefined  // module-wide

Error raised when Hwi is already defined

C synopsis target-domain
extern const Error_Id Hwi_E_alreadyDefined;
config Hwi_E_busFault  // module-wide

Error raised when bus fault exception occurs

C synopsis target-domain
extern const Error_Id Hwi_E_busFault;
config Hwi_E_debugMon  // module-wide

Error raised when debugMon exception occurs

C synopsis target-domain
extern const Error_Id Hwi_E_debugMon;
config Hwi_E_exception  // module-wide

Error raised when an exception occurs

C synopsis target-domain
extern const Error_Id Hwi_E_exception;
config Hwi_E_hardFault  // module-wide

Error raised when hard fault exception occurs

C synopsis target-domain
extern const Error_Id Hwi_E_hardFault;
config Hwi_E_memFault  // module-wide

Error raised when memory fault exception occurs

C synopsis target-domain
extern const Error_Id Hwi_E_memFault;
config Hwi_E_noIsr  // module-wide

Error raised when an uninitialized interrupt occurs

C synopsis target-domain
extern const Error_Id Hwi_E_noIsr;
config Hwi_E_reserved  // module-wide

Error raised when reserved exception occurs

C synopsis target-domain
extern const Error_Id Hwi_E_reserved;
config Hwi_E_svCall  // module-wide

Error raised when svCall exception occurs

C synopsis target-domain
extern const Error_Id Hwi_E_svCall;
config Hwi_E_usageFault  // module-wide

Error raised when usage fault exception occurs

C synopsis target-domain
extern const Error_Id Hwi_E_usageFault;
config Hwi_LD_end  // module-wide

Issued just after return from Hwi function (with interrupts disabled)

C synopsis target-domain
extern const Log_Event Hwi_LD_end;
config Hwi_LM_begin  // module-wide

Issued just prior to Hwi function invocation (with interrupts disabled)

C synopsis target-domain
extern const Log_Event Hwi_LM_begin;
config Hwi_disablePriority  // module-wide

The priority that BASEPRI is set to by Hwi_disable()

C synopsis target-domain
extern const UInt Hwi_disablePriority;
DETAILS
All interrupts configured with equal or less priority (equal or higher number) than disablePriority are disabled by Hwi_disable. Interrupts configured with higher priority (smaller number) than disablePriority are non-maskable (ie zero-latency).
The default setting is the second highest interrupt priority defined for the device. This results in priority 0 (and all other values in the same priority group) being the non-maskable interrupt priority. All other priorities are disabled with Hwi_disable().
config Hwi_dispatcherAutoNestingSupport  // module-wide

Include interrupt nesting logic in interrupt dispatcher?

C synopsis target-domain
extern const Bool Hwi_dispatcherAutoNestingSupport;
DETAILS
Default is true.
This option provides the user with the ability to optimize interrupt dispatcher performance when support for interrupt nesting is not required.
Setting this parameter to false will disable the logic in the interrupt dispatcher that manipulates interrupt mask registers and enables and disables interrupts before and after invoking the user's Hwi function.
Set this parameter to false if you don't need interrupts enabled during the execution of your Hwi functions.
config Hwi_dispatcherIrpTrackingSupport  // module-wide

Controls whether the dispatcher retains the interrupted thread's return address

C synopsis target-domain
extern const Bool Hwi_dispatcherIrpTrackingSupport;
DETAILS
This option is enabled by default.
Setting this parameter to false will disable the logic in the interrupt dispatcher that keeps track of the interrupt's return address and provide a small savings in interrupt latency.
The application can get an interrupt's most recent return address using the getIrp API.
config Hwi_dispatcherSwiSupport  // module-wide

Include Swi scheduling logic in interrupt dispatcher?

C synopsis target-domain
extern const Bool Hwi_dispatcherSwiSupport;
DETAILS
Default is inherited from BIOS.swiEnabled, which is true by default.
This option provides the user with the ability to optimize interrupt dispatcher performance when it is known that Swis will not be posted from any of their Hwi threads.
Setting this parameter to false will disable the logic in the interrupt dispatcher that invokes the Swi scheduler prior to returning from an interrupt.
config Hwi_dispatcherTaskSupport  // module-wide

Include Task scheduling logic in interrupt dispatcher?

C synopsis target-domain
extern const Bool Hwi_dispatcherTaskSupport;
DETAILS
Default is inherited from BIOS.taskEnabled, which is true by default.
This option provides the user with the ability to optimize interrupt dispatcher performance when it is known that no Task scheduling APIs (ie Semaphore_post()) will be executed from any of their Hwi threads.
Setting this parameter to false will disable the logic in the interrupt dispatcher that invokes the Task scheduler prior to returning from an interrupt.
config Hwi_excHookFunc  // module-wide

User Exception hook function

C synopsis target-domain
extern const Hwi_ExceptionHookFuncPtr Hwi_excHookFunc;
DETAILS
Called just after the exception context has been initialized.
This function will be run on the ISR stack.
This function must run to completion.
It is called without any Task or Swi scheduling protection and therefore can not call any functions that may cause a Swi or Task scheduling operation (Swi_post(), Semaphore_post(), Event_post(), etc).
config Hwi_priGroup  // module-wide

The PRIGROUP setting. Default is 0

C synopsis target-domain
extern const UInt Hwi_priGroup;
DETAILS
This value will be written to the PRIGROUP field within the NVIC's Application Interrupt and Reset Control Register (Hwi_nvic.AIRCR). It defines how the 8 bit priority values are interpreted by the hardware.
Valid settings are 0-7.
The default setting of 0 causes bits 7-1 of an interrupt's priority value to be used to as a pre-emption priority, and bit 0 is used to determine which of two simultaneous interrupts with the same pre-emption priority will be serviced first.
Hwi_clearInterrupt()  // module-wide

Clear a specific interrupt

C synopsis target-domain
Void Hwi_clearInterrupt(UInt intNum);
ARGUMENTS
intNum — interrupt number to clear
DETAILS
Clears a specific interrupt's pending status. The implementation is family-specific.
Hwi_disable()  // module-wide

Globally disable interrupts

C synopsis target-domain
UInt Hwi_disable();
RETURNS
opaque key for use by Hwi_restore()
DETAILS
Hwi_disable globally disables hardware interrupts and returns an opaque key indicating whether interrupts were globally enabled or disabled on entry to Hwi_disable(). The actual value of the key is target/device specific and is meant to be passed to Hwi_restore().
Call Hwi_disable before a portion of a function that needs to run without interruption. When critical processing is complete, call Hwi_restore or Hwi_enable to reenable hardware interrupts.
Servicing of interrupts that occur while interrupts are disabled is postponed until interrupts are reenabled. However, if the same type of interrupt occurs several times while interrupts are disabled, the interrupt's function is executed only once when interrupts are reenabled.
A context switch can occur when calling Hwi_enable or Hwi_restore if an enabled interrupt occurred while interrupts are disabled.
Hwi_disable may be called from main(). However, since Hwi interrupts are already disabled in main(), such a call has no effect.
CONSTRAINTS
If a Task switching API such as Semaphore_pend(), Semaphore_post(), Task_sleep(), or Task_yield() is invoked which results in a context switch while interrupts are disabled, an embedded call to Hwi_enable occurs on the way to the new thread context which unconditionally re-enables interrupts. Interrupts will remain enabled until a subsequent Hwi_disable invocation.
Swis always run with interrupts enabled. See Swi_post() for a discussion Swis and interrupts.
Hwi_disableInterrupt()  // module-wide

Disable a specific interrupt

C synopsis target-domain
UInt Hwi_disableInterrupt(UInt intNum);
ARGUMENTS
intNum — interrupt number to disable
RETURNS
key to restore previous enable/disable state
DETAILS
Disable a specific interrupt identified by an interrupt number.
Hwi_enable()  // module-wide

Globally enable interrupts

C synopsis target-domain
UInt Hwi_enable();
RETURNS
opaque key for use by Hwi_restore()
DETAILS
Hwi_enable globally enables hardware interrupts and returns an opaque key indicating whether interrupts were globally enabled or disabled on entry to Hwi_enable(). The actual value of the key is target/device specific and is meant to be passed to Hwi_restore().
This function is called as part of SYS/BIOS Startup_POST_APP_MAIN phase.
Hardware interrupts are enabled unless a call to Hwi_disable disables them.
Servicing of interrupts that occur while interrupts are disabled is postponed until interrupts are reenabled. However, if the same type of interrupt occurs several times while interrupts are disabled, the interrupt's function is executed only once when interrupts are reenabled.
A context switch can occur when calling Hwi_enable or Hwi_restore if an enabled interrupt occurred while interrupts are disabled.
Any call to Hwi_enable enables interrupts, even if Hwi_disable has been called several times.
Hwi_enable must not be called from main().
Hwi_enableInterrupt()  // module-wide

Enable a specific interrupt

C synopsis target-domain
UInt Hwi_enableInterrupt(UInt intNum);
ARGUMENTS
intNum — interrupt number to enable
RETURNS
key to restore previous enable/disable state
DETAILS
Enables a specific interrupt identified by an interrupt number.
Hwi_excSetBuffers()  // module-wide

Set the exception context and stack buffer pointers

C synopsis target-domain
Void Hwi_excSetBuffers(Ptr excContextBuffer, Ptr excStackBuffer);
ARGUMENTS
excContextBuffer — Address to place ExcContext
excStackBuffer — Address to place ExcStack
Hwi_getHandle()  // module-wide

Returns Hwi_handle associated with intNum

C synopsis target-domain
Hwi_Handle Hwi_getHandle(UInt intNum);
ARGUMENTS
intNum — interrupt number
Hwi_restore()  // module-wide

Globally restore interrupts

C synopsis target-domain
Void Hwi_restore(UInt key);
ARGUMENTS
key — enable/disable state to restore
DETAILS
Hwi_restore globally restores interrupts to the state determined by the key argument provided by a previous invocation of Hwi_disable.
A context switch may occur when calling Hwi_restore if Hwi_restore reenables interrupts and another Hwi occurred while interrupts were disabled.
Hwi_restore may be called from main(). However, since Hwi_enable cannot be called from main(), interrupts are always disabled in main(), and a call to Hwi_restore has no effect.
Hwi_restoreInterrupt()  // module-wide

Restore a specific interrupt's enabled/disabled state

C synopsis target-domain
Void Hwi_restoreInterrupt(UInt intNum, UInt key);
ARGUMENTS
intNum — interrupt number to restore
key — key returned from enableInt or disableInt
DETAILS
Restores a specific interrupt identified by an interrupt number. restoreInterrupt is generally used to restore an interrupt to its state before disableInterrupt or enableInterrupt was invoked
Hwi_setPriority()  // module-wide

Set an interrupt's relative priority

C synopsis target-domain
Void Hwi_setPriority(UInt intNum, UInt priority);
ARGUMENTS
intNum — ID of interrupt
priority — priority
DETAILS
Valid priorities are 0 - 255. 0 is highest priority.
Hwi_startup()  // module-wide

Initially enable interrupts

C synopsis target-domain
Void Hwi_startup();
DETAILS
Called within BIOS_start
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId Hwi_Module_id();
// Get this module's unique id
 
Bool Hwi_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle Hwi_Module_heap();
// The heap from which this module allocates memory
 
Bool Hwi_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 Hwi_Module_getMask();
// Returns the diagnostics mask for this module
 
Void Hwi_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types

C synopsis target-domain
typedef struct Hwi_Object Hwi_Object;
// Opaque internal representation of an instance object
 
typedef Hwi_Object *Hwi_Handle;
// Client reference to an instance object
 
typedef struct Hwi_Struct Hwi_Struct;
// Opaque client structure large enough to hold an instance object
 
Hwi_Handle Hwi_handle(Hwi_Struct *structP);
// Convert this instance structure pointer into an instance handle
 
Hwi_Struct *Hwi_struct(Hwi_Handle handle);
// Convert this instance handle into an instance structure pointer
Instance Config Parameters

C synopsis target-domain
typedef struct Hwi_Params {
// Instance config-params structure
    IInstance_Params *instance;
    // Common per-instance configs
    UArg arg;
    // ISR function argument. Default is 0
    Bool enableInt;
    // Enable this interrupt now? Default is true
    Int eventId;
    // Interrupt event ID (Interrupt Selection Number) Default is -1. Not all targets/devices support this instance parameter. On those that don't, this parameter is ignored
    IHwi_MaskingOption maskSetting;
    // The interrupt controller is designed for priority based interrupts
    Int priority;
    // Interrupt priority. Valid priorities are 0 - 255. 0 is the highest priority. The default is 255 which is the lowest priority interrupt
} Hwi_Params;
 
Void Hwi_Params_init(Hwi_Params *params);
// Initialize this config-params structure with supplier-specified defaults before instance creation
config Hwi_arg  // instance

ISR function argument. Default is 0

C synopsis target-domain
struct Hwi_Params {
      ...
    UArg arg;
config Hwi_enableInt  // instance

Enable this interrupt now? Default is true

C synopsis target-domain
struct Hwi_Params {
      ...
    Bool enableInt;
config Hwi_eventId  // instance

Interrupt event ID (Interrupt Selection Number) Default is -1. Not all targets/devices support this instance parameter. On those that don't, this parameter is ignored

C synopsis target-domain
struct Hwi_Params {
      ...
    Int eventId;
config Hwi_maskSetting  // instance

The interrupt controller is designed for priority based interrupts

C synopsis target-domain
struct Hwi_Params {
      ...
    IHwi_MaskingOption maskSetting;
config Hwi_priority  // instance

Interrupt priority. Valid priorities are 0 - 255. 0 is the highest priority. The default is 255 which is the lowest priority interrupt

C synopsis target-domain
struct Hwi_Params {
      ...
    Int priority;
Instance Creation

C synopsis target-domain
Hwi_Handle Hwi_create(Int intNum, IHwi_FuncPtr hwiFxn, const Hwi_Params *params, Error_Block *eb);
// Allocate and initialize a new instance object and return its handle
 
Void Hwi_construct(Hwi_Struct *structP, Int intNum, IHwi_FuncPtr hwiFxn, const Hwi_Params *params, Error_Block *eb);
// Initialize a new instance object inside the provided structure
ARGUMENTS
intNum — interrupt number
hwiFxn — pointer to ISR function
params — per-instance config params, or NULL to select default values (target-domain only)
eb — active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
A Hwi dispatcher table entry is created and filled with the function specified by the fxn parameter and the attributes specified by the params parameter.
If params is NULL, the Hwi's dispatcher properties are assigned a default set of values. Otherwise, the following properties are specified by a structure of type Hwi_Params.
  • The arg element is a generic argument that is passed to the plugged function as its only parameter. The default value is 0.
  • The enableInt element determines whether the interrupt should be enabled in the IER by create.
  • The maskSetting element defines the dispatcherAutoNestingSupport behavior of the interrupt.
Hwi_create returns a pointer to the created Hwi object.
Instance Deletion

C synopsis target-domain
Void Hwi_delete(Hwi_Handle *handleP);
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
 
Void Hwi_destruct(Hwi_Struct *structP);
// Finalize the instance object inside the provided structure
Hwi_getFunc()  // instance

Get Hwi function and arg

C synopsis target-domain
IHwi_FuncPtr Hwi_getFunc(Hwi_Handle handle, UArg *arg);
ARGUMENTS
handle — handle of a previously-created Hwi instance object
arg — pointer for returning hwi's ISR function argument
RETURNS
hwi's ISR function
Hwi_getHookContext()  // instance

Get hook instance's context for a Hwi

C synopsis target-domain
Ptr Hwi_getHookContext(Hwi_Handle handle, Int id);
ARGUMENTS
handle — handle of a previously-created Hwi instance object
RETURNS
hook instance's context for hwi
Hwi_getIrp()  // instance

Get address of interrupted instruction

C synopsis target-domain
IHwi_Irp Hwi_getIrp(Hwi_Handle handle);
ARGUMENTS
handle — handle of a previously-created Hwi instance object
RETURNS
most current IRP of a Hwi
Hwi_reconfig()  // instance

Reconfigure a dispatched interrupt

C synopsis target-domain
Void Hwi_reconfig(Hwi_Handle handle, Hwi_FuncPtr fxn, Hwi_Params *params);
ARGUMENTS
handle — handle of a previously-created Hwi instance object
Hwi_setFunc()  // instance

Overwrite Hwi function and arg

C synopsis target-domain
Void Hwi_setFunc(Hwi_Handle handle, IHwi_FuncPtr fxn, UArg arg);
ARGUMENTS
handle — handle of a previously-created Hwi instance object
fxn — pointer to ISR function
arg — argument to ISR function
DETAILS
Replaces a Hwi object's hwiFxn function originally provided in create.
Hwi_setHookContext()  // instance

Set hook instance's context for a Hwi

C synopsis target-domain
Void Hwi_setHookContext(Hwi_Handle handle, Int id, Ptr hookContext);
ARGUMENTS
handle — handle of a previously-created Hwi instance object
id — hook instance's ID
hookContext — value to write to context
Instance Convertors

C synopsis target-domain
IHwi_Handle Hwi_Handle_upCast(Hwi_Handle handle);
// unconditionally move one level up the inheritance hierarchy
 
Hwi_Handle Hwi_Handle_downCast(IHwi_Handle handle);
// conditionally move one level down the inheritance hierarchy; NULL upon failure
Instance Built-Ins

C synopsis target-domain
Int Hwi_Object_count();
// The number of statically-created instance objects
 
Hwi_Handle Hwi_Object_get(Hwi_Object *array, Int i);
// The handle of the i-th statically-created instance object (array == NULL)
 
Hwi_Handle Hwi_Object_first();
// The handle of the first dynamically-created instance object, or NULL
 
Hwi_Handle Hwi_Object_next(Hwi_Handle handle);
// The handle of the next dynamically-created instance object, or NULL
 
IHeap_Handle Hwi_Object_heap();
// The heap used to allocate dynamically-created instance objects
 
Types_Label *Hwi_Handle_label(Hwi_Handle handle, Types_Label *buf);
// The label associated with this instance object
 
String Hwi_Handle_name(Hwi_Handle handle);
// The name of this instance object
 
XDCscript usage meta-domain sourced in ti/sysbios/family/arm/m3/Hwi.xdc
var Hwi = xdc.useModule('ti.sysbios.family.arm.m3.Hwi');
module-wide constants & types
        obj.STKALIGN// Auto stack alignment in exception = Bits8  ...
        obj.BFHFNMIGN// All faults ignore BUS Faults = Bits8  ...
        obj.DIV_0_TRP// Trap on divige be zero = Bits8  ...
        obj.UNALIGN_TRP// Trap on all unaligned accesses = Bits8  ...
        obj.USERSETMPEND// Allow user to trigger interrupts = Bits8  ...
        obj.NONEBASETHRDENA// Allow entering thread mode anytime = Bits8  ...
        obj.threadType = BIOS.ThreadType  ...
        obj.threadHandle = Ptr  ...
        obj.threadStack = Ptr  ...
        obj.threadStackSize = SizeT  ...
        obj.r0 = Ptr  ...
        obj.r1 = Ptr  ...
        obj.r2 = Ptr  ...
        obj.r3 = Ptr  ...
        obj.r4 = Ptr  ...
        obj.r5 = Ptr  ...
        obj.r6 = Ptr  ...
        obj.r7 = Ptr  ...
        obj.r8 = Ptr  ...
        obj.r9 = Ptr  ...
        obj.r10 = Ptr  ...
        obj.r11 = Ptr  ...
        obj.r12 = Ptr  ...
        obj.sp = Ptr  ...
        obj.lr = Ptr  ...
        obj.pc = Ptr  ...
        obj.psr = Ptr  ...
        obj.ICSR = Ptr  ...
        obj.MMFSR = Ptr  ...
        obj.BFSR = Ptr  ...
        obj.UFSR = Ptr  ...
        obj.HFSR = Ptr  ...
        obj.DFSR = Ptr  ...
        obj.MMAR = Ptr  ...
        obj.BFAR = Ptr  ...
        obj.AFSR = Ptr  ...
        obj.registerFxn = Void(*)(Int)  ...
        obj.createFxn = Void(*)(IHwi.Handle,Error.Block*)  ...
        obj.beginFxn = Void(*)(IHwi.Handle)  ...
        obj.endFxn = Void(*)(IHwi.Handle)  ...
        obj.deleteFxn = Void(*)(IHwi.Handle)  ...
        obj.RES_00// 0xE000E000 reserved = UInt32  ...
        obj.ICTR// 0xE000E004 Interrupt Control Type = UInt32  ...
        obj.RES_08// 0xE000E008 reserved = UInt32  ...
        obj.RES_0C// 0xE000E00C reserved = UInt32  ...
        obj.STCSR// 0xE000E010 SysTick Control & Status Register = UInt32  ...
        obj.STRVR// 0xE000E014 SysTick Reload Value Register = UInt32  ...
        obj.STCVR// 0xE000E018 SysTick Current Value Register = UInt32  ...
        obj.STCALIB// 0xE000E01C SysTick Calibration Value Register = UInt32  ...
        obj.RES_20// 0xE000E020-0xE000E0FC reserved = UInt32[56]  ...
        obj.ISER// 0xE000E100-0xE000E11C Interrupt Set Enable Registers = UInt32[8]  ...
        obj.RES_120// 0xE000E120-0xE000E17C reserved = UInt32[24]  ...
        obj.RES_1A0// 0xE000E1A0-0xE000E1FC reserved = UInt32[24]  ...
        obj.ISPR// 0xE000E200-0xE000E21C Interrupt Set Pending Registers = UInt32[8]  ...
        obj.RES_220// 0xE000E220-0xE000E7C reserved = UInt32[24]  ...
        obj.RES_2A0// 0xE000E2A0-0xE000E2FC reserved = UInt32[24]  ...
        obj.IABR// 0xE000E300-0xE000E31C Interrupt Active Bit Registers = UInt32[8]  ...
        obj.RES_320// 0xE000E320-0xE000E3FC reserved = UInt32[56]  ...
        obj.IPR// 0xE000E400-0xE000E4EF Interrupt Priority Registers = UInt8[240]  ...
        obj.RES_4F0// 0xE000E4F0-0xE000ECFC reserved = UInt32[516]  ...
        obj.CPUIDBR// 0xE000ED00 CPUID Base Register = UInt32  ...
        obj.ICSR// 0xE000ED04 Interrupt Control State Register = UInt32  ...
        obj.VTOR// 0xE000ED08 Vector Table Offset Register = UInt32  ...
        obj.SCR// 0xE000ED10 System Control Register = UInt32  ...
        obj.CCR// 0xE000ED14 Configuration Control Register = UInt32  ...
        obj.SHPR// 0xE000ED18 System Handlers 4-15 Priority Registers = UInt8[12]  ...
        obj.MMFSR// 0xE000ED28 Memory Manage Fault Status Register = UInt8  ...
        obj.BFSR// 0xE000ED29 Bus Fault Status Register = UInt8  ...
        obj.UFSR// 0xE000ED2A Usage Fault Status Register = UInt16  ...
        obj.HFSR// 0xE000ED2C Hard Fault Status Register = UInt32  ...
        obj.DFSR// 0xE000ED30 Debug Fault Status Register = UInt32  ...
        obj.MMAR// 0xE000ED34 Memory Manager Address Register = UInt32  ...
        obj.BFAR// 0xE000ED38 Bus Fault Address Register = UInt32  ...
        obj.AFSR// 0xE000ED3C Auxiliary Fault Status Register = UInt32  ...
        obj.PFR0// 0xE000ED40 Processor Feature Register = UInt32  ...
        obj.PFR1// 0xE000ED44 Processor Feature Register = UInt32  ...
        obj.DFR0// 0xE000ED48 Debug Feature Register = UInt32  ...
        obj.AFR0// 0xE000ED4C Auxiliary Feature Register = UInt32  ...
        obj.MMFR0// 0xE000ED50 Memory Model Fault Register0 = UInt32  ...
        obj.MMFR1// 0xE000ED54 Memory Model Fault Register1 = UInt32  ...
        obj.MMFR2// 0xE000ED58 Memory Model Fault Register2 = UInt32  ...
        obj.MMFR3// 0xE000ED5C Memory Model Fault Register3 = UInt32  ...
        obj.ISAR0// 0xE000ED60 ISA Feature Register0 = UInt32  ...
        obj.ISAR1// 0xE000ED64 ISA Feature Register1 = UInt32  ...
        obj.ISAR2// 0xE000ED68 ISA Feature Register2 = UInt32  ...
        obj.ISAR3// 0xE000ED6C ISA Feature Register3 = UInt32  ...
        obj.ISAR4// 0xE000ED70 ISA Feature Register4 = UInt32  ...
        obj.RES_D74// 0xE000ED74-0xE000EEFC reserved = UInt32[99]  ...
        obj.STI// 0xE000EF00 Software Trigger Interrupt Register = UInt32  ...
        obj.PID4// 0xE000EFD0 Peripheral ID Register4 = UInt32  ...
        obj.PID5// 0xE000EFD4 Peripheral ID Register5 = UInt32  ...
        obj.PID6// 0xE000EFD8 Peripheral ID Register6 = UInt32  ...
        obj.PID7// 0xE000EFDC Peripheral ID Register7 = UInt32  ...
        obj.PID0// 0xE000EFE0 Peripheral ID Register0 = UInt32  ...
        obj.PID1// 0xE000EFE4 Peripheral ID Register1 = UInt32  ...
        obj.PID2// 0xE000EFE8 Peripheral ID Register2 = UInt32  ...
        obj.PID3// 0xE000EFEC Peripheral ID Register3 = UInt32  ...
        obj.CID0// 0xE000EFF0 Component ID Register0 = UInt32  ...
        obj.CID1// 0xE000EFF4 Component ID Register1 = UInt32  ...
        obj.CID2// 0xE000EFF8 Component ID Register2 = UInt32  ...
        obj.CID3// 0xE000EFFC Component ID Register3 = UInt32  ...
        obj.intNum = Int  ...
        obj.vfxn = Void(*)(Void)  ...
        obj.priority = UInt  ...
        obj.enableInt = Bool  ...
module-wide config parameters
        msg: "A_unsupportedMaskingOption: unsupported maskSetting."
    };
        msg: "E_NMI: %s"
    };
        msg: "E_alreadyDefined: Hwi already defined: intr# %d"
    };
        msg: "E_busFault: %s"
    };
        msg: "E_debugMon: %s"
    };
        msg: "E_exception: id = %d, pc = %08x.\nTo see more exception detail, set ti.sysbios.family.arm.m3.Hwi.enableException = true or,\nexamine the Exception view for the ti.sysbios.family.arm.m3.Hwi module using ROV."
    };
        msg: "E_hardFault: %s"
    };
        msg: "E_memFault: %s"
    };
        msg: "E_noIsr: id = %d, pc = %08x"
    };
        msg: "E_reserved: %s %d"
    };
        msg: "E_svCall: svNum = %d"
    };
        msg: "E_usageFault: %s"
    };
        mask: Diags.USER2,
        msg: "LD_end: hwi: 0x%x"
    };
        mask: Diags.USER1 | Diags.USER2,
        msg: "LM_begin: hwi: 0x%x, func: 0x%x, preThread: %d, intNum: %d, irp: 0x%x"
    };
        STKALIGN: 1,
        BFHFNMIGN: 0,
        DIV_0_TRP: 0,
        UNALIGN_TRP: 0,
        USERSETMPEND: 0,
        NONEBASETHRDENA: 0
    };
    Hwi.resetFunc// Reset Handler. Default is c_int00 = Void(*)(Void) undefined;
module-wide functions
per-instance config parameters
    var params = new Hwi.Params// Instance config-params object;
        params.arg// ISR function argument. Default is 0 = UArg 0;
        params.enableInt// Enable this interrupt now? Default is true = Bool true;
per-instance creation
    var inst = Hwi.create// Create an instance-object(Int intNum, Void(*)(UArg) hwiFxn, params);
 
enum Hwi.MaskingOption

Shorthand interrupt masking options

XDCscript usage meta-domain
values of type Hwi.MaskingOption
    const Hwi.MaskingOption_NONE;
    // No interrupts are disabled
    const Hwi.MaskingOption_ALL;
    // All interrupts are disabled
    const Hwi.MaskingOption_SELF;
    // Only this interrupt is disabled
    const Hwi.MaskingOption_BITMASK;
    // User supplies IER masks
    const Hwi.MaskingOption_LOWER;
    // All current and lower priority interrupts are disabled. Only a few targets/devices truly support this masking option. For those that don't, this setting is treated the same as MaskingOption_SELF
C SYNOPSIS
struct Hwi.CCR

NVIC Configuration Control Register (CCR)

XDCscript usage meta-domain
var obj = new Hwi.CCR;
 
    obj.STKALIGN = Bits8  ...
    // Auto stack alignment in exception
    obj.BFHFNMIGN = Bits8  ...
    // All faults ignore BUS Faults
    obj.DIV_0_TRP = Bits8  ...
    // Trap on divige be zero
    obj.UNALIGN_TRP = Bits8  ...
    // Trap on all unaligned accesses
    obj.USERSETMPEND = Bits8  ...
    // Allow user to trigger interrupts
    obj.NONEBASETHRDENA = Bits8  ...
    // Allow entering thread mode anytime
C SYNOPSIS
struct Hwi.ExcContext

Exception Context - Register contents at the time of an exception

XDCscript usage meta-domain
var obj = new Hwi.ExcContext;
 
    obj.threadType = BIOS.ThreadType  ...
    obj.threadHandle = Ptr  ...
    obj.threadStack = Ptr  ...
    obj.threadStackSize = SizeT  ...
    obj.r0 = Ptr  ...
    obj.r1 = Ptr  ...
    obj.r2 = Ptr  ...
    obj.r3 = Ptr  ...
    obj.r4 = Ptr  ...
    obj.r5 = Ptr  ...
    obj.r6 = Ptr  ...
    obj.r7 = Ptr  ...
    obj.r8 = Ptr  ...
    obj.r9 = Ptr  ...
    obj.r10 = Ptr  ...
    obj.r11 = Ptr  ...
    obj.r12 = Ptr  ...
    obj.sp = Ptr  ...
    obj.lr = Ptr  ...
    obj.pc = Ptr  ...
    obj.psr = Ptr  ...
    obj.ICSR = Ptr  ...
    obj.MMFSR = Ptr  ...
    obj.BFSR = Ptr  ...
    obj.UFSR = Ptr  ...
    obj.HFSR = Ptr  ...
    obj.DFSR = Ptr  ...
    obj.MMAR = Ptr  ...
    obj.BFAR = Ptr  ...
    obj.AFSR = Ptr  ...
C SYNOPSIS
struct Hwi.HookSet

Hwi hook set type definition

XDCscript usage meta-domain
var obj = new Hwi.HookSet;
 
    obj.registerFxn = Void(*)(Int)  ...
    obj.createFxn = Void(*)(IHwi.Handle,Error.Block*)  ...
    obj.beginFxn = Void(*)(IHwi.Handle)  ...
    obj.endFxn = Void(*)(IHwi.Handle)  ...
    obj.deleteFxn = Void(*)(IHwi.Handle)  ...
DETAILS
The functions that make up a hookSet have certain restrictions. They cannot call any Hwi instance functions other than Hwi_getHookContext() and Hwi_setHookContext(). For all practical purposes, they should treat the Hwi_Handle passed to these functions as an opaque handle.
C SYNOPSIS
struct Hwi.NVIC

Nested Vectored Interrupt Controller

XDCscript usage meta-domain
var obj = new Hwi.NVIC;
 
    obj.RES_00 = UInt32  ...
    // 0xE000E000 reserved
    obj.ICTR = UInt32  ...
    // 0xE000E004 Interrupt Control Type
    obj.RES_08 = UInt32  ...
    // 0xE000E008 reserved
    obj.RES_0C = UInt32  ...
    // 0xE000E00C reserved
    obj.STCSR = UInt32  ...
    // 0xE000E010 SysTick Control & Status Register
    obj.STRVR = UInt32  ...
    // 0xE000E014 SysTick Reload Value Register
    obj.STCVR = UInt32  ...
    // 0xE000E018 SysTick Current Value Register
    obj.STCALIB = UInt32  ...
    // 0xE000E01C SysTick Calibration Value Register
    obj.RES_20 = UInt32[56]  ...
    // 0xE000E020-0xE000E0FC reserved
    obj.ISER = UInt32[8]  ...
    // 0xE000E100-0xE000E11C Interrupt Set Enable Registers
    obj.RES_120 = UInt32[24]  ...
    // 0xE000E120-0xE000E17C reserved
    obj.ICER = UInt32[8]  ...
    // 0xE000E180-0xE000E19C Interrupt Clear Enable Registers
    obj.RES_1A0 = UInt32[24]  ...
    // 0xE000E1A0-0xE000E1FC reserved
    obj.ISPR = UInt32[8]  ...
    // 0xE000E200-0xE000E21C Interrupt Set Pending Registers
    obj.RES_220 = UInt32[24]  ...
    // 0xE000E220-0xE000E7C reserved
    obj.ICPR = UInt32[8]  ...
    // 0xE000E280-0xE000E29C Interrupt Clear Pending Registers
    obj.RES_2A0 = UInt32[24]  ...
    // 0xE000E2A0-0xE000E2FC reserved
    obj.IABR = UInt32[8]  ...
    // 0xE000E300-0xE000E31C Interrupt Active Bit Registers
    obj.RES_320 = UInt32[56]  ...
    // 0xE000E320-0xE000E3FC reserved
    obj.IPR = UInt8[240]  ...
    // 0xE000E400-0xE000E4EF Interrupt Priority Registers
    obj.RES_4F0 = UInt32[516]  ...
    // 0xE000E4F0-0xE000ECFC reserved
    obj.CPUIDBR = UInt32  ...
    // 0xE000ED00 CPUID Base Register
    obj.ICSR = UInt32  ...
    // 0xE000ED04 Interrupt Control State Register
    obj.VTOR = UInt32  ...
    // 0xE000ED08 Vector Table Offset Register
    obj.AIRCR = UInt32  ...
    // 0xE000ED0C Application Interrupt/Reset Control Register
    obj.SCR = UInt32  ...
    // 0xE000ED10 System Control Register
    obj.CCR = UInt32  ...
    // 0xE000ED14 Configuration Control Register
    obj.SHPR = UInt8[12]  ...
    // 0xE000ED18 System Handlers 4-15 Priority Registers
    obj.SHCSR = UInt32  ...
    // 0xE000ED24 System Handler Control & State Register
    obj.MMFSR = UInt8  ...
    // 0xE000ED28 Memory Manage Fault Status Register
    obj.BFSR = UInt8  ...
    // 0xE000ED29 Bus Fault Status Register
    obj.UFSR = UInt16  ...
    // 0xE000ED2A Usage Fault Status Register
    obj.HFSR = UInt32  ...
    // 0xE000ED2C Hard Fault Status Register
    obj.DFSR = UInt32  ...
    // 0xE000ED30 Debug Fault Status Register
    obj.MMAR = UInt32  ...
    // 0xE000ED34 Memory Manager Address Register
    obj.BFAR = UInt32  ...
    // 0xE000ED38 Bus Fault Address Register
    obj.AFSR = UInt32  ...
    // 0xE000ED3C Auxiliary Fault Status Register
    obj.PFR0 = UInt32  ...
    // 0xE000ED40 Processor Feature Register
    obj.PFR1 = UInt32  ...
    // 0xE000ED44 Processor Feature Register
    obj.DFR0 = UInt32  ...
    // 0xE000ED48 Debug Feature Register
    obj.AFR0 = UInt32  ...
    // 0xE000ED4C Auxiliary Feature Register
    obj.MMFR0 = UInt32  ...
    // 0xE000ED50 Memory Model Fault Register0
    obj.MMFR1 = UInt32  ...
    // 0xE000ED54 Memory Model Fault Register1
    obj.MMFR2 = UInt32  ...
    // 0xE000ED58 Memory Model Fault Register2
    obj.MMFR3 = UInt32  ...
    // 0xE000ED5C Memory Model Fault Register3
    obj.ISAR0 = UInt32  ...
    // 0xE000ED60 ISA Feature Register0
    obj.ISAR1 = UInt32  ...
    // 0xE000ED64 ISA Feature Register1
    obj.ISAR2 = UInt32  ...
    // 0xE000ED68 ISA Feature Register2
    obj.ISAR3 = UInt32  ...
    // 0xE000ED6C ISA Feature Register3
    obj.ISAR4 = UInt32  ...
    // 0xE000ED70 ISA Feature Register4
    obj.RES_D74 = UInt32[99]  ...
    // 0xE000ED74-0xE000EEFC reserved
    obj.STI = UInt32  ...
    // 0xE000EF00 Software Trigger Interrupt Register
    obj.PID4 = UInt32  ...
    // 0xE000EFD0 Peripheral ID Register4
    obj.PID5 = UInt32  ...
    // 0xE000EFD4 Peripheral ID Register5
    obj.PID6 = UInt32  ...
    // 0xE000EFD8 Peripheral ID Register6
    obj.PID7 = UInt32  ...
    // 0xE000EFDC Peripheral ID Register7
    obj.PID0 = UInt32  ...
    // 0xE000EFE0 Peripheral ID Register0
    obj.PID1 = UInt32  ...
    // 0xE000EFE4 Peripheral ID Register1
    obj.PID2 = UInt32  ...
    // 0xE000EFE8 Peripheral ID Register2
    obj.PID3 = UInt32  ...
    // 0xE000EFEC Peripheral ID Register3
    obj.CID0 = UInt32  ...
    // 0xE000EFF0 Component ID Register0
    obj.CID1 = UInt32  ...
    // 0xE000EFF4 Component ID Register1
    obj.CID2 = UInt32  ...
    // 0xE000EFF8 Component ID Register2
    obj.CID3 = UInt32  ...
    // 0xE000EFFC Component ID Register3
C SYNOPSIS
metaonly struct Hwi.NonDispatchedInterrupt

non-dispatched interrupt object. provided so that XGCONF users can easily plug non-dispatched interrupts

XDCscript usage meta-domain
var obj = new Hwi.NonDispatchedInterrupt;
 
    obj.intNum = Int  ...
    obj.vfxn = Void(*)(Void)  ...
    obj.priority = UInt  ...
    obj.enableInt = Bool  ...
config Hwi.NUM_INTERRUPTS  // module-wide

The Cortex M3 NVIC supports up to 256 interrupts/exceptions

XDCscript usage meta-domain
const Hwi.NUM_INTERRUPTS = Int computed value;
DETAILS
The actual number supported is device specific and provided by the catalog device specification.
C SYNOPSIS
config Hwi.NUM_PRIORITIES  // module-wide

The Cortex M3 NVIC supports up to 256 interrupt priorities

XDCscript usage meta-domain
const Hwi.NUM_PRIORITIES = Int computed value;
DETAILS
The actual number supported is device specific and provided by the catalog device specification.
C SYNOPSIS
config Hwi.A_unsupportedMaskingOption  // module-wide

Assert when bad maskSetting parameter provided

XDCscript usage meta-domain
Hwi.A_unsupportedMaskingOption = Assert.Desc {
    msg: "A_unsupportedMaskingOption: unsupported maskSetting."
};
C SYNOPSIS
config Hwi.E_NMI  // module-wide

Error raised when NMI exception occurs

XDCscript usage meta-domain
Hwi.E_NMI = Error.Desc {
    msg: "E_NMI: %s"
};
C SYNOPSIS
config Hwi.E_alreadyDefined  // module-wide

Error raised when Hwi is already defined

XDCscript usage meta-domain
Hwi.E_alreadyDefined = Error.Desc {
    msg: "E_alreadyDefined: Hwi already defined: intr# %d"
};
C SYNOPSIS
config Hwi.E_busFault  // module-wide

Error raised when bus fault exception occurs

XDCscript usage meta-domain
Hwi.E_busFault = Error.Desc {
    msg: "E_busFault: %s"
};
C SYNOPSIS
config Hwi.E_debugMon  // module-wide

Error raised when debugMon exception occurs

XDCscript usage meta-domain
Hwi.E_debugMon = Error.Desc {
    msg: "E_debugMon: %s"
};
C SYNOPSIS
config Hwi.E_exception  // module-wide

Error raised when an exception occurs

XDCscript usage meta-domain
Hwi.E_exception = Error.Desc {
    msg: "E_exception: id = %d, pc = %08x.\nTo see more exception detail, set ti.sysbios.family.arm.m3.Hwi.enableException = true or,\nexamine the Exception view for the ti.sysbios.family.arm.m3.Hwi module using ROV."
};
C SYNOPSIS
config Hwi.E_hardFault  // module-wide

Error raised when hard fault exception occurs

XDCscript usage meta-domain
Hwi.E_hardFault = Error.Desc {
    msg: "E_hardFault: %s"
};
C SYNOPSIS
config Hwi.E_memFault  // module-wide

Error raised when memory fault exception occurs

XDCscript usage meta-domain
Hwi.E_memFault = Error.Desc {
    msg: "E_memFault: %s"
};
C SYNOPSIS
config Hwi.E_noIsr  // module-wide

Error raised when an uninitialized interrupt occurs

XDCscript usage meta-domain
Hwi.E_noIsr = Error.Desc {
    msg: "E_noIsr: id = %d, pc = %08x"
};
C SYNOPSIS
config Hwi.E_reserved  // module-wide

Error raised when reserved exception occurs

XDCscript usage meta-domain
Hwi.E_reserved = Error.Desc {
    msg: "E_reserved: %s %d"
};
C SYNOPSIS
config Hwi.E_svCall  // module-wide

Error raised when svCall exception occurs

XDCscript usage meta-domain
Hwi.E_svCall = Error.Desc {
    msg: "E_svCall: svNum = %d"
};
C SYNOPSIS
config Hwi.E_usageFault  // module-wide

Error raised when usage fault exception occurs

XDCscript usage meta-domain
Hwi.E_usageFault = Error.Desc {
    msg: "E_usageFault: %s"
};
C SYNOPSIS
config Hwi.LD_end  // module-wide

Issued just after return from Hwi function (with interrupts disabled)

XDCscript usage meta-domain
Hwi.LD_end = Log.EventDesc {
    mask: Diags.USER2,
    msg: "LD_end: hwi: 0x%x"
};
C SYNOPSIS
config Hwi.LM_begin  // module-wide

Issued just prior to Hwi function invocation (with interrupts disabled)

XDCscript usage meta-domain
Hwi.LM_begin = Log.EventDesc {
    mask: Diags.USER1 | Diags.USER2,
    msg: "LM_begin: hwi: 0x%x, func: 0x%x, preThread: %d, intNum: %d, irp: 0x%x"
};
C SYNOPSIS
config Hwi.disablePriority  // module-wide

The priority that BASEPRI is set to by Hwi_disable()

XDCscript usage meta-domain
Hwi.disablePriority = UInt undefined;
DETAILS
All interrupts configured with equal or less priority (equal or higher number) than disablePriority are disabled by Hwi_disable. Interrupts configured with higher priority (smaller number) than disablePriority are non-maskable (ie zero-latency).
The default setting is the second highest interrupt priority defined for the device. This results in priority 0 (and all other values in the same priority group) being the non-maskable interrupt priority. All other priorities are disabled with Hwi_disable().
C SYNOPSIS
config Hwi.dispatcherAutoNestingSupport  // module-wide

Include interrupt nesting logic in interrupt dispatcher?

XDCscript usage meta-domain
Hwi.dispatcherAutoNestingSupport = Bool true;
DETAILS
Default is true.
This option provides the user with the ability to optimize interrupt dispatcher performance when support for interrupt nesting is not required.
Setting this parameter to false will disable the logic in the interrupt dispatcher that manipulates interrupt mask registers and enables and disables interrupts before and after invoking the user's Hwi function.
Set this parameter to false if you don't need interrupts enabled during the execution of your Hwi functions.
C SYNOPSIS
config Hwi.dispatcherIrpTrackingSupport  // module-wide

Controls whether the dispatcher retains the interrupted thread's return address

XDCscript usage meta-domain
Hwi.dispatcherIrpTrackingSupport = Bool true;
DETAILS
This option is enabled by default.
Setting this parameter to false will disable the logic in the interrupt dispatcher that keeps track of the interrupt's return address and provide a small savings in interrupt latency.
The application can get an interrupt's most recent return address using the getIrp API.
C SYNOPSIS
config Hwi.dispatcherSwiSupport  // module-wide

Include Swi scheduling logic in interrupt dispatcher?

XDCscript usage meta-domain
Hwi.dispatcherSwiSupport = Bool undefined;
DETAILS
Default is inherited from BIOS.swiEnabled, which is true by default.
This option provides the user with the ability to optimize interrupt dispatcher performance when it is known that Swis will not be posted from any of their Hwi threads.
Setting this parameter to false will disable the logic in the interrupt dispatcher that invokes the Swi scheduler prior to returning from an interrupt.
C SYNOPSIS
config Hwi.dispatcherTaskSupport  // module-wide

Include Task scheduling logic in interrupt dispatcher?

XDCscript usage meta-domain
Hwi.dispatcherTaskSupport = Bool undefined;
DETAILS
Default is inherited from BIOS.taskEnabled, which is true by default.
This option provides the user with the ability to optimize interrupt dispatcher performance when it is known that no Task scheduling APIs (ie Semaphore_post()) will be executed from any of their Hwi threads.
Setting this parameter to false will disable the logic in the interrupt dispatcher that invokes the Task scheduler prior to returning from an interrupt.
C SYNOPSIS
config Hwi.excHookFunc  // module-wide

User Exception hook function

XDCscript usage meta-domain
Hwi.excHookFunc = Void(*)(Hwi.ExcContext*) null;
DETAILS
Called just after the exception context has been initialized.
This function will be run on the ISR stack.
This function must run to completion.
It is called without any Task or Swi scheduling protection and therefore can not call any functions that may cause a Swi or Task scheduling operation (Swi_post(), Semaphore_post(), Event_post(), etc).
C SYNOPSIS
config Hwi.priGroup  // module-wide

The PRIGROUP setting. Default is 0

XDCscript usage meta-domain
Hwi.priGroup = UInt 0;
DETAILS
This value will be written to the PRIGROUP field within the NVIC's Application Interrupt and Reset Control Register (Hwi_nvic.AIRCR). It defines how the 8 bit priority values are interpreted by the hardware.
Valid settings are 0-7.
The default setting of 0 causes bits 7-1 of an interrupt's priority value to be used to as a pre-emption priority, and bit 0 is used to determine which of two simultaneous interrupts with the same pre-emption priority will be serviced first.
C SYNOPSIS
metaonly config Hwi.busFaultFunc  // module-wide

Bus Fault Handler. Default is set to an internal exception handler

XDCscript usage meta-domain
Hwi.busFaultFunc = Void(*)(Void) undefined;
metaonly config Hwi.common$  // module-wide

Common module configuration parameters

XDCscript usage meta-domain
Hwi.common$ = Types.Common$ undefined;
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
metaonly config Hwi.debugMonFunc  // module-wide

Debug Mon Handler. Default is set to an internal exception handler

XDCscript usage meta-domain
Hwi.debugMonFunc = Void(*)(Void) undefined;
metaonly config Hwi.enableException  // module-wide

Enable full exception decoding

XDCscript usage meta-domain
Hwi.enableException = Bool false;
DETAILS
When this is enabled, the exception handler will fully decode an exception and dump the registers to the system console.
metaonly config Hwi.excContextBuffer  // module-wide

User Exception Context Buffer Address

XDCscript usage meta-domain
Hwi.excContextBuffer = Ptr undefined;
DETAILS
By default, when an exception occurs, an ExcContext structure is allocated on the ISR stack and filled in within the exception handler.
If excContextBuffer is initialized by the user, the ExcContext structure will be placed at that address instead.
The buffer must be large enough to contain an ExcContext structure.
metaonly config Hwi.excStackBuffer  // module-wide

User Exception Stack Buffer Address

XDCscript usage meta-domain
Hwi.excStackBuffer = Ptr undefined;
DETAILS
By default, when an exception occurs, a pointer to the base address of the stack being used by the thread causing the exception is placed
If excStackBuffer is initialized by the user, the stack contents of the thread causing the exception will be copied to that address instead.
The buffer must be large enough to contain the largest task stack or ISR stack defined in the application.
metaonly config Hwi.hardFaultFunc  // module-wide

Hard Fault Handler. Default is set to an internal exception handler

XDCscript usage meta-domain
Hwi.hardFaultFunc = Void(*)(Void) undefined;
metaonly config Hwi.memFaultFunc  // module-wide

Hard Mem Handler. Default is set to an internal exception handler

XDCscript usage meta-domain
Hwi.memFaultFunc = Void(*)(Void) undefined;
metaonly config Hwi.nmiFunc  // module-wide

NMI Handler. Default is set to an internal exception handler

XDCscript usage meta-domain
Hwi.nmiFunc = Void(*)(Void) undefined;
metaonly config Hwi.nonDispatchedInterrupts  // module-wide

non-dispatched interrupt array. provided so that XGCONF users can easily plug non-dispatched interrupts

XDCscript usage meta-domain
Hwi.nonDispatchedInterrupts = Hwi.NonDispatchedInterrupt[string] undefined;
metaonly config Hwi.nullIsrFunc  // module-wide

Uninitialized ISR Handler. Default is set to an internal exception handler

XDCscript usage meta-domain
Hwi.nullIsrFunc = Void(*)(Void) undefined;
metaonly config Hwi.nvicCCR  // module-wide

NVIC CCR register settings

XDCscript usage meta-domain
Hwi.nvicCCR = Hwi.CCR {
    STKALIGN: 1,
    BFHFNMIGN: 0,
    DIV_0_TRP: 0,
    UNALIGN_TRP: 0,
    USERSETMPEND: 0,
    NONEBASETHRDENA: 0
};
DETAILS
These setting are written to Hwi_nvic.CCR at startup time.
See the Cortex M3 architecture reference manual for details on the meanings of these parameters.
metaonly config Hwi.reservedFunc  // module-wide

Reserved Exception Handler. Default is set to an internal exception handler

XDCscript usage meta-domain
Hwi.reservedFunc = Void(*)(Void) undefined;
metaonly config Hwi.resetFunc  // module-wide

Reset Handler. Default is c_int00

XDCscript usage meta-domain
Hwi.resetFunc = Void(*)(Void) undefined;
metaonly config Hwi.resetVectorAddress  // module-wide

Alternate reset vector address. Default is 0x00000000

XDCscript usage meta-domain
Hwi.resetVectorAddress = Ptr 0x00000000;
DETAILS
if initialized by the user then an additional reset vector is created and placed in the ".resetVecs" section. To place the .resetVecs section into a specific memory section, add the following command to your config script:
	Program.sectMap[".resetVecs"] = YourMemorySection; 
metaonly config Hwi.rovViewInfo  // module-wide
XDCscript usage meta-domain
Hwi.rovViewInfo = ViewInfo.Instance ViewInfo.create;
metaonly config Hwi.svCallFunc  // module-wide

SVCall Handler. Default is set to an internal exception handler

XDCscript usage meta-domain
Hwi.svCallFunc = Void(*)(Void) undefined;
metaonly config Hwi.usageFaultFunc  // module-wide

Usage Fault Handler. Default is set to an internal exception handler

XDCscript usage meta-domain
Hwi.usageFaultFunc = Void(*)(Void) undefined;
metaonly config Hwi.vectorTableAddress  // module-wide

Location of the Interrupt Vector Table

XDCscript usage meta-domain
Hwi.vectorTableAddress = Ptr 0x00000000;
DETAILS
This parameter allows the user to override the default placement of the interrupt vector table. The NVIC's Vector Table Offset Register (VTOR) is also programmed to this value.
By default, the interrupt vector table will be placed at address 0x00000000.
Some systems require the vector table to be placed at an address other than 0 but still need a copy of the two M3 boot vectors (SP and reset PC), located there. To achieve this, a separate parameter resetVectorAdress is provided. If the resetVectorAddress has a different value then the vectorTableAddress then a separate 2 vector table is generated and placed at that address.
The vector table must be placed at an address at or lower than 0x3FFFFC00 and must be aligned on an even 64 word boundary.
metaonly Hwi.addHookSet()  // module-wide

addHookSet is used in a config file to add a hook set (defined by struct HookSet)

XDCscript usage meta-domain
Hwi.addHookSet(IHwi.HookSet hook) returns Void
ARGUMENTS
hook — structure of type HookSet
DETAILS
HookSet structure elements may be omitted, in which case those elements will not exist.
Instance Config Parameters

XDCscript usage meta-domain
var params = new Hwi.Params;
// Instance config-params object
    params.arg = UArg 0;
    // ISR function argument. Default is 0
    params.enableInt = Bool true;
    // Enable this interrupt now? Default is true
    params.eventId = Int -1;
    // Interrupt event ID (Interrupt Selection Number) Default is -1. Not all targets/devices support this instance parameter. On those that don't, this parameter is ignored
    params.maskSetting = IHwi.MaskingOption IHwi.MaskingOption_LOWER;
    // The interrupt controller is designed for priority based interrupts
    params.priority = Int 255;
    // Interrupt priority. Valid priorities are 0 - 255. 0 is the highest priority. The default is 255 which is the lowest priority interrupt
config Hwi.arg  // instance

ISR function argument. Default is 0

XDCscript usage meta-domain
var params = new Hwi.Params;
  ...
params.arg = UArg 0;
C SYNOPSIS
config Hwi.enableInt  // instance

Enable this interrupt now? Default is true

XDCscript usage meta-domain
var params = new Hwi.Params;
  ...
params.enableInt = Bool true;
C SYNOPSIS
config Hwi.eventId  // instance

Interrupt event ID (Interrupt Selection Number) Default is -1. Not all targets/devices support this instance parameter. On those that don't, this parameter is ignored

XDCscript usage meta-domain
var params = new Hwi.Params;
  ...
params.eventId = Int -1;
C SYNOPSIS
config Hwi.maskSetting  // instance

The interrupt controller is designed for priority based interrupts

XDCscript usage meta-domain
var params = new Hwi.Params;
  ...
C SYNOPSIS
config Hwi.priority  // instance

Interrupt priority. Valid priorities are 0 - 255. 0 is the highest priority. The default is 255 which is the lowest priority interrupt

XDCscript usage meta-domain
var params = new Hwi.Params;
  ...
params.priority = Int 255;
C SYNOPSIS
Instance Creation

XDCscript usage meta-domain
var params = new Hwi.Params;
// Allocate instance config-params
params.config =   ...
// Assign individual configs
 
var inst = Hwi.create(Int intNum, Void(*)(UArg) hwiFxn, params);
// Create an instance-object
ARGUMENTS
intNum — interrupt number
hwiFxn — pointer to ISR function
params — per-instance config params, or NULL to select default values (target-domain only)
eb — active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
A Hwi dispatcher table entry is created and filled with the function specified by the fxn parameter and the attributes specified by the params parameter.
If params is NULL, the Hwi's dispatcher properties are assigned a default set of values. Otherwise, the following properties are specified by a structure of type Hwi_Params.
  • The arg element is a generic argument that is passed to the plugged function as its only parameter. The default value is 0.
  • The enableInt element determines whether the interrupt should be enabled in the IER by create.
  • The maskSetting element defines the dispatcherAutoNestingSupport behavior of the interrupt.
Hwi_create returns a pointer to the created Hwi object.
generated on Fri, 21 Jan 2011 00:19:06 GMT