xdc.services.spec
Enum Type.Modifier
java.lang.Object
java.lang.Enum<Type.Modifier>
xdc.services.spec.Type.Modifier
- All Implemented Interfaces:
- java.io.Serializable, java.lang.Comparable<Type.Modifier>
- Enclosing class:
- Type
public static enum Type.Modifier
- extends java.lang.Enum<Type.Modifier>
Method Summary |
static Type.Modifier |
valueOf(java.lang.String name)
Returns the enum constant of this type with the specified name. |
static Type.Modifier[] |
values()
Returns an array containing the constants of this enum type, in
the order they're declared. |
Methods inherited from class java.lang.Enum |
clone, compareTo, equals, getDeclaringClass, hashCode, name, ordinal, toString, valueOf |
Methods inherited from class java.lang.Object |
finalize, getClass, notify, notifyAll, wait, wait, wait |
CONST
public static final Type.Modifier CONST
RESTRICT
public static final Type.Modifier RESTRICT
VOLATILE
public static final Type.Modifier VOLATILE
values
public static final Type.Modifier[] values()
- Returns an array containing the constants of this enum type, in
the order they're declared. This method may be used to iterate
over the constants as follows:
for(Type.Modifier c : Type.Modifier.values())
System.out.println(c);
- Returns:
- an array containing the constants of this enum type, in
the order they're declared
valueOf
public static Type.Modifier valueOf(java.lang.String name)
- Returns the enum constant of this type with the specified name.
The string must match exactly an identifier used to declare an
enum constant in this type. (Extraneous whitespace characters are
not permitted.)
- Parameters:
name
- the name of the enum constant to be returned.
- Returns:
- the enum constant with the specified name
- Throws:
java.lang.IllegalArgumentException
- if this enum type has no constant
with the specified name