IPC API
3.36.02.13
|
Multiple fixed size buffer heap implementation.
The HeapMultiBufMP manager provides functions to allocate and free storage from a shared memory heap of type HeapMultiBufMP which inherits from IHeap. HeapMultiBufMP manages multiple fixed-size memory buffers. Each buffer contains a fixed number of allocatable memory 'blocks' of the same size. HeapMultiBufMP is intended as a fast and deterministic memory manager which can service requests for blocks of arbitrary size.
An example HeapMultiBufMP instance might have sixteen 32-byte blocks in one buffer, and four 128-byte blocks in another buffer. A request for memory will be serviced by the smallest possible block, so a request for 100 bytes would receive a 128-byte block in our example.
Allocating from HeapMultiBufMP will try to return a block from the first buffer which has:
Buffer configuration for a new instance is primarily supplied via the HeapMultiBufMP_Params.bucketEntries instance configuration parameter. Once buckets are adjusted for size and alignment, buffers with equal sizes and alignments are combined.
Block Sizes and Alignment
In addition to the buffer configuration, a HeapMultiBufMP_Params.name and a HeapMultiBufMP_Params.regionId (from which shared memory is allocated) must be supplied when creating an instance.
Once an instance is created, HeapMultiBufMP_open() can be performed using the name that was supplied in HeapMultiBufMP_create(). The open is used to gain access to the same HeapMultiBufMP instance. Generally an instance is created on one processor and opened on the other processor(s). The open returns (by reference) a HeapMultiBufMP instance handle like the create, however the open does not modify the shared memory.
HeapMultiBufMP_open() will return HeapMultiBufMP_E_FAIL if called before the instance is created.
The HeapMultiBufMP header should be included in an application as follows:
#include <ti/ipc/GateMP.h>
Go to the source code of this file.
Data Structures | |
struct | HeapMultiBufMP_Bucket |
Structure for bucket configuration. More... | |
struct | HeapMultiBufMP_Params |
Structure defining parameters for the HeapMultiBufMP module. More... | |
struct | HeapMultiBufMP_ExtendedStats |
Stats structure for the HeapMultiBufMP_getExtendedStats() API. More... | |
Macros | |
#define | HeapMultiBufMP_S_BUSY 2 |
The resource is still in use. More... | |
#define | HeapMultiBufMP_S_ALREADYSETUP 1 |
The module has been already setup. More... | |
#define | HeapMultiBufMP_S_SUCCESS 0 |
Operation is successful. More... | |
#define | HeapMultiBufMP_E_FAIL -1 |
Generic failure. More... | |
#define | HeapMultiBufMP_E_INVALIDARG -2 |
Argument passed to function is invalid. More... | |
#define | HeapMultiBufMP_E_MEMORY -3 |
Operation resulted in memory failure. More... | |
#define | HeapMultiBufMP_E_ALREADYEXISTS -4 |
The specified entity already exists. More... | |
#define | HeapMultiBufMP_E_NOTFOUND -5 |
Unable to find the specified entity. More... | |
#define | HeapMultiBufMP_E_TIMEOUT -6 |
Operation timed out. More... | |
#define | HeapMultiBufMP_E_INVALIDSTATE -7 |
Module is not initialized. More... | |
#define | HeapMultiBufMP_E_OSFAILURE -8 |
A failure occurred in an OS-specific call. More... | |
#define | HeapMultiBufMP_E_RESOURCE -9 |
Specified resource is not available. More... | |
#define | HeapMultiBufMP_E_RESTART -10 |
Operation was interrupted. Please restart the operation. More... | |
#define | HeapMultiBufMP_MAXBUCKETS ((UInt)8) |
Maximum number of buffer buckets supported. More... | |
Typedefs | |
typedef struct HeapMultiBufMP_Object * | HeapMultiBufMP_Handle |
HeapMultiBufMP_Handle type. More... | |
typedef struct HeapMultiBufMP_Bucket | HeapMultiBufMP_Bucket |
Structure for bucket configuration. More... | |
typedef struct HeapMultiBufMP_Params | HeapMultiBufMP_Params |
Structure defining parameters for the HeapMultiBufMP module. More... | |
typedef struct HeapMultiBufMP_ExtendedStats | HeapMultiBufMP_ExtendedStats |
Stats structure for the HeapMultiBufMP_getExtendedStats() API. More... | |
Functions | |
Int | HeapMultiBufMP_close (HeapMultiBufMP_Handle *handlePtr) |
Close a HeapMultiBufMP instance. More... | |
HeapMultiBufMP_Handle | HeapMultiBufMP_create (const HeapMultiBufMP_Params *params) |
Create a HeapMultiBufMP instance. More... | |
Int | HeapMultiBufMP_delete (HeapMultiBufMP_Handle *handlePtr) |
Delete a created HeapMultiBufMP instance. More... | |
Int | HeapMultiBufMP_open (String name, HeapMultiBufMP_Handle *handlePtr) |
Open a created HeapMultiBufMP instance. More... | |
Void | HeapMultiBufMP_Params_init (HeapMultiBufMP_Params *params) |
Initialize a HeapMultiBufMP parameters struct. More... | |
Void * | HeapMultiBufMP_alloc (HeapMultiBufMP_Handle handle, SizeT size, SizeT align) |
Allocate a block of memory of specified size and alignment. More... | |
Void | HeapMultiBufMP_free (HeapMultiBufMP_Handle handle, Ptr block, SizeT size) |
Frees a block of memory. More... | |
Void | HeapMultiBufMP_getExtendedStats (HeapMultiBufMP_Handle handle, HeapMultiBufMP_ExtendedStats *stats) |
Get extended memory statistics. More... | |
Void | HeapMultiBufMP_getStats (HeapMultiBufMP_Handle handle, Ptr stats) |
Get memory statistics. More... | |
#define HeapMultiBufMP_S_BUSY 2 |
The resource is still in use.
#define HeapMultiBufMP_S_ALREADYSETUP 1 |
The module has been already setup.
#define HeapMultiBufMP_S_SUCCESS 0 |
Operation is successful.
#define HeapMultiBufMP_E_FAIL -1 |
Generic failure.
#define HeapMultiBufMP_E_INVALIDARG -2 |
Argument passed to function is invalid.
#define HeapMultiBufMP_E_MEMORY -3 |
Operation resulted in memory failure.
#define HeapMultiBufMP_E_ALREADYEXISTS -4 |
The specified entity already exists.
#define HeapMultiBufMP_E_NOTFOUND -5 |
Unable to find the specified entity.
#define HeapMultiBufMP_E_TIMEOUT -6 |
Operation timed out.
#define HeapMultiBufMP_E_INVALIDSTATE -7 |
Module is not initialized.
#define HeapMultiBufMP_E_OSFAILURE -8 |
A failure occurred in an OS-specific call.
#define HeapMultiBufMP_E_RESOURCE -9 |
Specified resource is not available.
#define HeapMultiBufMP_E_RESTART -10 |
Operation was interrupted. Please restart the operation.
#define HeapMultiBufMP_MAXBUCKETS ((UInt)8) |
Maximum number of buffer buckets supported.
typedef struct HeapMultiBufMP_Object* HeapMultiBufMP_Handle |
HeapMultiBufMP_Handle type.
typedef struct HeapMultiBufMP_Bucket HeapMultiBufMP_Bucket |
Structure for bucket configuration.
An array of buckets is a required parameter to create any HeapMultiBufMP instance. The fields of each bucket correspond to the attributes of each buffer in the HeapMultiBufMP. The actual block sizes and alignments may be adjusted per the process described at HeapMultiBufMP_Params.bucketEntries.
typedef struct HeapMultiBufMP_Params HeapMultiBufMP_Params |
Structure defining parameters for the HeapMultiBufMP module.
typedef struct HeapMultiBufMP_ExtendedStats HeapMultiBufMP_ExtendedStats |
Stats structure for the HeapMultiBufMP_getExtendedStats() API.
Int HeapMultiBufMP_close | ( | HeapMultiBufMP_Handle * | handlePtr | ) |
Close a HeapMultiBufMP instance.
Closing an instance will free local memory consumed by the opened instance. All opened instances should be closed before the instance is deleted.
[in,out] | handlePtr | Pointer to handle returned from HeapMultiBufMP_open |
HeapMultiBufMP_Handle HeapMultiBufMP_create | ( | const HeapMultiBufMP_Params * | params | ) |
Create a HeapMultiBufMP instance.
[in] | params | HeapMultiBufMP parameters |
Int HeapMultiBufMP_delete | ( | HeapMultiBufMP_Handle * | handlePtr | ) |
Delete a created HeapMultiBufMP instance.
[in,out] | handlePtr | Pointer to handle to delete. |
Int HeapMultiBufMP_open | ( | String | name, |
HeapMultiBufMP_Handle * | handlePtr | ||
) |
Open a created HeapMultiBufMP instance.
Once an instance is created, an open can be performed. The open is used to gain access to the same HeapMultiBufMP instance. Generally an instance is created on one processor and opened on the other processor.
The open returns a HeapMultiBufMP instance handle like the create, however the open does not initialize the shared memory. The supplied name is used to identify the created instance.
Call HeapMultiBufMP_close() when the opened instance is not longer needed.
[in] | name | Name of created HeapMultiBufMP instance |
[out] | handlePtr | Pointer to HeapMultiBufMP handle to be opened |
Void HeapMultiBufMP_Params_init | ( | HeapMultiBufMP_Params * | params | ) |
Initialize a HeapMultiBufMP parameters struct.
[out] | params | Pointer to GateMP parameters |
Void* HeapMultiBufMP_alloc | ( | HeapMultiBufMP_Handle | handle, |
SizeT | size, | ||
SizeT | align | ||
) |
Allocate a block of memory of specified size and alignment.
NULL is returned if alloc fails.
[in] | handle | Handle to previously created/opened instance. |
[in] | size | Size to be allocated (in MADUs) |
[in] | align | Alignment for allocation (power of 2) |
Void HeapMultiBufMP_free | ( | HeapMultiBufMP_Handle | handle, |
Ptr | block, | ||
SizeT | size | ||
) |
Frees a block of memory.
[in] | handle | Handle to previously created/opened instance. |
[in] | block | Block of memory to be freed. |
[in] | size | Size to be freed (in MADUs) |
Void HeapMultiBufMP_getExtendedStats | ( | HeapMultiBufMP_Handle | handle, |
HeapMultiBufMP_ExtendedStats * | stats | ||
) |
Get extended memory statistics.
This function retrieves the extended statistics for a HeapMultiBufMP instance. It does not retrieve the standard Memory_Stats information. Refer to HeapMultiBufMP_ExtendedStats for more information regarding what information is returned.
In BIOS, HeapMultiBufMP.trackAllocs needs to be set to 'true' in the configuration to get meaningful extended stats.
[in] | handle | Handle to previously created/opened instance. |
[out] | stats | ExtendedStats structure |
Void HeapMultiBufMP_getStats | ( | HeapMultiBufMP_Handle | handle, |
Ptr | stats | ||
) |
Get memory statistics.
[in] | handle | Handle to previously created/opened instance. |
[out] | stats | Memory statistics structure |