module ti.sdo.ipc.gates.GatePetersonN

IGateMPSupport gate based on the Peterson's algorithm

This module implements the ti.sdo.ipc.interfaces.IGateMPSupport interface using the Peterson Algorithm in shared memory. This implementation works for N processors. [ more ... ]
C synopsis target-domain sourced in ti/sdo/ipc/gates/GatePetersonN.xdc
#include <ti/sdo/ipc/gates/GatePetersonN.h>
Functions
Void
Void
Void
Void
Functions common to all IGateProvider modules
Bool 
Functions common to all IGateMPSupport modules
SizeT 
Functions common to all target instances
Functions common to all target modules
Defines
#define
#define
Typedefs
typedef struct
typedef struct
typedef struct
Constants
extern const UInt 
extern const UInt 
 
DETAILS
This module implements the ti.sdo.ipc.interfaces.IGateMPSupport interface using the Peterson Algorithm in shared memory. This implementation works for N processors.
Each GatePetersonN instance requires a small piece of shared memory. The base address of this shared memory is specified as the 'sharedAddr' argument to the create. The amount of shared memory consumed by a single instance can be obtained using the sharedMemReq call.
Shared memory has to conform to the following specification. Padding is added between certain elements in shared memory if cache alignment is required for the region in which the instance is placed.
              shmBaseAddr -> ------------------------------ bytes
                             |  enteredStage[0]           | 4
                             |  (PADDING if aligned)      |
                             |----------------------------|
                             |  enteredStage[1]           | 4
                             |  (PADDING if aligned)      |
                             |----------------------------|
                                      . . . 
                             |----------------------------|
                             |  enteredStage[N-1]         | 4
                             |  (PADDING if aligned)      |
                             |----------------------------|
                             |  lastProcEnteringStage[1]  | 4
                             |  (PADDING if aligned)      |
                             |----------------------------|
                                      . . . 
                             |----------------------------|
                             |  lastProcEnteringStage[N-1]| 4
                             |  (PADDING if aligned)      |
                             |----------------------------|
 
const GatePetersonN_Q_BLOCKING

Blocking quality

C synopsis target-domain
#define GatePetersonN_Q_BLOCKING (Int)1
 
DETAILS
Gates with this "quality" may cause the calling thread to block; i.e., suspend execution until another thread leaves the gate.
 
const GatePetersonN_Q_PREEMPTING

Preempting quality

C synopsis target-domain
#define GatePetersonN_Q_PREEMPTING (Int)2
 
DETAILS
Gates with this "quality" allow other threads to preempt the thread that has already entered the gate.
 
config GatePetersonN_MAX_NUM_PROCS  // module-wide
C synopsis target-domain
extern const UInt GatePetersonN_MAX_NUM_PROCS;
 
 
config GatePetersonN_numInstances  // module-wide

Maximum number of instances supported by the GatePetersonN module

C synopsis target-domain
extern const UInt GatePetersonN_numInstances;
 
 
GatePetersonN_query()  // module-wide

Runtime test for a particular gate quality

C synopsis target-domain
Bool GatePetersonN_query(Int qual);
 
ARGUMENTS
qual — constant describing a quality
RETURNS
Returns TRUE if the gate has the given quality, and FALSE otherwise, which includes the case when the gate does not recognize the constant describing the quality.
 
GatePetersonN_sharedMemReq()  // module-wide

Amount of shared memory required for creation of each instance

C synopsis target-domain
SizeT GatePetersonN_sharedMemReq(IGateMPSupport_Params *params);
 
ARGUMENTS
params — Pointer to the parameters that will be used in the create.
DETAILS
The value returned by this function may depend on the cache alignment requirements for the shared region from which memory will be used.
RETURNS
Number of MAUs needed to create the instance.
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId GatePetersonN_Module_id();
// Get this module's unique id
 
Bool GatePetersonN_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle GatePetersonN_Module_heap();
// The heap from which this module allocates memory
 
Bool GatePetersonN_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 GatePetersonN_Module_getMask();
// Returns the diagnostics mask for this module
 
Void GatePetersonN_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types

C synopsis target-domain
typedef struct GatePetersonN_Object GatePetersonN_Object;
// Opaque internal representation of an instance object
 
typedef GatePetersonN_Object *GatePetersonN_Handle;
// Client reference to an instance object
 
typedef struct GatePetersonN_Struct GatePetersonN_Struct;
// Opaque client structure large enough to hold an instance object
 
GatePetersonN_Handle GatePetersonN_handle(GatePetersonN_Struct *structP);
// Convert this instance structure pointer into an instance handle
 
GatePetersonN_Struct *GatePetersonN_struct(GatePetersonN_Handle handle);
// Convert this instance handle into an instance structure pointer
Instance Config Parameters

C synopsis target-domain
typedef struct GatePetersonN_Params {
// Instance config-params structure
    IInstance_Params *instance;
    // Common per-instance configs
    UInt resourceId;
    // Logical resource id
    Ptr sharedAddr;
    // Physical address of the shared memory
} GatePetersonN_Params;
 
Void GatePetersonN_Params_init(GatePetersonN_Params *params);
// Initialize this config-params structure with supplier-specified defaults before instance creation
 
config GatePetersonN_resourceId  // instance

Logical resource id

C synopsis target-domain
      ...
    UInt resourceId;
 
 
config GatePetersonN_sharedAddr  // instance

Physical address of the shared memory

C synopsis target-domain
      ...
    Ptr sharedAddr;
 
DETAILS
This parameter is only used by GateMP delegates that use shared memory
Instance Creation

C synopsis target-domain
GatePetersonN_Handle GatePetersonN_create(IGateProvider_Handle localGate, const GatePetersonN_Params *params, Error_Block *eb);
// Allocate and initialize a new instance object and return its handle
 
Void GatePetersonN_construct(GatePetersonN_Struct *structP, IGateProvider_Handle localGate, const GatePetersonN_Params *params, Error_Block *eb);
// Initialize a new instance object inside the provided structure
ARGUMENTS
localGate — Gate to use for local protection.
params — per-instance config params, or NULL to select default values (target-domain only)
eb — active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
A Non-NULL gate for local protection must be passed to the create call. If no local protection is desired, a xdc.runtime.GateNull handle must be passed in.
Instance Deletion

C synopsis target-domain
Void GatePetersonN_delete(GatePetersonN_Handle *handleP);
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
 
Void GatePetersonN_destruct(GatePetersonN_Struct *structP);
// Finalize the instance object inside the provided structure
Instance Convertors

C synopsis target-domain
IGateMPSupport_Handle GatePetersonN_Handle_upCast(GatePetersonN_Handle handle);
// unconditionally move one level up the inheritance hierarchy
 
GatePetersonN_Handle GatePetersonN_Handle_downCast(IGateMPSupport_Handle handle);
// conditionally move one level down the inheritance hierarchy; NULL upon failure
 
IGateProvider_Handle GatePetersonN_Handle_upCast2(GatePetersonN_Handle handle);
// unconditionally move 2 levels up the inheritance hierarchy
 
GatePetersonN_Handle GatePetersonN_Handle_downCast2(IGateProvider_Handle handle);
// conditionally move 2 levels down the inheritance hierarchy; NULL upon failure
Instance Built-Ins

C synopsis target-domain
Int GatePetersonN_Object_count();
// The number of statically-created instance objects
 
GatePetersonN_Handle GatePetersonN_Object_get(GatePetersonN_Object *array, Int i);
// The handle of the i-th statically-created instance object (array == NULL)
 
GatePetersonN_Handle GatePetersonN_Object_first();
// The handle of the first dynamically-created instance object, or NULL
 
GatePetersonN_Handle GatePetersonN_Object_next(GatePetersonN_Handle handle);
// The handle of the next dynamically-created instance object, or NULL
 
IHeap_Handle GatePetersonN_Object_heap();
// The heap used to allocate dynamically-created instance objects
 
Types_Label *GatePetersonN_Handle_label(GatePetersonN_Handle handle, Types_Label *buf);
// The label associated with this instance object
 
String GatePetersonN_Handle_name(GatePetersonN_Handle handle);
// The name of this instance object
 
Configuration settings sourced in ti/sdo/ipc/gates/GatePetersonN.xdc
var GatePetersonN = xdc.useModule('ti.sdo.ipc.gates.GatePetersonN');
module-wide constants & types
module-wide config parameters
 
module-wide functions
per-instance config parameters
    var params = new GatePetersonN.Params// Instance config-params object;
        params.resourceId// Logical resource id = UInt 0;
        params.sharedAddr// Physical address of the shared memory = Ptr null;
per-instance creation
    var inst = GatePetersonN.create// Create an instance-object(IGateProvider.Handle localGate, params);
 
 
const GatePetersonN.Q_BLOCKING

Blocking quality

Configuration settings
const GatePetersonN.Q_BLOCKING = 1;
 
DETAILS
Gates with this "quality" may cause the calling thread to block; i.e., suspend execution until another thread leaves the gate.
C SYNOPSIS
 
const GatePetersonN.Q_PREEMPTING

Preempting quality

Configuration settings
const GatePetersonN.Q_PREEMPTING = 2;
 
DETAILS
Gates with this "quality" allow other threads to preempt the thread that has already entered the gate.
C SYNOPSIS
 
config GatePetersonN.MAX_NUM_PROCS  // module-wide
Configuration settings
GatePetersonN.MAX_NUM_PROCS = UInt 8;
 
C SYNOPSIS
 
config GatePetersonN.numInstances  // module-wide

Maximum number of instances supported by the GatePetersonN module

Configuration settings
GatePetersonN.numInstances = UInt 512;
 
C SYNOPSIS
 
metaonly config GatePetersonN.common$  // module-wide

Common module configuration parameters

Configuration settings
GatePetersonN.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
 
metaonly GatePetersonN.getNumResources()  // module-wide

Returns the number of resources offered by the GateMP delegate

Configuration settings
GatePetersonN.getNumResources() returns UInt
 
 
metaonly GatePetersonN.queryMeta()  // module-wide

Configuration time test for a particular gate quality

Configuration settings
GatePetersonN.queryMeta(Int qual) returns Bool
 
ARGUMENTS
qual — constant describing a quality
RETURNS
Returns TRUE if the gate has the given quality, and FALSE otherwise, which includes the case when the gate does not recognize the constant describing the quality.
Instance Config Parameters

Configuration settings
var params = new GatePetersonN.Params;
// Instance config-params object
    params.resourceId = UInt 0;
    // Logical resource id
    params.sharedAddr = Ptr null;
    // Physical address of the shared memory
 
config GatePetersonN.resourceId  // instance

Logical resource id

Configuration settings
var params = new GatePetersonN.Params;
  ...
params.resourceId = UInt 0;
 
C SYNOPSIS
 
config GatePetersonN.sharedAddr  // instance

Physical address of the shared memory

Configuration settings
var params = new GatePetersonN.Params;
  ...
params.sharedAddr = Ptr null;
 
DETAILS
This parameter is only used by GateMP delegates that use shared memory
C SYNOPSIS
Instance Creation

Configuration settings
var params = new GatePetersonN.Params;
// Allocate instance config-params
params.config =   ...
// Assign individual configs
 
var inst = GatePetersonN.create(IGateProvider.Handle localGate, params);
// Create an instance-object
ARGUMENTS
localGate — Gate to use for local protection.
params — per-instance config params, or NULL to select default values (target-domain only)
eb — active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
A Non-NULL gate for local protection must be passed to the create call. If no local protection is desired, a xdc.runtime.GateNull handle must be passed in.
generated on Wed, 10 Dec 2014 03:08:55 GMT