IPC API  3.10.02.13
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Data Structures | Macros | Typedefs | Functions
HeapBufMP.h File Reference

Detailed Description

Multi-processor fixed-size buffer heap implementation.

Note:
HeapBufMP is currently only available for SYS/BIOS.

Heap implementation that manages fixed size buffers that can be used in a multiprocessor system with shared memory.

The HeapBufMP manager provides functions to allocate and free storage from a heap of type HeapBufMP which inherits from IHeap. HeapBufMP manages a single fixed-size buffer, split into equally sized allocatable blocks.

The HeapBufMP manager is intended as a very fast memory manager which can only allocate blocks of a single size. It is ideal for managing a heap that is only used for allocating a single type of object, or for objects that have very similar sizes.

The HeapBufMP module uses a NameServer instance to store instance information when an instance is created. The name supplied must be unique for all HeapBufMP instances.

HeapBufMP_create() initializes the shared memory as needed. Once an instance is created, HeapBufMP_open() can be performed. The open is used to gain access to the same HeapBufMP instance. Generally an instance is created on one processor and opened on the other processor(s).

The open returns a HeapBufMP instance handle like the create, however the open does not modify the shared memory.

The HeapBufMP header should be included in an application as follows:

#include <ti/ipc/HeapBufMP.h>
#include <ti/ipc/GateMP.h>
Include dependency graph for HeapBufMP.h:

Go to the source code of this file.

Data Structures

struct  HeapBufMP_Params
 Structure defining parameters for the HeapBufMP module. More...
struct  HeapBufMP_ExtendedStats
 Stats structure for HeapBufMP_getExtendedStats() More...

Macros

#define HeapBufMP_S_BUSY   2
 The resource is still in use.
#define HeapBufMP_S_ALREADYSETUP   1
 The module has been already setup.
#define HeapBufMP_S_SUCCESS   0
 Operation is successful.
#define HeapBufMP_E_FAIL   -1
 Generic failure.
#define HeapBufMP_E_INVALIDARG   -2
 Argument passed to function is invalid.
#define HeapBufMP_E_MEMORY   -3
 Operation resulted in memory failure.
#define HeapBufMP_E_ALREADYEXISTS   -4
 The specified entity already exists.
#define HeapBufMP_E_NOTFOUND   -5
 Unable to find the specified entity.
#define HeapBufMP_E_TIMEOUT   -6
 Operation timed out.
#define HeapBufMP_E_INVALIDSTATE   -7
 Module is not initialized.
#define HeapBufMP_E_OSFAILURE   -8
 A failure occurred in an OS-specific call.
#define HeapBufMP_E_RESOURCE   -9
 Specified resource is not available.
#define HeapBufMP_E_RESTART   -10
 Operation was interrupted. Please restart the operation.

Typedefs

typedef struct HeapBufMP_Object * HeapBufMP_Handle
 HeapBufMP_Handle type.
typedef struct HeapBufMP_Params HeapBufMP_Params
 Structure defining parameters for the HeapBufMP module.
typedef struct
HeapBufMP_ExtendedStats 
HeapBufMP_ExtendedStats
 Stats structure for HeapBufMP_getExtendedStats()

Functions

Int HeapBufMP_close (HeapBufMP_Handle *handlePtr)
 Close a HeapBufMP instance.
HeapBufMP_Handle HeapBufMP_create (const HeapBufMP_Params *params)
 Create a HeapBufMP instance.
Int HeapBufMP_delete (HeapBufMP_Handle *handlePtr)
 Delete a created HeapBufMP instance.
Int HeapBufMP_open (String name, HeapBufMP_Handle *handlePtr)
 Open a created HeapBufMP instance.
Void HeapBufMP_Params_init (HeapBufMP_Params *params)
 Initialize a HeapBufMP parameters struct.
Void * HeapBufMP_alloc (HeapBufMP_Handle handle, SizeT size, SizeT align)
 Allocate a block of memory of specified size and alignment.
Void HeapBufMP_free (HeapBufMP_Handle handle, Ptr block, SizeT size)
 Frees a block of memory.
Void HeapBufMP_getExtendedStats (HeapBufMP_Handle handle, HeapBufMP_ExtendedStats *stats)
 Get extended memory statistics.
Void HeapBufMP_getStats (HeapBufMP_Handle handle, Ptr stats)
 Get memory statistics.

Macro Definition Documentation

#define HeapBufMP_S_BUSY   2

The resource is still in use.

#define HeapBufMP_S_ALREADYSETUP   1

The module has been already setup.

#define HeapBufMP_S_SUCCESS   0

Operation is successful.

#define HeapBufMP_E_FAIL   -1

Generic failure.

#define HeapBufMP_E_INVALIDARG   -2

Argument passed to function is invalid.

#define HeapBufMP_E_MEMORY   -3

Operation resulted in memory failure.

#define HeapBufMP_E_ALREADYEXISTS   -4

The specified entity already exists.

#define HeapBufMP_E_NOTFOUND   -5

Unable to find the specified entity.

#define HeapBufMP_E_TIMEOUT   -6

Operation timed out.

#define HeapBufMP_E_INVALIDSTATE   -7

Module is not initialized.

#define HeapBufMP_E_OSFAILURE   -8

A failure occurred in an OS-specific call.

#define HeapBufMP_E_RESOURCE   -9

Specified resource is not available.

#define HeapBufMP_E_RESTART   -10

Operation was interrupted. Please restart the operation.


Typedef Documentation

typedef struct HeapBufMP_Object* HeapBufMP_Handle

HeapBufMP_Handle type.

Structure defining parameters for the HeapBufMP module.

See also:
HeapBufMP_create()

Function Documentation

Int HeapBufMP_close ( HeapBufMP_Handle handlePtr)

Close a HeapBufMP instance.

Closing an instance will free local memory consumed by the opened instance. All opened instances should be closed before the instance is deleted.

Parameters:
[in,out]handlePtrPointer to handle returned from HeapBufMP_open()
Returns:
HeapBufMP status:
See also:
HeapBufMP_open()
HeapBufMP_Handle HeapBufMP_create ( const HeapBufMP_Params params)

Create a HeapBufMP instance.

Parameters:
[in]paramsHeapBufMP parameters
Returns:
HeapBufMP Handle
See also:
HeapBufMP_delete()
Int HeapBufMP_delete ( HeapBufMP_Handle handlePtr)

Delete a created HeapBufMP instance.

Parameters:
[in,out]handlePtrPointer to handle to delete.
Returns:
HeapBufMP status:
See also:
HeapBufMP_create()
Int HeapBufMP_open ( String  name,
HeapBufMP_Handle handlePtr 
)

Open a created HeapBufMP instance.

Once an instance is created, an open can be performed. The open is used to gain access to the same HeapBufMP instance. Generally an instance is created on one processor and opened on the other processor.

The open returns a HeapBufMP instance handle like the create, however the open does not initialize the shared memory. The supplied name is used to identify the created instance.

Call HeapBufMP_close when the opened instance is not longer needed.

Parameters:
[in]nameName of created HeapBufMP instance
[out]handlePtrPointer to HeapBufMP handle to be opened
Returns:
HeapBufMP status:
See also:
HeapBufMP_close()
Void HeapBufMP_Params_init ( HeapBufMP_Params params)

Initialize a HeapBufMP parameters struct.

Parameters:
[out]paramsPointer to creation parameters
See also:
HeapBufMP_create()
Void* HeapBufMP_alloc ( HeapBufMP_Handle  handle,
SizeT  size,
SizeT  align 
)

Allocate a block of memory of specified size and alignment.

The actual block returned may be larger than requested to satisfy alignment requirements. NULL is returned if the allocation fails.

HeapBufMP_alloc() will lock the heap using the HeapBufMP gate while it traverses the list of free blocks to find a large enough block for the request.

Guidelines for using large heaps and multiple alloc() calls.

  • If possible, allocate larger blocks first. Previous allocations of small memory blocks can reduce the size of the blocks available for larger memory allocations.
  • Realize that allocation can fail even if the heap contains a sufficient absolute amount of unallocated space. This is because the largest free memory block may be smaller than total amount of unallocated memory.
Parameters:
[in]handleHandle to previously created/opened instance.
[in]sizeSize to be allocated (in MADUs)
[in]alignAlignment for allocation (power of 2)
See also:
HeapBufMP_free()
Void HeapBufMP_free ( HeapBufMP_Handle  handle,
Ptr  block,
SizeT  size 
)

Frees a block of memory.

HeapBufMP_free() places the memory block specified by addr and size back into the free pool of the heap specified. The newly freed block is combined with any adjacent free blocks. The space is then available for future allocations.

HeapBufMP_free() will lock the heap using the HeapBufMP gate if one is specified or the system GateMP if not.

Parameters:
[in]handleHandle to previously created/opened instance.
[in]blockBlock of memory to be freed.
[in]sizeSize to be freed (in MADUs)
See also:
HeapBufMP_alloc()
Void HeapBufMP_getExtendedStats ( HeapBufMP_Handle  handle,
HeapBufMP_ExtendedStats stats 
)

Get extended memory statistics.

This function retrieves extended statistics for a HeapBufMP instance. Refer to HeapBufMP_ExtendedStats for more information regarding what information is returned.

In SYS/BIOS, HeapBufMP.trackAllocs needs to be set to 'true' in the configuration to get meaningful extended stats.

Parameters:
[in]handleHandle to previously created/opened instance.
[out]statsExtendedStats structure
See also:
HeapBufMP_getStats()
Void HeapBufMP_getStats ( HeapBufMP_Handle  handle,
Ptr  stats 
)

Get memory statistics.

Parameters:
[in]handleHandle to previously created/opened instance.
[out]statsMemory statistics structure
See also:
HeapBufMP_getExtendedStats()
Copyright 2013, Texas Instruments Incorporated