IPC API
3.00.03.28
|
Multiple processor gate that provides local and remote context protection.
A GateMP instance can be used to enforce both local and remote context context protection. That is, entering a GateMP can prevent preemption by another thread running on the same processor and simultaneously prevent a remote processor from entering the same gate. GateMP's are typically used to protect reads/writes to a shared resource, such as shared memory.
Creating a GateMP requires supplying the following configuration
In addition, the following parameters should be configured as necessary:
Once created, GateMP allows the gate to be opened on another processor using GateMP_open() and the name that was used in GateMP_create().
A GateMP can be entered and left using GateMP_enter() and GateMP_leave() like any other gate that implements the IGateProvider interface.
GateMP has the following proxies - RemoteSystemProxy, RemoteCustom1Proxy and RemoteCustom2Proxy which are automatically plugged with device-specific delegates that implement multiple processor mutexes using a variety of hardware mechanisms.
GateMP creates a default system gate whose handle may be obtained using GateMP_getDefaultRemote(). Most IPC modules typically use this gate by default if they require gates and no instance gate is configured by the user.
The GateMP header should be included in an application as follows:
Go to the source code of this file.
Data Structures | |
struct | GateMP_Params |
Structure defining parameters for the GateMP module. More... |
Macros | |
#define | GateMP_S_BUSY 2 |
The resource is still in use. | |
#define | GateMP_S_ALREADYSETUP 1 |
The module has been already setup. | |
#define | GateMP_S_SUCCESS 0 |
Operation is successful. | |
#define | GateMP_E_FAIL -1 |
Generic failure. | |
#define | GateMP_E_INVALIDARG -2 |
Argument passed to function is invalid. | |
#define | GateMP_E_MEMORY -3 |
Operation resulted in memory failure. | |
#define | GateMP_E_ALREADYEXISTS -4 |
The specified entity already exists. | |
#define | GateMP_E_NOTFOUND -5 |
Unable to find the specified entity. | |
#define | GateMP_E_TIMEOUT -6 |
Operation timed out. | |
#define | GateMP_E_INVALIDSTATE -7 |
Module is not initialized. | |
#define | GateMP_E_OSFAILURE -8 |
A failure occurred in an OS-specific call. | |
#define | GateMP_E_RESOURCE -9 |
Specified resource is not available. | |
#define | GateMP_E_RESTART -10 |
Operation was interrupted. Please restart the operation. |
Typedefs | |
typedef enum GateMP_LocalProtect | GateMP_LocalProtect |
A set of local context protection levels. | |
typedef enum GateMP_RemoteProtect | GateMP_RemoteProtect |
Type of remote Gate. | |
typedef struct GateMP_Object * | GateMP_Handle |
GateMP_Handle type. | |
typedef struct GateMP_Params | GateMP_Params |
Structure defining parameters for the GateMP module. |
Enumerations | |
enum | GateMP_LocalProtect { GateMP_LocalProtect_NONE = 0, GateMP_LocalProtect_INTERRUPT = 1, GateMP_LocalProtect_TASKLET = 2, GateMP_LocalProtect_THREAD = 3, GateMP_LocalProtect_PROCESS = 4 } |
A set of local context protection levels. More... | |
enum | GateMP_RemoteProtect { GateMP_RemoteProtect_NONE = 0, GateMP_RemoteProtect_SYSTEM = 1, GateMP_RemoteProtect_CUSTOM1 = 2, GateMP_RemoteProtect_CUSTOM2 = 3 } |
Type of remote Gate. More... |
Functions | |
Int | GateMP_close (GateMP_Handle *handlePtr) |
Close an opened gate. | |
GateMP_Handle | GateMP_create (const GateMP_Params *params) |
Create a GateMP instance. | |
Int | GateMP_delete (GateMP_Handle *handlePtr) |
Delete a created GateMP instance. | |
GateMP_Handle | GateMP_getDefaultRemote (Void) |
Get the default remote gate. | |
GateMP_LocalProtect | GateMP_getLocalProtect (GateMP_Handle handle) |
Get the local protection level configured in a GateMP instance. | |
GateMP_RemoteProtect | GateMP_getRemoteProtect (GateMP_Handle handle) |
Get the remote protection level configured in a GateMP instance. | |
Int | GateMP_open (String name, GateMP_Handle *handlePtr) |
Open a created GateMP by name. | |
Void | GateMP_Params_init (GateMP_Params *params) |
Initialize a GateMP parameters struct. | |
IArg | GateMP_enter (GateMP_Handle handle) |
Enter the GateMP. | |
Void | GateMP_leave (GateMP_Handle handle, IArg key) |
Leave the GateMP. |
#define GateMP_S_BUSY 2 |
The resource is still in use.
#define GateMP_S_ALREADYSETUP 1 |
The module has been already setup.
#define GateMP_S_SUCCESS 0 |
Operation is successful.
#define GateMP_E_FAIL -1 |
Generic failure.
#define GateMP_E_INVALIDARG -2 |
Argument passed to function is invalid.
#define GateMP_E_MEMORY -3 |
Operation resulted in memory failure.
#define GateMP_E_ALREADYEXISTS -4 |
The specified entity already exists.
#define GateMP_E_NOTFOUND -5 |
Unable to find the specified entity.
#define GateMP_E_TIMEOUT -6 |
Operation timed out.
#define GateMP_E_INVALIDSTATE -7 |
Module is not initialized.
#define GateMP_E_OSFAILURE -8 |
A failure occurred in an OS-specific call.
#define GateMP_E_RESOURCE -9 |
Specified resource is not available.
#define GateMP_E_RESTART -10 |
Operation was interrupted. Please restart the operation.
typedef enum GateMP_LocalProtect GateMP_LocalProtect |
A set of local context protection levels.
Each member corresponds to a specific local processor gates used for local protection.
For SYS/BIOS users, the following are the mappings for the constants
typedef enum GateMP_RemoteProtect GateMP_RemoteProtect |
Type of remote Gate.
Each member corresponds to a specific type of remote gate. Each enum value corresponds to the following remote protection levels:
typedef struct GateMP_Object* GateMP_Handle |
GateMP_Handle type.
typedef struct GateMP_Params GateMP_Params |
Structure defining parameters for the GateMP module.
enum GateMP_LocalProtect |
A set of local context protection levels.
Each member corresponds to a specific local processor gates used for local protection.
For SYS/BIOS users, the following are the mappings for the constants
enum GateMP_RemoteProtect |
Type of remote Gate.
Each member corresponds to a specific type of remote gate. Each enum value corresponds to the following remote protection levels:
GateMP_RemoteProtect_NONE |
No remote protection (the GateMP instance will exclusively offer local protection configured in GateMP_Params.localProtect) |
GateMP_RemoteProtect_SYSTEM |
Use the SYSTEM remote protection level (default remote protection) |
GateMP_RemoteProtect_CUSTOM1 |
Use the CUSTOM1 remote protection level |
GateMP_RemoteProtect_CUSTOM2 |
Use the CUSTOM2 remote protection level |
Int GateMP_close | ( | GateMP_Handle * | handlePtr | ) |
Close an opened gate.
[in,out] | handlePtr | Pointer to handle to opened GateMP instance |
GateMP_Handle GateMP_create | ( | const GateMP_Params * | params | ) |
Create a GateMP instance.
The params structure should be initialized using GateMP_Params_init().
[in] | params | GateMP parameters |
Int GateMP_delete | ( | GateMP_Handle * | handlePtr | ) |
Delete a created GateMP instance.
[in,out] | handlePtr | Pointer to GateMP handle |
GateMP_Handle GateMP_getDefaultRemote | ( | Void | ) |
Get the default remote gate.
GateMP_LocalProtect GateMP_getLocalProtect | ( | GateMP_Handle | handle | ) |
Get the local protection level configured in a GateMP instance.
GateMP_RemoteProtect GateMP_getRemoteProtect | ( | GateMP_Handle | handle | ) |
Get the remote protection level configured in a GateMP instance.
Int GateMP_open | ( | String | name, |
GateMP_Handle * | handlePtr | ||
) |
Open a created GateMP by name.
[in] | name | Name of the GateMP instance |
[out] | handlePtr | Pointer to GateMP handle to be opened |
Void GateMP_Params_init | ( | GateMP_Params * | params | ) |
Initialize a GateMP parameters struct.
[out] | params | Pointer to GateMP parameters |
IArg GateMP_enter | ( | GateMP_Handle | handle | ) |
Enter the GateMP.
[in] | handle | GateMP handle |
Void GateMP_leave | ( | GateMP_Handle | handle, |
IArg | key | ||
) |
Leave the GateMP.
[in] | handle | GateMP handle |
[in] | key | key returned from GateMP_enter |