![]() |
![]() |
Codec Engine Application Programming Interface (API)
ce-w08
|
![]() ![]() | Descriptor for an alg. This object can be passed to Engine_addAlg() , to dynamically add an alg to an engine |
![]() ![]() | Properties of an Engine algorithm |
![]() ![]() | Properties of an Engine algorithm |
![]() ![]() | Attributes of an Engine |
![]() ![]() | This structure is passed to Engine_add() , and contains parameters to specify an engine |
![]() ![]() | Descriptor for a dynamically loaded alg. A dynamic library for a codec must export a function that fills in a structure of this type |
![]() ![]() | Defines the fields and methods that must be supplied by all XDAIS algorithms |
![]() ![]() | Memory records |
![]() ![]() | Algorithm instance object definition |
![]() ![]() | Algorithm instance creation parameters |
![]() ![]() | Pointer to algorithm specific status structure |
![]() ![]() | This structure defines the codec parameters that can be modified after creation via control() calls |
![]() ![]() | Defines all of the operations on IAUDDEC1 objects |
![]() ![]() | Defines the input arguments for all IAUDDEC1 instance process function |
![]() ![]() | This must be the first field of all IAUDDEC1 instance objects |
![]() ![]() | Defines the run time output arguments for all IAUDDEC1 instance objects |
![]() ![]() | Defines the creation time parameters for all IAUDDEC1 instance objects |
![]() ![]() | Defines instance status parameters (read-only) |
![]() ![]() | This structure defines the codec parameters that can be modified after creation via control() calls |
![]() ![]() | Defines all of the operations on IAUDDEC objects |
![]() ![]() | Defines the input arguments for all IAUDDEC instance process function |
![]() ![]() | This must be the first field of all IAUDDEC instance objects |
![]() ![]() | Defines the run time output arguments for all IAUDDEC instance objects |
![]() ![]() | Defines the creation time parameters for all IAUDDEC instance objects |
![]() ![]() | Defines instance status parameters (read-only) |
![]() ![]() | This structure defines the algorithm parameters that can be modified after creation via control() calls |
![]() ![]() | Defines all of the operations on IAUDENC1 objects |
![]() ![]() | Defines the input arguments for all IAUDENC1 instance process function |
![]() ![]() | This must be the first field of all IAUDENC1 instance objects |
![]() ![]() | Defines the run time output arguments for all IAUDENC1 instance objects |
![]() ![]() | Defines the creation time parameters for all IAUDENC1 instance objects |
![]() ![]() | Defines instance status parameters (read-only) |
![]() ![]() | This structure defines the algorithm parameters that can be modified after creation via control() calls |
![]() ![]() | Defines all of the operations on IAUDENC objects |
![]() ![]() | Defines the input arguments for all IAUDENC instance process function |
![]() ![]() | This must be the first field of all IAUDENC instance objects |
![]() ![]() | Defines the run time output arguments for all IAUDENC instance objects |
![]() ![]() | Defines the creation time parameters for all IAUDENC instance objects |
![]() ![]() | Defines instance status parameters (read-only) |
![]() ![]() | Definition of IIMGDEC1 codec class configurable parameters |
![]() ![]() | This structure defines the codec parameters that can be modified after creation via control() calls |
![]() ![]() | Defines all of the operations on IIMGDEC1 objects |
![]() ![]() | Defines the input arguments for all IIMGDEC1 instance process() function |
![]() ![]() | This must be the first field of all IIMGDEC1 instance objects |
![]() ![]() | Defines the run time output arguments for all IIMGDEC1 instance objects |
![]() ![]() | Defines the creation time parameters for all IIMGDEC1 instance objects |
![]() ![]() | Defines instance status parameters |
![]() ![]() | Definition of IIMGDEC codec class configurable parameters |
![]() ![]() | This structure defines the codec parameters that can be modified after creation via control() calls |
![]() ![]() | Defines all of the operations on IIMGDEC objects |
![]() ![]() | Defines the input arguments for all IIMGDEC instance process() function |
![]() ![]() | This must be the first field of all IIMGDEC instance objects |
![]() ![]() | Defines the run time output arguments for all IIMGDEC instance objects |
![]() ![]() | Defines the creation time parameters for all IIMGDEC instance objects |
![]() ![]() | Defines instance status parameters (read-only) |
![]() ![]() | Definition of IIMGENC1 codec class configurable parameters |
![]() ![]() | This structure defines the algorithm parameters that can be modified after creation via control() calls |
![]() ![]() | Defines all of the operations on IIMGENC1 objects |
![]() ![]() | Defines the input arguments for all IIMGENC1 instance process() function |
![]() ![]() | This must be the first field of all IIMGENC1 instance objects |
![]() ![]() | Defines the run time output arguments for all IIMGENC1 instance objects |
![]() ![]() | Defines the creation time parameters for all IIMGENC1 instance objects |
![]() ![]() | Defines instance status parameters |
![]() ![]() | Definition of IIMGENC codec class configurable parameters |
![]() ![]() | This structure defines the algorithm parameters that can be modified after creation via control() calls |
![]() ![]() | Defines all of the operations on IIMGENC objects |
![]() ![]() | Defines the input arguments for all IIMGENC instance process() function |
![]() ![]() | This must be the first field of all IIMGENC instance objects |
![]() ![]() | Defines the run time output arguments for all IIMGENC instance objects |
![]() ![]() | Defines the creation time parameters for all IIMGENC instance objects |
![]() ![]() | Defines instance status parameters (read-only) |
![]() ![]() | This structure defines the codec parameters that can be modified after creation via ISPHDEC1_Fxns.control() |
![]() ![]() | Defines all of the operations on ISPHDEC1 objects |
![]() ![]() | Defines the input arguments for all ISPHDEC1 instance process function |
![]() ![]() | This must be the first field of all ISPHDEC1 instance objects |
![]() ![]() | Defines the run time output arguments for all ISPHDEC1 instance objects |
![]() ![]() | Defines the creation time parameters for all ISPHDEC1 instance objects |
![]() ![]() | Defines instance status parameters |
![]() ![]() | This structure defines the codec parameters that can be modified after creation via control() calls |
![]() ![]() | Defines all of the operations on ISPHDEC objects |
![]() ![]() | Defines the input arguments for all ISPHDEC instance process function |
![]() ![]() | This must be the first field of all ISPHDEC instance objects |
![]() ![]() | Defines the run time output arguments for all ISPHDEC instance objects |
![]() ![]() | Defines the creation time parameters for all ISPHDEC instance objects |
![]() ![]() | Defines instance status parameters (read-only) |
![]() ![]() | This structure defines the codec parameters that can be modified after creation via ISPHENC1_Fxns.control() |
![]() ![]() | Defines all of the operations on ISPHENC1 objects |
![]() ![]() | Defines the input arguments for all ISPHENC1 instance process function |
![]() ![]() | This must be the first field of all ISPHENC1 instance objects |
![]() ![]() | Defines the run time output arguments for all ISPHENC1 instance objects |
![]() ![]() | Defines the creation time parameters for all ISPHENC1 instance objects |
![]() ![]() | Defines instance status parameters |
![]() ![]() | This structure defines the codec parameters that can be modified after creation via control() calls |
![]() ![]() | Defines all of the operations on ISPHENC objects |
![]() ![]() | Defines the input arguments for all ISPHENC instance process function |
![]() ![]() | This must be the first field of all ISPHENC instance objects |
![]() ![]() | Defines the run time output arguments for all ISPHENC instance objects |
![]() ![]() | Defines the creation time parameters for all ISPHENC instance objects |
![]() ![]() | Defines instance status parameters (read-only) |
![]() ![]() | Definition of IUNIVERSAL codec class configurable parameters |
![]() ![]() | This structure defines the codec parameters that can be modified after creation via control() calls |
![]() ![]() | Defines all of the operations on IUNIVERSAL objects |
![]() ![]() | Defines the input arguments for all IUNIVERSAL instance process function |
![]() ![]() | This must be the first field of all IUNIVERSAL instance objects |
![]() ![]() | Defines the run time output arguments for all IUNIVERSAL instance objects |
![]() ![]() | Defines the creation time parameters for all IUNIVERSAL instance objects |
![]() ![]() | Defines instance status parameters (read-only) |
![]() ![]() | This structure defines the algorithm parameters that can be modified after creation via control() calls |
![]() ![]() | Defines all of the operations on IVIDANALYTICS objects |
![]() ![]() | Access modes used to declare how the algorithm accessed buffers |
![]() ![]() | Defines the input arguments for all IVIDANALYTICS instance process function |
![]() ![]() | This must be the first field of all IVIDANALYTICS instance objects |
![]() ![]() | Defines the run time output arguments for all IVIDANALYTICS instance objects |
![]() ![]() | Defines the creation time parameters for all IVIDANALYTICS instance objects |
![]() ![]() | Analytics rule |
![]() ![]() | Defines instance status parameters |
![]() ![]() | Definition of IVIDDEC1 codec class configurable parameters |
![]() ![]() | This structure defines the codec parameters that can be modified after creation via control() calls |
![]() ![]() | Defines all of the operations on IVIDDEC1 objects |
![]() ![]() | Defines the input arguments for all IVIDDEC1 instance process function |
![]() ![]() | This must be the first field of all IVIDDEC1 instance objects |
![]() ![]() | Defines the run time output arguments for all IVIDDEC1 instance objects |
![]() ![]() | Defines the creation time parameters for all IVIDDEC1 instance objects |
![]() ![]() | Defines instance status parameters |
![]() ![]() | Definition of IVIDDEC2 codec class configurable parameters |
![]() ![]() | This structure defines the codec parameters that can be modified after creation via control() calls |
![]() ![]() | Defines all of the operations on IVIDDEC2 objects |
![]() ![]() | Defines the input arguments for all IVIDDEC2 instance process function |
![]() ![]() | This must be the first field of all IVIDDEC2 instance objects |
![]() ![]() | Defines the run time output arguments for all IVIDDEC2 instance objects |
![]() ![]() | Defines the creation time parameters for all IVIDDEC2 instance objects |
![]() ![]() | Defines instance status parameters |
![]() ![]() | Definition of IVIDDEC2BACK codec class configurable parameters |
![]() ![]() | Defines all of the operations on IVIDDEC2BACK objects |
![]() ![]() | This must be the first field of all IVIDDEC2BACK instance objects |
![]() ![]() | Defines all of the operations on IVIDDEC2FRONT objects |
![]() ![]() | This must be the first field of all IVIDDEC2FRONT instance objects |
![]() ![]() | Defines the run time output arguments for all IVIDDEC2FRONT instance objects |
![]() ![]() | Defines instance status parameters |
![]() ![]() | Definition of IVIDDEC3 codec class configurable parameters |
![]() ![]() | This structure defines the algorithm parameters that can be modified after creation via IVIDDEC3_Fxns.control() calls |
![]() ![]() | Defines all of the operations on IVIDDEC3 objects |
![]() ![]() | Defines the input arguments for all IVIDDEC3 instance process function |
![]() ![]() | This must be the first field of all IVIDDEC3 instance objects |
![]() ![]() | Defines the run time output arguments for all IVIDDEC3 instance objects |
![]() ![]() | Defines the creation time parameters for all IVIDDEC3 instance objects |
![]() ![]() | Defines instance status parameters |
![]() ![]() | Definition of VIDDEC codec class configurable parameters |
![]() ![]() | This structure defines the codec parameters that can be modified after creation via control() calls |
![]() ![]() | Defines all of the operations on IVIDDEC objects |
![]() ![]() | Defines the input arguments for all IVIDDEC instance process function |
![]() ![]() | This must be the first field of all IVIDDEC instance objects |
![]() ![]() | Defines the run time output arguments for all IVIDDEC instance objects |
![]() ![]() | Defines the creation time parameters for all IVIDDEC instance objects |
![]() ![]() | Defines instance status parameters |
![]() ![]() | Definition of IVIDENC1 codec class configurable parameters |
![]() ![]() | This structure defines the algorithm parameters that can be modified after creation via control() calls |
![]() ![]() | Defines all of the operations on IVIDENC1 objects |
![]() ![]() | Defines the input arguments for all IVIDENC1 instance process function |
![]() ![]() | Defines the structure that contains macroblock related encoding parameter estimates |
![]() ![]() | This must be the first field of all IVIDENC1 instance objects |
![]() ![]() | Defines the run time output arguments for all IVIDENC1 instance objects |
![]() ![]() | Defines the creation time parameters for all IVIDENC1 instance objects |
![]() ![]() | Defines instance status parameters |
![]() ![]() | Definition of IVIDENC2 codec class configurable parameters |
![]() ![]() | This structure defines the algorithm parameters that can be modified after creation via control() calls |
![]() ![]() | Defines all of the operations on IVIDENC2 objects |
![]() ![]() | Defines the input arguments for all IVIDENC2 instance process function |
![]() ![]() | This must be the first field of all IVIDENC2 instance objects |
![]() ![]() | Defines the run time output arguments for all IVIDENC2 instance objects |
![]() ![]() | Defines the creation time parameters for all IVIDENC2 instance objects |
![]() ![]() | Defines instance status parameters |
![]() ![]() | Definition of IVIDENC codec class configurable parameters |
![]() ![]() | This structure defines the codec parameters that can be modified after creation via control() calls |
![]() ![]() | Defines all of the operations on IVIDENC objects |
![]() ![]() | Defines the input arguments for all IVIDENC instance process function |
![]() ![]() | This must be the first field of all IVIDENC instance objects |
![]() ![]() | Defines the run time output arguments for all IVIDENC instance objects |
![]() ![]() | Defines the creation time parameters for all IVIDENC instance objects |
![]() ![]() | Defines instance status parameters |
![]() ![]() | Detailed buffer descriptor for video buffers |
![]() ![]() | Buffer descriptor for input video buffers |
![]() ![]() | Detailed buffer descriptor for video buffers |
![]() ![]() | Buffer descriptor for video buffers |
![]() ![]() | This structure defines the codec parameters that can be modified after creation via control() calls |
![]() ![]() | Defines all of the operations on IVIDTRANSCODE objects |
![]() ![]() | Defines the input arguments for all IVIDTRANSCODE instance process function |
![]() ![]() | This must be the first field of all IVIDTRANSCODE instance objects |
![]() ![]() | Defines the run time output arguments for all IVIDTRANSCODE instance objects |
![]() ![]() | Defines the creation time parameters for all IVIDTRANSCODE instance objects |
![]() ![]() | Defines instance status parameters |
![]() ![]() | |
![]() ![]() | Information for a memory heap of a remote DSP server |
![]() ![]() | Parameters for ti_sdo_ce_osal_Memory_alloc() & ti_sdo_ce_osal_Memory_free() |
![]() ![]() | VISA message header |
![]() ![]() | |
![]() ![]() | Buffer information descriptor for input and output buffers |
![]() ![]() | Buffer descriptor |
![]() ![]() | Single buffer descriptor |
![]() ![]() | Buffer descriptor |
![]() ![]() | Union describing a buffer size |
![]() ![]() | Descriptor for a buffer to move |
![]() ![]() | Single buffer descriptor |
![]() ![]() | Buffer information descriptor for input and output buffers |
![]() ![]() | Buffer descriptor for multiple buffers |
![]() ![]() | Context used by split codecs |
![]() ![]() | Buffer information descriptor for input and output buffers |
![]() ![]() | Descriptor for the chunk of data being transferred in one call to putData or getData |
![]() ![]() | Date and time |
![]() ![]() | 2-dimensional point |
![]() ![]() | Rectangle |
![]() ![]() | Single buffer descriptor |