![]() |
![]() |
Data Structures | |
struct | Engine_Attrs |
Attributes of an Engine. More... | |
struct | Engine_AlgInfo |
Properties of an Engine algorithm. More... | |
struct | Engine_DllAlgDesc |
Discriptor for a dynamically loaded codec. A dynamic library for a codec must export a function that fills in a structure of this type. More... | |
struct | Engine_DllAlgParams |
This structure is passed to Engine_addAlg() , and contains parameters to create a dynamic codec with. More... | |
Defines | |
#define | Engine_MODNAME "ti.sdo.ce.Engine" |
Name to pass to Diags_setMask() to enable logging for Engine functions. For example, Diags_setMask(Engine_MODNAME"+EX1234567"); turns on all Log statements in this module. Diags_setMask() must be called after initialization to take effect. | |
#define | Engine_EOK 0 |
#define | Engine_EEXIST 1 |
#define | Engine_ENOMEM 2 |
#define | Engine_EDSPLOAD 3 |
#define | Engine_ENOCOMM 4 |
#define | Engine_ENOSERVER 5 |
#define | Engine_ECOMALLOC 6 |
#define | Engine_ERUNTIME 7 |
#define | Engine_ECODECCREATE 8 |
#define | Engine_ECODECSTART 9 |
#define | Engine_EINVAL 10 |
#define | Engine_EBADSERVER 11 |
#define | Engine_ENOTAVAIL 12 |
#define | Engine_EWRONGSTATE 13 |
#define | Engine_EINUSE 14 |
#define | Engine_ENOTFOUND 15 |
#define | Engine_ETIMEOUT 16 |
#define | Engine_GETALGDESCFXN "GetEngineAlgDesc" |
Name of function that a dynamically loaded codec must supply. | |
Typedefs | |
typedef struct Engine_Obj * | Engine_Handle |
Opaque handle to an engine. | |
typedef Int | Engine_Error |
Engine error code. | |
typedef struct Engine_Attrs | Engine_Attrs |
Attributes of an Engine. | |
typedef struct Engine_AlgInfo | Engine_AlgInfo |
Properties of an Engine algorithm. | |
typedef struct Engine_DllAlgDesc | Engine_DllAlgDesc |
Discriptor for a dynamically loaded codec. A dynamic library for a codec must export a function that fills in a structure of this type. | |
typedef Int(* | Engine_GetAlgDescFxn )(Engine_DllAlgDesc *dllAlgDesc) |
Prototype of function that must be supplied by a dynamic codec library to fill in a Engine_DllAlgDesc structure. | |
typedef struct Engine_DllAlgParams | Engine_DllAlgParams |
This structure is passed to Engine_addAlg() , and contains parameters to create a dynamic codec with. | |
Functions | |
Void | CERuntime_exit (Void) |
Exit the Codec Engine Runtime. | |
Void | CERuntime_init (Void) |
Initialize the Codec Engine Runtime. | |
Engine_Error | Engine_add (String engineName, String remoteName) |
Add an Engine to the database of engines that can be opened with Engine_open() | |
Engine_Error | Engine_addAlg (Engine_Handle engine, String location, Engine_DllAlgParams *pAlgParams) |
Dynamically add an algorithm to an Engine instance. | |
Engine_Error | Engine_removeAlg (Engine_Handle engine, String name) |
Dynamically remove an algorithm from an Engine instance. | |
Void | Engine_close (Engine_Handle engine) |
Close an Engine. | |
Engine_Handle | Engine_open (String name, Engine_Attrs *attrs, Engine_Error *ec) |
Open an Engine. | |
Int | Engine_fwriteTrace (Engine_Handle engine, String prefix, FILE *out) |
Write Server's trace buffer to specifed file stream. | |
Engine_Error | Engine_getAlgInfo (String name, Engine_AlgInfo *algInfo, Int index) |
Get details of an algorithm configured into an engine. | |
Int | Engine_getCpuLoad (Engine_Handle engine) |
Get Server's cpu usage in percent. | |
Engine_Error | Engine_getLastError (Engine_Handle engine) |
Get error code of the last failed operation. | |
String | Engine_getName (Engine_Handle engine) |
Get the name of an opened engine. | |
Engine_Error | Engine_getNumAlgs (String name, Int *numAlgs) |
Get the number of algorithms configured into an Engine. | |
Server_Handle | Engine_getServer (Engine_Handle engine) |
Get handle to an Engine's Server. | |
UInt32 | Engine_getUsedMem (Engine_Handle engine) |
Get Server's total memory usage. | |
Engine_Error | Engine_remove (String engineName) |
Remove an engine from the list of engines that can be opened. | |
Int | Engine_setTrace (Engine_Handle engine, String mask) |
Set Server's trace mask. | |
Variables | |
Engine_Attrs | Engine_ATTRS |
Default engine attributes. |
#define Engine_MODNAME "ti.sdo.ce.Engine" |
Name to pass to Diags_setMask() to enable logging for Engine functions. For example, Diags_setMask(Engine_MODNAME"+EX1234567"); turns on all Log statements in this module. Diags_setMask() must be called after initialization to take effect.
#define Engine_EOK 0 |
Success.
#define Engine_EEXIST 1 |
Name does not exist.
#define Engine_ENOMEM 2 |
Unable to allocate memory.
#define Engine_EDSPLOAD 3 |
Unable to load the DSP.
#define Engine_ENOCOMM 4 |
Unable to create a comm connection to the DSP.
#define Engine_ENOSERVER 5 |
Unable to locate the server on the DSP.
#define Engine_ECOMALLOC 6 |
Unable to allocate communication buffer.
#define Engine_ERUNTIME 7 |
Internal engine runtime failure.
#define Engine_ECODECCREATE 8 |
Creation of the Codec failed.
#define Engine_ECODECSTART 9 |
Start of the Codec failed. For codecs which are implemented as a thread, this implies that the codec thread of execution failed to start.
#define Engine_EINVAL 10 |
Bad paramater passed to method.
#define Engine_EBADSERVER 11 |
Incompatible server specified.
#define Engine_ENOTAVAIL 12 |
Service not available.
#define Engine_EWRONGSTATE 13 |
Call can not be made at this time.
#define Engine_EINUSE 14 |
Call can't be made at this time because a required name/resource is in use.
#define Engine_ENOTFOUND 15 |
Entity was not found.
#define Engine_ETIMEOUT 16 |
Timeout-based operation timed out.
#define Engine_GETALGDESCFXN "GetEngineAlgDesc" |
Name of function that a dynamically loaded codec must supply.
typedef struct Engine_Obj* Engine_Handle |
Opaque handle to an engine.
typedef Int Engine_Error |
Engine error code.
typedef struct Engine_Attrs Engine_Attrs |
Attributes of an Engine.
typedef struct Engine_AlgInfo Engine_AlgInfo |
Properties of an Engine algorithm.
typedef struct Engine_DllAlgDesc Engine_DllAlgDesc |
Discriptor for a dynamically loaded codec. A dynamic library for a codec must export a function that fills in a structure of this type.
typedef Int(* Engine_GetAlgDescFxn)(Engine_DllAlgDesc *dllAlgDesc) |
Prototype of function that must be supplied by a dynamic codec library to fill in a Engine_DllAlgDesc
structure.
Engine_addAlg()
to fill in the dynamic codec's descriptor.typedef struct Engine_DllAlgParams Engine_DllAlgParams |
This structure is passed to Engine_addAlg()
, and contains parameters to create a dynamic codec with.
Void CERuntime_exit | ( | Void | ) |
Exit the Codec Engine Runtime.
Void CERuntime_init | ( | Void | ) |
Initialize the Codec Engine Runtime.
Engine_Error Engine_add | ( | String | engineName, |
String | remoteName | ||
) |
Add an Engine to the database of engines that can be opened with Engine_open()
[in] | engineName | The name of the engine to create. This must not be NULL. |
[in] | remoteName | The name of the remote server to load (if any). |
Engine_EINVAL | Bad parameter passed. |
Engine_EINUSE | An engine with the given name already exists. |
Engine_ENOMEM | A memory allocation failed. |
Engine_EOK | Success. |
engineName
.Engine_Error Engine_addAlg | ( | Engine_Handle | engine, |
String | location, | ||
Engine_DllAlgParams * | pAlgParams | ||
) |
Dynamically add an algorithm to an Engine instance.
[in] | engine | The handle to an engine, previously acquired by a call to Engine_open(). |
[in] | location | String identifying the location of the algorithm. Often this is a file name, but for systems without a file system, it may be a system-specific string identifier. |
[in] | pAlgParams | Parameters describing the algorithm being added. |
engine
is a valid (non-NULL) engine handle which is in the open state.name
, an error will be returned.Engine_EOK | Success. |
Engine_EINUSE | attrs.name is in use. |
Engine_Error Engine_removeAlg | ( | Engine_Handle | engine, |
String | name | ||
) |
Dynamically remove an algorithm from an Engine instance.
[in] | engine | The handle to an engine, previously acquired by a call to Engine_open(). |
[in] | name | Name of the algorithm to remove. |
Engine_EOK | Success. |
Engine_ENOTFOUND | name could not be found in engine . |
Void Engine_close | ( | Engine_Handle | engine ) |
Close an Engine.
[in] | engine | The handle to an engine, previously acquired by a call to Engine_open(). |
engine
must not be referenced by any algorithm instance objects; i.e., you must first delete all algorithm instances associated with engine
before closing it.engine
is a valid (non-NULL) engine handle which is in the open state. Engine_Handle Engine_open | ( | String | name, |
Engine_Attrs * | attrs, | ||
Engine_Error * | ec | ||
) |
Open an Engine.
The handle returned may be used to create one or more instances of an algorithm contained in the specified Engine.
An Engine may be opened more than once; each open returns a unique handle that can be used to create algorithm instances or get status of the Engine.
Engine handles must not be concurrently accessed by multiple threads; each thread must either obtain its own handle (via Engine_open()) or explicitly serialize access to a shared handle.
[in] | name | The name of the engine to open. name is specified in the engine configuration. |
[in] | attrs | Attributes for the open engine. |
[out] | ec | Optional output error code |
NULL | An error has occurred. |
non-NULL | The handle to the opened engine. |
name
is a non-NULL string.name
is a valid, pre-configured name of an engine.ec
is non-NULL, *ec
is set to a non-zero value indicating the cause of the failure.ec
is non-NULL, the Engine_Error value is set to one of the following values:Int Engine_fwriteTrace | ( | Engine_Handle | engine, |
String | prefix, | ||
FILE * | out | ||
) |
Write Server's trace buffer to specifed file stream.
[in] | engine | The handle to the opened engine. |
[in] | prefix | A string to prepend to each line output; this allows one to easily identify trace from the server from the application's trace, for example. |
[in] | out | A open FILE stream used to output the Server's trace characters. |
Integer | number of characters copied to the specified FILE stream. |
engine
is a valid (non-NULL) engine handle and the engine is in the open state.Engine_Error Engine_getAlgInfo | ( | String | name, |
Engine_AlgInfo * | algInfo, | ||
Int | index | ||
) |
Get details of an algorithm configured into an engine.
[in] | name | The name of the engine. name is specified in the engine configuration. |
[out] | algInfo | Structure to store algorithm details. The algInfoSize field of this structure must be set to sizeof(Engine_AlgInfo) by the application. |
[out] | index | The index of the algorithm to get the information. |
Engine_EOK | Success. |
Engine_EEXIST | There is no engine with the given name. |
Engine_ENOTFOUND | index is greater than or equal to the total number of algorithms configured for the engine, or index < 0. |
Engine_EINVAL | The value of algInfoSize passed to this function does not match the CE library's sizeof(Engine_AlgInfo) . |
name
is a non-NULL string.algInfo
is non-NULL.name
is a valid engine name and 0 <= index
< the total number of algorithms configured for the engine, then algInfo
will contain the information for the engine's ith (i = index
) algorithm.Int Engine_getCpuLoad | ( | Engine_Handle | engine ) |
Get Server's cpu usage in percent.
[in] | engine | The handle to the opened engine. |
integer | between 0-100 indicating percentage of time the Server is processing measured over a period of approximately 1 second. If the load is unavailable, a negative value is returned. |
engine
is a valid (non-NULL) engine handle and the engine is in the open state.Engine_Error Engine_getLastError | ( | Engine_Handle | engine ) |
Get error code of the last failed operation.
[in] | engine | The handle to the opened engine. |
error | code (Engine_Error) of the last failed engine operation. |
engine
is a valid (non-NULL) engine handle and the engine is in the open state. String Engine_getName | ( | Engine_Handle | engine ) |
Get the name of an opened engine.
[in] | engine | The handle to the opened engine. |
NULL | An error has occurred. |
non-NULL | The name of the opened engine. |
Engine_Error Engine_getNumAlgs | ( | String | name, |
Int * | numAlgs | ||
) |
Get the number of algorithms configured into an Engine.
[in] | name | The name of the Engine. name is specified in the engine configuration. |
[out] | numAlgs | The number of algorithms that are configured in the given engine. |
Engine_EOK | Success. |
Engine_EEXIST | There is no engine with the given name. |
name
is a non-NULL string.numAlgs
is non-NULL.name
is a valid engine name, then numAlgs will contain the number of algorithms configured for the given engine.Server_Handle Engine_getServer | ( | Engine_Handle | engine ) |
Get handle to an Engine's Server.
This function returns the handle to an Engines server, that can be used with Server APIs to obtain information from and control the remote DSP server.
[in] | engine | The handle to the opened engine. |
Handle | to engine's server. |
engine
is a valid (non-NULL) engine handle and the engine is in the open state. UInt32 Engine_getUsedMem | ( | Engine_Handle | engine ) |
Get Server's total memory usage.
[in] | engine | The handle to the opened engine. |
Total | amount of used memory (in MAUs). If the amount is not available, 0 is returned and the reason can be retrieved via Engine_getLastError(). |
engine
is a valid (non-NULL) engine handle and the engine is in the open state.Engine_Error Engine_remove | ( | String | engineName ) |
Remove an engine from the list of engines that can be opened.
[in] | engineName | The name of the engine to be removed. |
engineName
is non-NULL.Engine_EINUSE | The engine cannot be removed because an instance of it is still opened. |
Engine_EEXIST | No engine by this name exists. |
Engine_EOK | Success. |
Int Engine_setTrace | ( | Engine_Handle | engine, |
String | mask | ||
) |
Set Server's trace mask.
[in] | engine | The handle to the opened engine. |
[in] | mask | Trace mask, e.g. "*=01234567" |
Engine_ENOSERVER | No server for this engine. |
Engine_EINUSE | Trace resource is already in use. |
Engine_ERUNTIME | Internal runtime error has occurred. |
engine
is a valid (non-NULL) engine handle and the engine is in the open state.Default engine attributes.
Default attrs.