OP-TEE ======================================== .. rubric:: Overview OP-TEE is a Trusted Execution Environment (TEE) designed as companion to a non-secure Linux kernel running on Arm; Cortex-A cores using the TrustZone technology. OP-TEE implements TEE Internal Core API v1.1.x which is the API exposed to Trusted Applications and the TEE Client API v1.0, which is the API describing how to communicate with a TEE. Those APIs are defined in the GlobalPlatform API specifications. .. rubric:: Getting the OP-TEE Source Code :: $ git clone https://github.com/OP-TEE/optee_os.git .. rubric:: Building OP-TEE :: $ make CROSS_COMPILE64=aarch64-linux-gnu- PLATFORM=k3 CFG_ARM64_core=y all