€cdocutils.nodes document q)�q}q(U nametypesq}q(Xgplv3 disclaimerqNX*how-to-remove-target-side-gplv3-componentsqˆX$how-to-identify-the-gplv3-componentsqˆuUsubstitution_defsq }q Uparse_messagesq ]q Ucurrent_sourceq NU decorationqNUautofootnote_startqKUnameidsq}q(hUgplv3-disclaimerqhU*how-to-remove-target-side-gplv3-componentsqhU$how-to-identify-the-gplv3-componentsquUchildrenq]qcdocutils.nodes section q)�q}q(U rawsourceqUUparentqhUsourceqcdocutils.nodes reprunicode qXBsource/linux/Overview/Processor_SDK_Linux_GPLv3_Disclaimer.rst.incq…�q}q bUtagnameq!Usectionq"U attributesq#}q$(Udupnamesq%]Uclassesq&]Ubackrefsq']Uidsq(]q)haUnamesq*]q+hauUlineq,KUdocumentq-hh]q.(cdocutils.nodes title q/)�q0}q1(hXGPLv3 Disclaimerq2hhhhh!Utitleq3h#}q4(h%]h&]h']h(]h*]uh,Kh-hh]q5cdocutils.nodes Text q6XGPLv3 Disclaimerq7…�q8}q9(hh2hh0ubaubcdocutils.nodes comment q:)�q;}q<(hXLhttp://processors.wiki.ti.com/index.php/Processor_SDK_Linux_GPLv3_Disclaimerhhhhh!Ucommentq=h#}q>(U xml:spaceq?Upreserveq@h(]h']h%]h&]h*]uh,Kh-hh]qAh6XLhttp://processors.wiki.ti.com/index.php/Processor_SDK_Linux_GPLv3_DisclaimerqB…�qC}qD(hUhh;ubaubcdocutils.nodes paragraph qE)�qF}qG(hXIThere are GPLv3 licensed software components contained within the Processor SDK for Linux on both the target and the host.  The software manifest (software\_manifest.htm) for the Linux SDK is located in the docs/ directory of the installed SDK.  All GPLv3 components for both target and host are contained in the SDK directory.hhhhh!U paragraphqHh#}qI(h%]h&]h']h(]h*]uh,Kh-hh]qJh6XHThere are GPLv3 licensed software components contained within the Processor SDK for Linux on both the target and the host.  The software manifest (software_manifest.htm) for the Linux SDK is located in the docs/ directory of the installed SDK.  All GPLv3 components for both target and host are contained in the SDK directory.qK…�qL}qM(hXIThere are GPLv3 licensed software components contained within the Processor SDK for Linux on both the target and the host.  The software manifest (software\_manifest.htm) for the Linux SDK is located in the docs/ directory of the installed SDK.  All GPLv3 components for both target and host are contained in the SDK directory.hhFubaubcdocutils.nodes warning qN)�qO}qP(hXnThese GPLv3 components are provided for development purposes only and may be removed for production solutions.hhhhh!UwarningqQh#}qR(h%]h&]h']h(]h*]uh,Nh-hh]qShE)�qT}qU(hXnThese GPLv3 components are provided for development purposes only and may be removed for production solutions.qVhhOhhh!hHh#}qW(h%]h&]h']h(]h*]uh,K h]qXh6XnThese GPLv3 components are provided for development purposes only and may be removed for production solutions.qY…�qZ}q[(hhVhhTubaubaubcdocutils.nodes rubric q\)�q]}q^(hX$How to Identify the GPLv3 componentsq_hhhhh!Urubricq`h#}qa(h(]qbhah']h%]h&]h*]qchauh,Nh-hh]qdh6X$How to Identify the GPLv3 componentsqe…�qf}qg(hh_hh]ubaubhE)�qh}qi(hX®To idenitfy the GPLv3 components installed on the target file system, run the gplv3-notice script located on the target file system located here: **/etc/init.d/gplv3-notice**hhhhh!hHh#}qj(h%]h&]h']h(]h*]uh,Kh-hh]qk(h6X’To idenitfy the GPLv3 components installed on the target file system, run the gplv3-notice script located on the target file system located here: ql…�qm}qn(hX’To idenitfy the GPLv3 components installed on the target file system, run the gplv3-notice script located on the target file system located here: hhhubcdocutils.nodes strong qo)�qp}qq(hX**/etc/init.d/gplv3-notice**h#}qr(h%]h&]h']h(]h*]uhhhh]qsh6X/etc/init.d/gplv3-noticeqt…�qu}qv(hUhhpubah!UstrongqwubeubhE)�qx}qy(hXÇThe gplv3-notice script will list all Processor SDK Linux installed packages as shipped.  If you installed additional GPLv3 components this script may not identify them until the next target reboot.qzhhhhh!hHh#}q{(h%]h&]h']h(]h*]uh,Kh-hh]q|h6XÇThe gplv3-notice script will list all Processor SDK Linux installed packages as shipped.  If you installed additional GPLv3 components this script may not identify them until the next target reboot.q}…�q~}q(hhzhhxubaubcdocutils.nodes line_block q€)�q�}q‚(hUhhhhh!U line_blockqƒh#}q„(h%]h&]h']h(]h*]uh,Kh-hh]q…cdocutils.nodes line q†)�q‡}qˆ(hUUindentq‰Khh�hhh!h,h#}qŠ(h%]h&]h']h(]h*]uh,Kh-hh]ubaubh\)�q‹}qŒ(hX*How to Remove Target side GPLv3 Componentsq�hhhhh!h`h#}qŽ(h(]q�hah']h%]h&]h*]q�hauh,Nh-hh]q‘h6X*How to Remove Target side GPLv3 Componentsq’…�q“}q”(hh�hh‹ubaubhE)�q•}q–(hXÉThe gplv3-notice script also outputs how to remove the packages.  To remove individual packages from the target development file system, use the opkg remove command which is: **opkg remove **hhhhh!hHh#}q—(h%]h&]h']h(]h*]uh,K h-hh]q˜(h6X°The gplv3-notice script also outputs how to remove the packages.  To remove individual packages from the target development file system, use the opkg remove command which is: q™…�qš}q›(hX°The gplv3-notice script also outputs how to remove the packages.  To remove individual packages from the target development file system, use the opkg remove command which is: hh•ubho)�qœ}q�(hX**opkg remove **h#}qž(h%]h&]h']h(]h*]uhh•h]qŸh6Xopkg remove q …�q¡}q¢(hUhhœubah!hwubeubeubahUU transformerq£NU footnote_refsq¤}q¥Urefnamesq¦}q§Usymbol_footnotesq¨]q©Uautofootnote_refsqª]q«Usymbol_footnote_refsq¬]q­U citationsq®]q¯h-hU current_lineq°NUtransform_messagesq±]q²Ureporterq³NUid_startq´KU autofootnotesqµ]q¶U citation_refsq·}q¸Uindirect_targetsq¹]qºUsettingsq»(cdocutils.frontend Values q¼oq½}q¾(Ufootnote_backlinksq¿KUrecord_dependenciesqÀNU rfc_base_urlqÁUhttps://tools.ietf.org/html/qÂU tracebackqÈUpep_referencesqÄNUstrip_commentsqÅNU toc_backlinksqÆUentryqÇU language_codeqÈUenqÉU datestampqÊNU report_levelqËKU _destinationqÌNU halt_levelqÍKU strip_classesqÎNh3NUerror_encoding_error_handlerqÏUbackslashreplaceqÐUdebugqÑNUembed_stylesheetqÒ‰Uoutput_encoding_error_handlerqÓUstrictqÔU sectnum_xformqÕKUdump_transformsqÖNU docinfo_xformq×KUwarning_streamqØNUpep_file_url_templateqÙUpep-%04dqÚUexit_status_levelqÛKUconfigqÜNUstrict_visitorqÝNUcloak_email_addressesqÞˆUtrim_footnote_reference_spaceq߉UenvqàNUdump_pseudo_xmlqáNUexpose_internalsqâNUsectsubtitle_xformqã‰U source_linkqäNUrfc_referencesqåNUoutput_encodingqæUutf-8qçU source_urlqèNUinput_encodingqéU utf-8-sigqêU_disable_configqëNU id_prefixqìUU tab_widthqíKUerror_encodingqîUUTF-8qïU_sourceqðXY/home/gtbldadm/nightlybuilds/processor-sdk-doc/source/linux/Overview_GPLv3_Disclaimer.rstqñUgettext_compactqòˆU generatorqóNUdump_internalsqôNU smart_quotesqõ‰U pep_base_urlqöU https://www.python.org/dev/peps/q÷Usyntax_highlightqøUlongqùUinput_encoding_error_handlerqúhÔUauto_id_prefixqûUidqüUdoctitle_xformqý‰Ustrip_elements_with_classesqþNU _config_filesqÿ]rUfile_insertion_enabledrˆU raw_enabledrKU dump_settingsrNubUsymbol_footnote_startrKUidsr}r(hh‹hhhh]uUsubstitution_namesr}rh!h-h#}r (h%]h(]h']Usourcehñh&]h*]uU footnotesr ]r Urefidsr }r ub.