2.3. Yocto Layer ConfigurationΒΆ
Processor SDK uses the following oe-layersetup configs to configure the meta layers. These are the <config> used in the command:
$ ./oe-layersetup.sh -f <config>
The following config files are located in the configs/processor-sdk
directory of the oe-layersetup git repo.
| Config File | Description | Supported machines/platforms |
|---|---|---|
| processor-sdk-05.02.00.10-config.txt | Processor SDK 5.2.0.10 Release | am335x-evm, am437x-evm, am57xx-evm, am65xx-evm, k2hk-evm, k2e-evm, k2l-evm, k2g-evm, omapl138-lcdk |