2.1. Release Notes¶
2.1.1. Overview¶
The Processor Software Development Kit (Processor-SDK) for Linux provides a fundamental software platform for development, deployment and execution of Linux based applications and includes the following:
- Bootloaders & Filesystems
- SDK Installer
- Setup Scripts
- Makefiles
- Matrix Application Launcher
- Example Applications
- WLAN support (Wilink 8)
- Code Composer Studio
2.1.2. Licensing¶
Please refer to the software manifest, which outlines the licensing status for all packages included in this release. The manifest can be found on the SDK download page. The manifest can be found on the SDK download page or in the installed directory as indicated below. In addition, see PLSDK GPLv3 Disclaimer
2.1.3. Documentation¶
- Processor SDK Linux Software Developer’s Guide: Provides information on features, functions, delivery package and, compile tools for the Processor SDK Linux release. This also provides detailed information regarding software elements and software infrastructure to allow developers to start creating applications.
- Processor SDK Linux Getting Started Guide: Provides information on getting the software and running examples/demonstrations bundled in the SDK.
- Software Manifest: Provides license information on software
included in the SDK release. This document is in the release at
[INSTALL-DIR]/docs. - EVM Quick Start Guide: Provides information on hardware setup and running the demonstration application that is loaded on flash. This document is provided as part of the EVM kit.
2.1.4. Release 05.01.00¶
Released October 2018
What’s New
Processor SDK Linux now supports AM65x family of devices, in addition to AM335x, AM437x, AM57x, K2H, K2E, K2L, K2G and OMAP-L138.
New platforms: AM65x Evaluation Module (TMDX654GPEVM), AM65x Industrial Development Kit (TMDX654IDKEVM)
- AM65x
- Features supported
- Boot: please refer to U-Boot for AM65x
- Baseport: Dual and Quad Core SMP support
- Connectivity: OSPI, MMC, CPSW, CIFS, USB host and client driver, UART, I2C, USB device, PRU Ethernet, SD card
- Audio: McASP, stereo, playback and record
- Graphics: 3D SGX Acceleration with Qt, Wayland/Weston, Matrix GUI
- Display: DSS, touchscreen, DRM, LCD backlight
- IPC: Hardware spinlocks and mailbox, R5F remoteproc
- DDR @ 1333 MHz, and CPU @ 800 MHz configuration
- Features not (yet) supported
- PCIe, USB 3.0
- Deep Learning
- AM57xx: TIDL performance optimizations: Concurrent processing on all 4 cores: 2xDSP + 2xEVE
- Port ARM NN inference engine to AM335x, AM437x, AM57xx. For more information on ARMNN, see here
- HSR/PRP
- Dual Instance support on the two PRU-ICSS on AM571x
- Support VLAN tag in supervision frames.
- Extend HSR/PRP support to AM335x, AM437x, K2G from AM57xx (Note: PTP SAN is supported only on AM57xx in this release)
- New TI Designs (available as part of Processor SDK Linux)
OpenCV Performance optimizatons: StereoBM with C66x offload
SDK Components & Versions
| Component | Version |
|---|---|
| Linux Kernel | 4.14.67+ (2018 LTS) |
| U-Boot | 2018.01 |
| Yocto Project | 2.4 (rocko) |
| Linaro Toolchain (gcc) | 7.2-2017.11 hard-float |
| Qt | 5.9.6 |
| OpenCL | 1.1.16 |
| OpenCV | 3.1 |
| Wayland | 1.13 |
| GStreamer | 1.12.2 |
| Chromium | v53 |
| TI PRU Compiler | 2.2.1 |
| TI C66x CGT Compiler | 8.2.2 |
2.1.5. Supported Platforms¶
See here for a list of supported platforms and links to more information.
2.1.6. Build Information¶
2.1.6.1. U-Boot¶
2.1.6.2. Kernel¶
Linux Kernel
Real Time (RT) Linux Kernel
Generic Kernel Release Notes
2.1.7. Issues Tracker¶
2.1.7.1. Issues opened in previous releases that were closed on this release¶
| Record ID | Platform | Title |
|---|---|---|
| LCPD-12778 | am335x-evm | Board hangs in standby & suspend state when wl12x card is attached |
| LCPD-12373 | am572x-idk, am57xx-evm | Gstreamer kmssink regressions observed |
| LCPD-12753 | am57xx-evm | Gstreamer: OOM reported and system instability observed with video decode + waylandsink |
| LCPD-13448 | am335x-ice, am437x-idk | AM3X-ice/AM437-idk: PRUEth: link comes up but ethernet communication does not work |
| LCPD-10451 | am335x-evm, am43xx-gpevm, am571x-idk, am572x-idk, am574x-idk, am57xx-evm | Context switch delay increased based on LMBench numbers |
| LCPD-13425 | ti2018.02-rc3 build failed with CONFIG_PCI=n | |
| LCPD-13340 | omapdrm: plane set/get property broken | |
| LCPD-12437 | am57xx-evm | CMEM DTS injection code doesn’t work with DT overlays |
| LCPD-10892 | gdbc6x build failures with gcc7 | |
| LCPD-7548 | am571x-idk, am572x-idk, am57xx-evm | Media Decode is not working |
| LCPD-13465 | systemd-networkd waits on all interfaces to come online | |
| LCPD-13464 | ldconfig is missing | |
| LCPD-12546 | am57xx-evm | Enabling PVR_DEBUG_MUTEXES option results in a compile error |
| LCPD-13427 | am57xx-evm | QT Touchscreen interaction - Bear Whack crash |
| PLSDK-1947 | k2g-ice, k2g-evm, k2hk-evm, k2e-evm, k2l-evm | Matrix Launcher:CMEM Error: failed to mmap buffer at physical address 0x818000000 |
| PLSDK-2113 | am571x-idk, am572x-idk | PTP BC overshoot caused by cable unplug and plug back in |
| PLSDK-2171 | am571x-idk, am572x-idk | PRU HSR firmware: small degradation in performance seen for MTU sized frames |
| PLSDK-2174 | am335x-evm, am335x-ice, am335x-sk, beagleboneblack, am437x-idk, am437x-sk, am437x-evm, am438x-epos-evm, am571x-idk, am572x-idk, am572x-evm, am574x-idk | boot stuck on “please wait” display screen when no input device is connected |
| PLSDK-2188 | am335x-evm, am572x-evm | Failure to load ftdi_sio kernel module |
| PLSDK-2192 | am572x-evm | Using OpenVX image causing kernel crash or hang during boot up |
| PLSDK-2228 | am572x-evm | AM572x GP EVM: Unable to boot with jailhouse dtb |
| PLSDK-2257 | am572x-evm | ROS: control on Kobuki is broken |
2.1.7.2. Issued found and closed on this release that may be applicable to prior releases¶
| Record ID | Platform | Title |
|---|---|---|
| LCPD-13488 | am571x-idk, am572x-idk, am574x-idk, am574x-hsidk, am57xx-evm, am57xx-beagle-x15, am57xx-hsevm | remoteproc/omap: remoteproc shutdown crashes when using CMA HIGHMEM pools |
| LCPD-13594 | am57xx-evm | VPE: Kernel Oops observed during v4l2 IOCTL check |
| LCPD-13576 | Transparency keying is not working correctly | |
| LCPD-13570 | am335x-evm, am335x-hsevm, am335x-ice, am335x-sk, am437x-idk, am437x-sk, am43xx-epos, am43xx-gpevm, am43xx-hsevm, am571x-idk, am572x-idk, am574x-idk, am574x-hsidk, am57xx-evm, am57xx-beagle-x15, am57xx-hsevm, beaglebone, beaglebone-black, k2e-evm, k2e-hsevm, k2g-evm, k2g-hsevm, k2g-ice, k2hk-evm, k2hk-hsevm, k2l-evm, k2l-hsevm, omapl138-lcdk | Upstream: remoteproc/core: remoteproc table_ptr not reset in failures in rproc_start() |
| LCPD-13574 | 8250_omap.c doesn’t compile in ti2018.03-rc1-int | |
| LCPD-13560 | Update documentation for eMMC alternate boot support | |
| LCPD-13520 | Build warnings on ti-linux-4.14.y for arm allmodconfig (second error) | |
| LCPD-13562 | am571x-idk, am572x-idk, am574x-idk, am574x-hsidk, am57xx-evm, am57xx-beagle-x15, am57xx-hsevm | iommu/omap: L2 PTEs do not get flushed properly |
| LCPD-13579 | am571x-idk, am572x-idk, am574x-idk, am574x-hsidk, am57xx-evm, am57xx-beagle-x15, am57xx-hsevm | iommu/omap: L2 PTEs do not get flushed properly |
| LCPD-13701 | am571x-idk, am572x-idk, am574x-idk, am574x-hsidk, am57xx-evm, am57xx-beagle-x15, am57xx-hsevm | remoteproc/omap: remoteproc shutdown crashes when using CMA HIGHMEM pools |
| LCPD-13792 | am571x-idk, am572x-idk, am574x-idk, am57xx-evm, am57xx-beagle-x15, omapl138-lcdk | remoteproc: fix improper cleanup of version handling |
| LCPD-13789 | RT: Integration Build Failure | |
| LCPD-13472 | am57xx-evm | AM572: Poweroff failure |
2.1.7.3. Errata Workarounds Available in this Release¶
| Record ID | Title |
|---|---|
| LCPD-5310 | i900: CTRL_CORE_MMR_LOCK_5 region after locking results in ctrl module inaccessible, recoverable only post a reset |
| LCPD-5311 | i893: DCAN ram init issues in HW AUTO and when traffic hitting CAN bus (open investigation) |
| LCPD-5309 | LCPD: i896: USB Port disable doesnt work |
| LCPD-4195 | J6: SATA: Investigate applicability of i807 |
| LCPD-9084 | i887: Software workaround to limit mmc3 speed to 64MHz |
| LCPD-4225 | J6: Errata: i834: Investigate possibility of software workaround |
| LCPD-7642 | MMC/SD: i832: return DLL to default reset state with CLK gated if not in SDR104/HS200 mode. |
| LCPD-1188 | J6: Baseport: Errata i877: RGMII clocks must be enabled to avoid IO timing degradation due to Assymetric Aging |
| LCPD-1022 | J6: Errata: i694: System I2C hang due to miss of Bus Clear support @ OMAP level |
| LCPD-976 | J6/J6eco: 32clk is psuedo (erratum i856) - clock source |
| LCPD-975 | J6/J6eco: 32clk is psuedo (erratum i856) - realtime counter |
| LCPD-5836 | CAL: Errata: i913: CSI2 LDO needs to be disabled when module is powered on |
| LCPD-4975 | DSS AM5/DRA7: implement WA for errata i886 |
| LCPD-5460 | Implement WA for Vayu errata i829 (Reusing Pipe Connected To Writeback Pipeline On The Fly To An Active Panel) |
| LCPD-5052 | Upstream: Post the dmtimer errata fix for i874 |
| LCPD-5924 | ALL: CONNECTIVITY: CPSW: errata i877 workarround for cpsw |
| LCPD-4647 | [rpmsg 2015 LTS] Implement errata i879 - DSP MStandby requires CD_EMU in SW_WKUP |
| LCPD-4648 | [rpmsg 2014 LTS] Implement errata i879 - DSP MStandby requires CD_EMU in SW_WKUP |
| LCPD-5931 | DRA7xx: AM57xx: mmc: upstream errata workaround for i834 |
| LCPD-8294 | 37 pins + VOUT pins need slow slew enabled for timing and reliability respectively |
| LCPD-8277 | u-boot: j6: SATA is not shutdown correctly as per errata i818 |
| LCPD-9173 | i897: USB Stop Endpoint doesnt work in certain circumstances |
| LCPD-6907 | Workaround errata i880 for RGMII2 is missing |
| LCPD-4218 | Implement Workaround for Errata i813 - Spurious Thermal Alert Generation When Temperature Remains in Expected Range |
| LCPD-4217 | Implement Workaround for Errata i814 - Bandgap Temperature read Dtemp can be corrupted |
| LCPD-4184 | Implement workaround for errata i814 - Bandgap Temperature read Dtemp can be corrupted |
| LCPD-4910 | J6/OMAP5: errata i810 implementation |
| LCPD-1146 | DMM hang: Errata VAYU-BUG02976 (i878) (register part) |
| LCPD-1108 | J6: Wrong Access In 1D Burst For YUV4:2:0-NV12 Format (Errata i631) |
| LCPD-1087 | J6: MMC: Errata: i802: OMAP5430 MMCHS: DCRC errors during tuning procedure |
| LCPD-876 | OMAP5: Errata i810: DPLL Controller Sticks when left clock requests are removed |
| LCPD-1776 | [J6 SATA Adaptation] J6 - Errata i783, SATA Lockup After SATA DPLL Unlock/Relock |
2.1.7.4. SDK Known Issues¶
| Record ID | Platform | Title | Workaround |
|---|---|---|---|
| LCPD-5578 | Exception triggered by graphics driver during boot if board does not have SGX (BBB A4) | Build Processor SDK without SGX following instructions here | |
| LCPD-7025 | am43xx-gpevm | System takes more than 10 seconds to go from login prompt to system prompt | Automated tests need to account for this boot delay |
| LCPD-8345 | am335x-evm, am437x-idk, k2e-evm, k2e-hsevm, k2hk-evm, k2l-evm | Board fails to start login console after waiting 3.5 minutes ( hard to reproduce, ~4/1000) | Restart the EVM |
| LCPD-8352 | am43xx-gpevm, am57xx-evm | weston: stress testing with 75 concurrent instances of simple-egl leads to unresponsive HMI due to running out of memory |
|
| LCPD-9006 | am57xx-evm | Some GLBenchmark tests fail to run | This is a limitation with Imagination DDK, and no workaround |
| LCPD-9616 | am57xx-evm | QtCreator GDB (remote) debugging stops working since QT5.7.1 | use GDB from Processor SDK 3.2 |
| LCPD-11010 | am574x-idk | AM574x-idk graphics performance is lower than am572x-idk | Performance issue, no workaround |
| LCPD-12784 | omapl138-lcdk | Board can’t resume from suspend state sometimes | None |
| LCPD-13417 | am43xx-gpevm | Error message with multiple egl, not shared context (double unmap) | Limitation with Imagination DDK, no workaround |
| LCPD-13470 | am335x-evm | klogd and syslog are not needed when using systemd | |
| LCPD-13475 | am437x-idk, am43xx-gpevm | Back trace seen on AM437x-IDK when we reboot | |
| PLSDK-832 | AM57 | OpenCL matmpy intermittent DSP1 crash due to EdmaMgr issues w/ suspend/resume | Disabling suspend/resume on the DSPs prevents this intermittent failure: echo on > /sys/bus/platform/devices/40800000.dsp/power/control; echo on > /sys/bus/platform/devices/41000000.dsp/power/control |
| PLSDK-885 | AM57 | OpenCV Video test failure w/ GStreamer errors | Use the workaround from PLSDK-832 |
| PLSDK-1266 | am572x-idk | PRP: stale IGMP packets (IPv6) seems directly sent to eth2/eth3 of a HRP node | None |
| PLSDK-1308 | am572x-idk | PRP: PRP node is shown as SAN at times in the node table dump when not offloaded | No problem with offload, which is default |
| PLSDK-1398 | k2g-hsevm, k2hk-hsevm, k2e-evm, k2e-hsevm | Document workaround for IPC demo hangs if run after OpenCL demos | Run IPC demo w/o running OpenCL first |
| PLSDK-1419 | k2l-evm | Intermittent-IP address display issue on LCD for K2L RT | Use ifconfig once Linux boots, to acquire IP address |
| PLSDK-1556 | k2hk-evm, k2hk-hsevm, k2e-evm, k2l-evm | SA LLD: saBasicExample test shows warning as ‘Alignment trap’ on K2x platforms. | Just a warning message. No impact to test output |
| PLSDK-1693 | am572x-evm | It takes long time to use “kill pid” to close matrix-browser | Start and stop Matrix GUI using /etc/init.d/matrix start, and /etc/init.d/matrix stop, respectively |
| PLSDK-1720 | am437x-evm | Simple people tracking demo: Tracking Incorrect Number of People | None |
| PLSDK-1817 | HSR/PRP: Outstanding Net-Jury tests failures: 92/105 passed, 7 blocked and 6 failed | None | |
| PLSDK-1828 | am571x-idk, am572x-idk | HSR: In a ring topology, seeing small performance degradation with concurrent traffic | None |
| PLSDK-1909 | am572x-evm | DLP SDK demo: Assertion `ctx->pollfds_cnt >= internal_nfds’ failed | None |
| PLSDK-1924 | am335x-ice, am335x-sk, beagleboneblack | AM3: Observed unwanted failure message in boot log. | No functionality affected except the log message |
| PLSDK-1945 | am572x-evm | qApp->quit() does not work with the enhanced eglfs_kms QPA | None |
| PLSDK-1953 | am571x-idk, am572x-idk | Linux PRP: lreTransparentReception - passRCT doesn’t work as expected | None |
| PLSDK-1963 | k2e-evm | K2E:Observed unwanted failure messages in boot log | No functionality affected except the log message. If not needed, do not connect anything to the PCIe slot. |
| PLSDK-2067 | am571x-idk | Transparent Clock crashes after a couple of days due to memory leak | |
| PLSDK-2095 | am571x-idk, am572x-idk | kernel: EXPORT symbol “__hyp_stub_vectors seen during kernel build | it is just a warning message, and can be ignored |
| PLSDK-2107 | k2g-ice | sorte for K2G: master is not working | None |
| PLSDK-2109 | am437x-evm, am572x-evm | QtWebengine demobrowser shows problems at LTS2018 on EGLFS QPA | None |
| PLSDK-2128 | am335x-evm, am437x-evm, am438x-epos-evm, am572x-evm | Weston 2.0: overlay window display issue | None. For Wayland demo, you may use qwindow-compositor instead of Weston. |
| PLSDK-2178 | am335x-ice, am437x-idk | ICSS EMAC intermittent error in received acyclic packet content | None |
| PLSDK-2181 | k2g-ice | k2g-ice Eth0 IP address not displayed | |
| PLSDK-2186 | am572x-evm | video-analytic-demo should run on top of Weston instead of qwindow-compistor | Run the demo on top of qwindow-compositor, as available from Matrix GUI |
| PLSDK-2190 | am571x-idk | Matrix Launcher: Independent_Video_with_QT_widgets_to_Different_Displays failing on am571-idk-rt platform | Intermittent issue |
| PLSDK-2220 | k2e-evm | UBI Image for K2E exceeds the available size limit | None |
| PLSDK-2253 | am571x-idk | Accidental loop (no STP enabled) crashed Linux | |
| PLSDK-2289 | am571x-idk | MatrixLauncher: ivahd_enc_4K_resolution failing on am571x-idk platform | |
| PLSDK-2312 | am335x-evm, am437x-evm, am572x-evm | Some Qt3d examples either crash or works with errors | |
| PLSDK-2319 | am654x-evm | QT5 Touch Screen demo: characters are corrupted | |
| PLSDK-2323 | am571x-idk | PRUETH: hsr/prp on PRUSS1/PRUSS2 can’t co-exists with Dual EMAC | |
| PLSDK-2326 | k2e-evm | K2E-RT: Kernel warning during boot at cryptomgr_probe | |
| PLSDK-2329 | am654x-evm | Matrix-GUI Multimedia demo H264 doesn’t play full screen | |
| PLSDK-2330 | am654x-evm | Simple People Tracking Demo doesn’t restart Matrix GUI intermittently, when there is no ToF EVM connected | |
| PLSDK-2331 | am654x-evm | Matrix-GUI EVSE demo Text overflows the button, and gets truncated | |
| PLSDK-2334 | am572x-evm | video-graphics-test runs with error messages and lower performance | |
| PLSDK-2339 | am335x-evm, am335x-ice, am335x-sk, beagleboneblack, am437x-idk, am437x-sk, am437x-evm, am438x-epos-evm, am571x-idk, am572x-idk, am572x-evm, am574x-idk | Matrix GUI takes 2 min to launch when not connected to ethernet | Need to convert Matrix GUI from initd script to systemd service |
| PLSDK-2340 | HSR/PRP: With VLAN tagged SV frame, nodes using untagged SV frames appears in NT | ||
| PLSDK-2352 | am335x-evm, am437x-evm, am571x-idk, am572x-idk, am572x-evm, am574x-idk | Graphics Demo: Video_Scaling_Overlaying_Positioning test failing on am platforms | |
| PLSDK-2355 | am572x-idk, am572x-evm | Openvx: openvx_tiovx_application hangs on am572x evm |
2.1.7.5. U-Boot Known Issues¶
| Record ID | Priority | Title | Platform | Workaround |
|---|---|---|---|---|
| LCPD-13725 | P2-High | AM6 Board: Board intermittently hangs before getting to u-boot | am654x-evm, am654x-idk | |
| LCPD-13711 | P3-Medium | U-Boot: EEPROM-based board detection support not available | am654x-evm, am654x-idk | |
| LCPD-12244 | P3-Medium | AM43xx u-boot needs to support PHY_INVERT_CLKOUT=1 | am437x-idk, am437x-sk, am43xx-epos, am43xx-gpevm | |
| LCPD-12176 | P3-Medium | U-boot: Fix IOdelay error path issue | am571x-idk, am572x-idk, am574x-idk, am574x-hsidk, am57xx-evm, am57xx-beagle-x15, am57xx-hsevm | |
| LCPD-11586 | P3-Medium | dhcp failed to get IP address after reboot for K2G-ICE non-RT linux | k2g-ice | |
| LCPD-10805 | P3-Medium | U-Boot: Fix uart boot on am335x-evm | am335x-evm | |
| LCPD-10726 | P3-Medium | Update DDR3 emif regs structure for EMIF2 for the beagle_x15 board in U-Boot board file | am572x-idk, am57xx-evm | |
| LCPD-9369 | P3-Medium | AM437x GP EVM older PG version Uboot UART boot fails intermittently | ||
| LCPD-8701 | P3-Medium | Soft reboot broken | k2g-ice | |
| LCPD-5416 | P3-Medium | U-BOOT: K2G: “reset” fails for certain SD cards | K2G | |
| LCPD-13875 | P3-Medium | U-boot: SD card times out in SPL when it is not the bootmode | am654x-evm, am654x-idk | |
| LCPD-13714 | P3-Medium | OSPI boot settings for AM65x EVM must be documented in U-Boot users guide | am654x-evm | |
| LCPD-13542 | P3-Medium | U-boot: HS400 fails to enumerate on some boards | am654x-evm, am654x-idk | |
| LCPD-13535 | P3-Medium | U-boot: HS400 has really low throughput in AM654 | am654x-evm | |
| LCPD-10668 | P3-Medium | Ethernet boot: Sometimes the board could not boot uboot from Ethernet on k2g-evm | k2g-evm | |
| LCPD-9539 | P3-Medium | dhcp does not work after soft reboot | k2g-evm | |
| LCPD-7864 | P3-Medium | U-Boot: Ethernet boot fails on AM335x and AM437x | am335x-evm, am335x-ice, am335x-sk, am437x-idk, am437x-sk, am43xx-gpevm | |
| LCPD-7547 | P3-Medium | uboot nand write hangs for big size on k2g | k2g-evm | |
| LCPD-7366 | P3-Medium | uboot McSPI driver drives multiple chip selects simultaneously | am335x-evm | |
| LCPD-5517 | P3-Medium | Board fails to load bootloader sometimes when eSATA is connected | AM572x | |
| LCPD-5116 | P3-Medium | BBB: U-Boot: Board fails to acquire dhcp address sometimes | AM335x | |
| LCPD-4817 | P4-Low | am57xx-evm: uboot: usb failed to detect Kingston DataTraveler usb msc device | AM572x |
2.1.7.6. Linux Kernel Known Issues¶
| Record ID | Priority | Title | Component | Subcomponent | Platform | Workaround | Impact |
|---|---|---|---|---|---|---|---|
| LCPD-9877 | P2-High | rtc alarm does not wakeup board from poweroff state | Power & Thermal | omapl138-lcdk | |||
| LCPD-13767 | P2-High | am654x: RT mmc probe errors | Connectivity | am654x-idk | |||
| LCPD-13766 | P2-High | am654x: RT latency numbers are 60 us versus ~25 in am574x | Connectivity | am654x-idk | |||
| LCPD-13710 | P2-High | KS3M: ICSSG: 100M link doesn’t work | Connectivity | ICSSG, ICSS_EMAC | am654x-evm, am654x-idk | ||
| LCPD-13664 | P2-High | Some boards stop booting from MMC/SD | Connectivity | am654x-evm, am654x-idk | |||
| LCPD-13632 | P2-High | AM65: icssg-prueth: Port 2 doesn’t work if Port 1 is not first brought up | Connectivity | ETHERNET, icssg | am654x-evm, am654x-idk | ||
| LCPD-13527 | P2-High | A few pcie eth cards could not be enumerated on am654x-evm | Connectivity | am654x-evm | |||
| LCPD-13354 | P2-High | PRU Ethernet ping fails with packet size > 4096 bytes | Connectivity | am654x-evm, am654x-idk | |||
| LCPD-9972 | P2-High | Soft reboot failed on k2g-evm with class 10 SD cards | Connectivity | k2g-evm | |||
| LCPD-13653 | P2-High | am65x-evm could not boot from MMC/SD when MMC/SD is backup boot mode | Baseport | am654x-evm, am654x-idk | |||
| LCPD-12513 | P2-High | Android O: Board takes longer to boot compared to MM | Baseport | am57xx-evm | |||
| LCPD-13412 | P2-High | VIP camera sensor (mt9t11) is not initialized properly | Audio & Display | am57xx-evm | |||
| LCPD-12781 | P3-Medium | ipu opencl-monitor causes suspend failures | IPC, System Integration | am57xx-evm | |||
| LCPD-10987 | P3-Medium | OpenCL tests failed due to missing CMEM carveouts in dts | IPC, System Integration | OpenCL | am574x-idk, k2g-evm | ||
| LCPD-12784 | P3-Medium | Board can’t resume from suspend state sometimes | Power & Thermal | omapl138-lcdk | |||
| LCPD-9527 | P3-Medium | Potential deadlock reported by pm_suspend on am335x | Power & Thermal | am335x-evm, am335x-sk, beaglebone, beaglebone-black | |||
| LCPD-7314 | P3-Medium | Active power is slighly higher than on 2015 LTS release (Linux 4.1) | Power & Thermal | am335x-evm | |||
| LCPD-7256 | P3-Medium | Board sometimes hangs after suspend/resume cycle | Power & Thermal | am335x-evm, am335x-hsevm, am57xx-evm | |||
| LCPD-6427 | P3-Medium | vpe fails to suspend sometimes | Power & Thermal | am571x-idk, am572x-idk, am57xx-evm | |||
| LCPD-1245 | P3-Medium | AM335x: Power: Reverse current leakage on poweroff | Power & Thermal | am335x-evm | |||
| LCPD-1204 | P3-Medium | AM335x - Some voltage rails remain active during poweroff | Power & Thermal | ||||
| LCPD-965 | P3-Medium | AM335x: Power: Poweroff is not shutting down voltage domains | Power & Thermal | ||||
| LCPD-13819 | P3-Medium | Kernel warning is sometimes observed when stopping a remoteproc | IPC | am654x-evm | |||
| LCPD-13813 | P3-Medium | In 2018 LTS, CCS can’t connect to DSP if ARM is running Linux | IPC | ||||
| LCPD-13832 | P3-Medium | usb: missing CONFIG_USB_ANNOUNCE_NEW_DEVICES option | Connectivity | USB | |||
| LCPD-13827 | P3-Medium | drivers/phy/ti/phy-ti-am654.c:278 serdes_am654_clk_mux_get_parent() warn: signedness bug returning ‘(-22)’ | Connectivity | ||||
| LCPD-13818 | P3-Medium | MMC could not be built to module for am65xx | Connectivity | am654x-evm | |||
| LCPD-13800 | P3-Medium | Seeing UBIFS assert failed error in OSPI stress test | Connectivity | ||||
| LCPD-13775 | P3-Medium | pcie performance test with pcie-eth card failed | Connectivity | am654x-evm | |||
| LCPD-13739 | P3-Medium | K3M: CPSW: default P0 rx fifo mode is Fixed priority | Connectivity | CPSW2G | am654x-evm, am654x-idk | ||
| LCPD-13724 | P3-Medium | AM6 Board: Getting continuously scrolling mmc error when trying to boot | Connectivity | am654x-evm, am654x-idk | |||
| LCPD-13722 | P3-Medium | MMC PHY IO lines must be calibrated before use | Connectivity | MMCSD | am654x-evm | ||
| LCPD-13720 | P3-Medium | SPI DMA TX Mode Halts During Continuous 16/32/64 bit Transfers | Connectivity | ||||
| LCPD-13718 | P3-Medium | musb: unbind musb-hdrc driver on one usb port breaks the other port | Connectivity | USB | am335x-evm | ||
| LCPD-13717 | P3-Medium | AM57xx PG1.1ÿ: emmc: does not work. error -84 transferring data | Connectivity | eMMC | am57xx-evm, am57xx-beagle-x15 | ||
| LCPD-13716 | P3-Medium | KS3M: eMMC boot: document board switch settings in users guide | Connectivity | MMCSD | am654x-evm | ||
| LCPD-13715 | P3-Medium | KS3M: USB: SERDES: SERDES clock must be enabled before USB clock | Connectivity | USB | am654x-evm | ||
| LCPD-13709 | P3-Medium | USB camera gadget does not work on am6 | Connectivity | am654x-evm | |||
| LCPD-13679 | P3-Medium | There is no i2c command in uboot on am65x | Connectivity | am654x-evm, am654x-idk | |||
| LCPD-13667 | P3-Medium | mmc 0 timeout and env could not be saved to eMMC on one board (farm26) | Connectivity | am654x-evm | |||
| LCPD-13666 | P3-Medium | Seeing mmc0 timeout errors on some boards | Connectivity | am654x-evm | |||
| LCPD-13603 | P3-Medium | One board could not boot rootfs from one SDHC card | Connectivity | am654x-evm | |||
| LCPD-13587 | P3-Medium | dwc3: g_audio can only record once | Connectivity | USB | am57xx-evm | ||
| LCPD-13561 | P3-Medium | AM64: icssg-prueth: prueth can fail occassionally with RX tdown timeout | Connectivity | UDMA | am654x-evm, am654x-idk | ||
| LCPD-13525 | P3-Medium | Update PCIe EP user guide for am654x | Connectivity | am654x-evm, am654x-idk | |||
| LCPD-13505 | P3-Medium | AM65: USB host: some high-speed devices fail to enumerate | Connectivity | USBHOST | am654x-evm, am654x-idk | ||
| LCPD-13458 | P3-Medium | MCAN FIFO errors seen in receive CANFD tests | Connectivity | ||||
| LCPD-13452 | P3-Medium | USB Gadget Camera Capture - guvcview causes kernel oops | Connectivity | k2g-evm | |||
| LCPD-13445 | P3-Medium | Seldom kernel oops triggered by prueth_netdev_init | Connectivity | am654x-evm | |||
| LCPD-13371 | P3-Medium | mmc0 enumeration commands timeout in kernel | Connectivity | MMCSD | am654x-evm | ||
| LCPD-13356 | P3-Medium | icssg-prueth pruss2_eth: slice 0: cmd 4 failed: -5 when pru eth interface is brought up | Connectivity | am654x-evm | |||
| LCPD-13333 | P3-Medium | KS3M: Kernel: ICSS-G: Use classifiers/filters to disable promiscuous mode | Connectivity | ICSSG | am654x-evm, am654x-idk | ||
| LCPD-13330 | P3-Medium | Uboot: usb storage device could not be found at second usb reset | Connectivity | k2g-evm | |||
| LCPD-13304 | P3-Medium | am335x-evm.dts lists wrong number of PHY’s | Connectivity | am335x-evm | |||
| LCPD-12673 | P3-Medium | Board refuses to suspend on setup with SATA device | Connectivity | omapl138-lcdk | |||
| LCPD-12664 | P3-Medium | Some of SATA tests failed with Internel oops error | Connectivity | am57xx-evm | |||
| LCPD-12566 | P3-Medium | CAN user guide references canconfig which is not supported any more | Connectivity | ||||
| LCPD-12470 | P3-Medium | Analyze / fix klocwork warnings for TSCADC | Connectivity | ADC | |||
| LCPD-12469 | P3-Medium | Analyze / fix klocwork warnings for QSPI | Connectivity | QSPI | |||
| LCPD-12467 | P3-Medium | Analyze / fix klocwork warnings for SPI | Connectivity | SPI | |||
| LCPD-12466 | P3-Medium | Analyze / fix klocwork warnings for UART | Connectivity | UART | |||
| LCPD-12463 | P3-Medium | Analyze / fix klocwork warnings for PHY core | Connectivity | ||||
| LCPD-12462 | P3-Medium | Analyze / fix klocwork warnings for PCIe | Connectivity | PCIE | |||
| LCPD-12392 | P3-Medium | USBhost video: higher resolution tests fail with some cameras | Connectivity | ||||
| LCPD-12226 | P3-Medium | mmcsd first write perf decreased on some platforms | Connectivity | am43xx-gpevm, am574x-idk, am57xx-evm, omapl138-lcdk | |||
| LCPD-11564 | P3-Medium | AM57xx-evm: eth1 1G connection failure to netgear switch | Connectivity | CPSW, ETHERNET, PHYIF | am57xx-evm | ||
| LCPD-10974 | P3-Medium | am43xx-gpevm - usb camera gadget shows halting frames | Connectivity | USB | |||
| LCPD-10781 | P3-Medium | NetCP module removal results in backtrace and kernel panic | Connectivity | NETCP | k2g-evm | ||
| LCPD-10777 | P3-Medium | mtd_stresstest failed on omapl138 | Connectivity | NAND | omapl138-lcdk | ||
| LCPD-10551 | P3-Medium | K2E eth0 does down when running udp traffic, eth1 stops working | Connectivity | NETCP | k2e-evm | ||
| LCPD-10221 | P3-Medium | Longer resume times observed on setup with usb device cable | Connectivity | USB | am335x-evm | ||
| LCPD-9974 | P3-Medium | PCIe x2 width is not at expected width on am571x-idk | Connectivity | PCIe | am571x-idk | ||
| LCPD-9905 | P3-Medium | AM437x: UART: Implement workaround for Advisory 27ÿ? Spurious UART interrupts when using EDMA | Connectivity | UART | am43xx-gpevm | ||
| LCPD-9816 | P3-Medium | USBdevice omapl138 - Flood ping from server to dut usbdevice at 65500 bytes has packet loss | Connectivity | USB | omapl138-lcdk | ||
| LCPD-9815 | P3-Medium | Failed to start Login Service when using debug systest build on omapl138 | Connectivity | omapl138-lcdk | |||
| LCPD-9804 | P3-Medium | SATA performance decreased by ~34% for read and ~54% for write compared to v2.6.33 kernel | Connectivity | SATA | omapl138-lcdk | ||
| LCPD-9658 | P3-Medium | OMAP-L138 LCDK: MUSB does not enumerate mouse connected to Keyboard hub | Connectivity | USB | omapl138-lcdk | ||
| LCPD-9591 | P3-Medium | CONNECTIVITY: USB NCM gadget ping with packet sizes > 10000 fails | Connectivity | ||||
| LCPD-9469 | P3-Medium | Fix race condition when adding VLAN entries | Connectivity | NETCP | k2e-evm, k2g-evm, k2g-ice, k2hk-evm, k2l-evm | ||
| LCPD-9466 | P3-Medium | SATA PMP causes suspend failures | Connectivity | SATA | am57xx-evm | ||
| LCPD-9455 | P3-Medium | Kernel Warning reported for a USB audio device when listing with pulseaudio | Connectivity | USB | am335x-evm | ||
| LCPD-9428 | P3-Medium | Ethernet performace UDP: iperf command fails with two threads for lower buffer length | Connectivity | NETCP | k2e-evm, k2hk-evm, k2l-evm | ||
| LCPD-9372 | P3-Medium | Nand stress tests failed on am335x-evm | Connectivity | NAND | am335x-evm | ||
| LCPD-9366 | P3-Medium | PCIe USB drive sometimes could not be enumerated | Connectivity | PCIe | k2g-evm | ||
| LCPD-9011 | P3-Medium | K2G-evm: usb devices do not enumerate behind a TUSB8041 usb3.0 hub | Connectivity | USB | |||
| LCPD-8984 | P3-Medium | Kernel boot to initramfs with PA enabled results in no DHCP IP address assigned to network interfaces | Connectivity | NETCP | k2e-evm, k2l-evm | ||
| LCPD-8637 | P3-Medium | K2HK: Long-term ping test fails due to ethernet link going down | Connectivity | ||||
| LCPD-8133 | P3-Medium | USB: “cannot reset” errors observed sometimes | Connectivity | USB | am335x-evm | ||
| LCPD-8100 | P3-Medium | CONNECTIVITY: K2G ethernet performance numbers are low | Connectivity | NETCP | k2g-evm | ||
| LCPD-8078 | P3-Medium | AM3 SK: Touchscreen isn’t responsive | Audio & Display, Connectivity | am335x-sk | |||
| LCPD-8033 | P3-Medium | AM3 SK: Unexpected USB2-1 Messages on UART | Connectivity | USB | |||
| LCPD-7955 | P3-Medium | Uncorrectable Bitflip errors seen after switch to SystemD | Connectivity | GPMC | am335x-evm, am43xx-gpevm, k2e-evm, k2g-evm, k2g-ice, k2hk-evm, k2hk-hsevm, k2l-evm | Workaround to erase the NAND flash completely if flashed with an incompatible flash writer. SystemD tries to mount all partitions and that is the reason this is being seen now. | |
| LCPD-7829 | P3-Medium | uboot: UHS card did not work on the expected speed in uboot | Connectivity | am57xx-evm | |||
| LCPD-7744 | P3-Medium | UHS SDR104 card works on different speed after soft reboot | Connectivity | am57xx-evm | |||
| LCPD-7623 | P3-Medium | Seeing SPI transfer failed error sometimes on k2hk when using rt kernel | Connectivity | SPI | k2hk-evm | ||
| LCPD-7559 | P3-Medium | K2E/K2HK does not enumerate usb3 devices through usb3.0 hub | Connectivity | USB | k2e-evm, k2hk-evm | ||
| LCPD-7265 | P3-Medium | Uboot eMMC does not use HS200 on am57xx-gpevm | Connectivity | am57xx-evm | |||
| LCPD-6334 | P3-Medium | k2g-evm: NAND is untestable due to data corruption issues | Connectivity | k2g-evm | |||
| LCPD-6300 | P3-Medium | am57xx-evm: A few UHS cards could not be numerated in kernel and mmc as rootfs failed. | Connectivity | am57xx-evm | |||
| LCPD-6144 | P3-Medium | am572x-idk: eMMC failed to enumerate | Connectivity | MMCSD | am572x-idk | ||
| LCPD-5699 | P3-Medium | pci: am572x-idk: pci broadcom card doesn’t enumerate | Connectivity | AM571x, AM572x | |||
| LCPD-5677 | P3-Medium | K2E-evm: Marvel SATA controller could not be detected sometimes when Power On Reset is involved | Connectivity | K2E | |||
| LCPD-5522 | P3-Medium | pcie-usb sometimes the usb drive/stick could not be enumerated | Connectivity | am571x-idk, am572x-idk, am57xx-evm, am57xx-hsevm | |||
| LCPD-5362 | P3-Medium | MUSB: Isoch IN only utilises 50% bandwidth | Connectivity | USB | AM335x | ||
| LCPD-5308 | P3-Medium | i897: USB Stop Endpoint doesnt work in certain circumstances | Connectivity | USB | AM437x, AM571x, AM572x, K2E, K2G, K2HK, K2L | ||
| LCPD-4849 | P3-Medium | K2hk: Connectivity: UART data corruption observed sometimes in loopback mode | Connectivity | ||||
| LCPD-4503 | P3-Medium | ALL: 8250 UART driver not enabeld as wake source by default | Connectivity | UART | |||
| LCPD-1239 | P3-Medium | J6: Connectivity: J6 could not resume when PCI-SATA card is in | Connectivity | PCIe | am572x-idk, am57xx-evm | ||
| LCPD-1198 | P3-Medium | am43xx-gpevm:Connectivity: when kmemleak debug is enabled and mmc stress test is run, OOM killer is seen to kick in. Does not happen without kernel debug. | Connectivity | ||||
| LCPD-1144 | P3-Medium | Logitech USB-PS/2 Optical Mouse cannot be detected every other time the system is suspended/resumed (AM335x-EVM) | Connectivity | ||||
| LCPD-1106 | P3-Medium | Connectivity:PCIe-SATA ext2 1G write performance is poor due to ata failed command | Connectivity | PCIe | am57xx-evm | ||
| LCPD-932 | P3-Medium | AM33X: CONNECTIVITY: MUSB MSC read numbers are lower in 3.14 compared to 3.12 | Connectivity | USB | |||
| LCPD-869 | P3-Medium | AM335x: Connectivity: USB data transfer fails if board is suspended/resumed | Connectivity | ||||
| LCPD-816 | P3-Medium | J6/J6eco:Connectivity:PCIe-PCI eth bridge doesn’t work on J6/J6eco | Connectivity | PCIe | |||
| LCPD-662 | P3-Medium | CONNECTIVITY: AM335X: distortion in USB audio when msc connect/disconnect happens in parallel | Connectivity | ||||
| LCPD-13726 | P3-Medium | Error: “NOHZ: local_softirq_pending” | Baseport | am335x-evm, am335x-hsevm, am335x-ice, am335x-sk, am437x-idk, am437x-sk, am43xx-epos, am43xx-gpevm, am43xx-hsevm, am571x-idk, am572x-idk, am574x-idk, am574x-hsidk, am57xx-evm, am57xx-beagle-x15, am57xx-hsevm, beaglebone, beaglebone-black | |||
| LCPD-13604 | P3-Medium | AM65x OLDI clock rate is badly off | Baseport | am654x-evm | |||
| LCPD-13410 | P3-Medium | Reboot command is not operational | Baseport | am654x-evm, am654x-idk | |||
| LCPD-11546 | P3-Medium | Rare kernel crash triggered by task_blocks_on_rt_mutex | Baseport | am574x-idk, k2e-evm | |||
| LCPD-10533 | P3-Medium | Cryptos: SHA1_Hash demo test fails on AM3/4/5 platforms | Baseport | am335x-evm, am335x-ice, am43xx-epos, am43xx-gpevm, am571x-idk, am572x-idk, am574x-idk, am57xx-evm | |||
| LCPD-9981 | P3-Medium | Some LTP’s memory management tests fail due to low amount of free memory | Baseport | omapl138-lcdk | |||
| LCPD-9980 | P3-Medium | LTP’s math tests float_exp_log and float_trigo fail due to OOM | Baseport | omapl138-lcdk | |||
| LCPD-9756 | P3-Medium | pm_runtime does not kicks in for some IPs (serial, gpio and wdt) | Baseport | omapl138-lcdk | |||
| LCPD-8640 | P3-Medium | Crypto performance for AES drops 3-10% in 2016.05 | Baseport | ||||
| LCPD-8550 | P3-Medium | CPSW memory allocation errors seen during boot | Audio & Display, Baseport | am335x-sk | |||
| LCPD-8406 | P3-Medium | K2G: PADCONFIG_202 register cannot be re-programmed | Baseport | k2g-evm, k2g-ice | This has proven to be a silicon issue related to locking RSTMUX. It is currently being discussed if it will be fixed in a newer silicon revision. Currently to avoid this issue the affected pins pinmux are not changed in the kernel. This is because U-boot locks RSTMUX which causes problems if the kernel tries to change the pinmuxing for the pins. | ||
| LCPD-8350 | P3-Medium | UART boot does not work on am57xx-evm | Baseport | am57xx-evm | |||
| LCPD-8347 | P3-Medium | BUG: sleeping function called from invalid context triggered by keystone_pcie_fault | Baseport | k2e-evm, k2g-evm | |||
| LCPD-8336 | P3-Medium | Soft reboot does not work on am43xx-hsevm rev1.5b | Baseport | am43xx-hsevm | |||
| LCPD-8257 | P3-Medium | Boot failed 1 of 1000 times on k2g | Baseport | k2g-evm | |||
| LCPD-7486 | P3-Medium | uboot debug with ccs is failing for K2 | Baseport | k2hk-evm | |||
| LCPD-6998 | P3-Medium | K2G sometimes boot failed with kernel oops error | Baseport | k2g-evm | |||
| LCPD-6663 | P3-Medium | [RT] Kmemleak is buggy and boot is crashed randomly | Baseport | ||||
| LCPD-13687 | P3-Medium | QtWebengine demobrowser crashes during window resize operations at LTS2018 | Audio & Display | am335x-evm, am43xx-gpevm, am57xx-evm, am654x-evm | None | ||
| LCPD-12680 | P3-Medium | Seeing i2c timeout error and board failed to boot | Audio & Display | k2g-evm | |||
| LCPD-12511 | P3-Medium | Audio record is not working | Audio & Display | Audio | am57xx-evm | ||
| LCPD-11138 | P3-Medium | VIP driver multi-channel capture issue with TVP5158 | Audio & Display | Capture, VIP | am571x-idk, am572x-idk, am574x-idk, am574x-hsidk, am57xx-evm, am57xx-beagle-x15, am57xx-hsevm | ||
| LCPD-10954 | P3-Medium | DSS sync-losts and underflows seen with bad config | Audio & Display | Display | am437x-sk | ||
| LCPD-7735 | P3-Medium | Powerdomain (vpe_pwrdm) didn’t enter target state 0 | Audio & Display, Power & Thermal | am57xx-evm | |||
| LCPD-7696 | P3-Medium | VPE: File2File checksum changes across multiple runs | Audio & Display | am571x-idk, am572x-idk, am57xx-evm, am57xx-hsevm | There is no workaround for this issue yet | No visual artifacts, but checksum on initial frame differs as couple of bytes are incorrect | |
| LCPD-7693 | P3-Medium | VIP: OV1063x: Video artifacts in LVDS cameras | Audio & Display | Capture | |||
| LCPD-6377 | P3-Medium | OMAP_BO_CACHED feature not functional | Audio & Display, Multimedia | Display | am437x-idk, am437x-sk, am43xx-gpevm, am43xx-hsevm, am571x-idk, am572x-idk, am57xx-evm | ||
| LCPD-5380 | P3-Medium | omapdss error: HDMI I2C Master Error | Audio & Display | AM572x | Occurs only with this monitor -ÿhttps://www.amazon.com/gp/product/B00PFLZV2G | ||
| LCPD-1191 | P4-Low | AM335x: Power: System resumes due to wakeup source USB1_PHY without any external trigger | Power & Thermal | Use GPIO interrupt instead of USB PHY for wakeup source. | |||
| LCPD-1013 | P4-Low | AM335x: Power: Seldom short-duration power increase (~38mw) in VDDSHV4 domain | Power & Thermal | ||||
| LCPD-10455 | P4-Low | remoteproc/keystone: Hang observed while running RPMSG_PROTO example app | IPC | DSP_remoteproc | k2g-evm, k2g-ice, k2hk-evm, k2l-evm | ||
| LCPD-9801 | P4-Low | remoteproc/davinci: DSP boot is broken after a suspend/resume cycle | IPC | DSP_remoteproc | omapl138-lcdk | ||
| LCPD-9481 | P4-Low | Sometime the system hangs while loading the rpmsg rpc modules | IPC | RPMSG-RPC | am571x-idk, am572x-idk, am57xx-evm, am57xx-hsevm | ||
| LCPD-7495 | P4-Low | Sometimes a Kernel Warning + Oops is seen when removing keystone_remoteproc module | IPC | k2hk-evm | |||
| LCPD-4855 | P4-Low | [rpmsg 2015 LTS] J6Eco: IPC: Board hangs when an MMU fault occurs in the first message | IPC | am572x-idk | |||
| LCPD-4699 | P4-Low | rpmsg-rpc: kernel crash during error recovery with dynamic debug traces enabled | IPC | am571x-idk, am572x-idk, am57xx-evm | |||
| LCPD-13794 | P4-Low | Usb stick could not be detected at the second time on k2g-evm | Connectivity | k2g-evm | |||
| LCPD-12783 | P4-Low | Missing instruction for pcie-ep config on k2g-evm for 4.14 kernel | Connectivity | k2g-evm | |||
| LCPD-11570 | P4-Low | Base ubi filesystem could not be mounted as ubifs on k2g-evm | Connectivity | k2g-evm | |||
| LCPD-9589 | P4-Low | I2C: Sometimes i2c read write failed on farm01 and farm02 | Connectivity | am335x-evm | |||
| LCPD-9222 | P4-Low | PRUSS Ethernet does not work on AM572x ES1.1 | Connectivity | PRUSS-Ethernet | am572x-idk | ||
| LCPD-8636 | P4-Low | Serial corruption being seen in kernel | Connectivity | UART | am335x-evm | ||
| LCPD-8477 | P4-Low | K2: serdes nodes doesn’t have a functional clock | Connectivity | SERDES | k2e-evm, k2e-hsevm, k2g-evm, k2g-ice, k2hk-evm, k2hk-hsevm, k2l-evm, k2l-hsevm | ||
| LCPD-8270 | P4-Low | K2: SerDes driver need to enable PD of the peripheral before access the SerDes h/w | Connectivity | SERDES | k2g-evm | ||
| LCPD-7998 | P4-Low | Realtime OSADL Test results degraded slightly for am572x-idk | Connectivity | am572x-idk | |||
| LCPD-7903 | P4-Low | Uboot phy startup failed and dhcp failed occasionally on k2 board | Connectivity | k2g-evm, k2hk-evm | |||
| LCPD-7480 | P4-Low | K2L/E EVMs doesn’t boot to Linux when both 1G Ethernet interfaces are connected | Connectivity | k2e-evm, k2l-evm | |||
| LCPD-7188 | P4-Low | PCIe-SATA test failed | Connectivity | am57xx-evm | TI custom board would help with signal integrity issues being seen with the EVM. | ||
| LCPD-1207 | P4-Low | AM43XX/AM57XX: CONNECTIVITY: dwc3_omap on am43xx and xhci_plat_hcd on am5 - removal results in segmentation fault | Connectivity | USB | |||
| LCPD-998 | P4-Low | MUSB does not free urbs causing usb audio playback to fail | Connectivity | AM335x | |||
| LCPD-727 | P4-Low | J6:Connectivity:SATA readwrite tests sometimes fail and dut hangs with cpuidle enabled | Connectivity | ||||
| LCPD-671 | P4-Low | AM33XX: CONNECTIVITY: MUSB in PIO mode - video issues | Connectivity | ||||
| LCPD-525 | P4-Low | AM438x: Connectivity: I2C operates 9% beyond desired frequency | Connectivity | ||||
| LCPD-10223 | P4-Low | Keystone-2 Linking RAM region 0 size register REGION0_SIZE programming | Baseport | k2hk-evm | |||
| LCPD-6075 | P4-Low | BUG: using smp_processor_id() in preemptible [00000000] code during remoteproc suspend/resume | Baseport, IPC | am572x-idk, am57xx-evm | |||
| LCPD-9098 | P4-Low | Writeback: error prints seen when doing wb capture | Audio & Display | Capture, Display, Writeback | am571x-idk, am572x-idk, am57xx-evm | ||
| LCPD-8884 | P4-Low | VIP does not work after incorrectly configuring captured YUYV frame as NV12 | Audio & Display | Capture, VIP | |||
| LCPD-5059 | P4-Low | omapdrm: moving plane from one enabled display to another causes errors | Audio & Display | Display | |||
| LCPD-4681 | P4-Low | omapdrm: an error when enabling a display is not handled correctly | Audio & Display | Display | |||
| LCPD-1171 | P4-Low | DMM errata i878 (framebuffer part) | Audio & Display | Display, TILER | am571x-idk, am572x-idk, am57xx-evm |
2.1.7.7. RT Linux Kernel Known Issues¶
| Record ID | Priority | Title | Component | Platform | Workaround |
|---|---|---|---|---|---|
| LCPD-6663 | P3-Medium | [RT] Kmemleak is buggy and boot is crashed randomly | Baseport | ||
| LCPD-7623 | P3-Medium | Seeing SPI transfer failed error sometimes on k2hk when using rt kernel | Connectivity | k2hk-evm | |
| LCPD-11546 | P3-Medium | Rare kernel crash triggered by task_blocks_on_rt_mutex | Baseport | am574x-idk, k2e-evm | |
| LCPD-11568 | P3-Medium | dhcp failed to get IP address after reboot for K2G-ICE non-RT linux | Baseport | k2g-ice | |
| LCPD-13766 | P2-High | am654x: RT latency numbers are 60 us versus ~25 in am574x | Connectivity | am654x-idk | |
| LCPD-13767 | P2-High | am654x: RT mmc probe errors | Connectivity | am654x-idk |
Installation and Usage
The Software Developer’s Guide provides instructions on how to setup up your Linux development environment, install the SDK and start your development. It also includes User’s Guides for various Example Applications and Code Composer Studio.
Host Support
The Processor SDK is developed, built and verified on Ubuntu 14.04, 16.04 and 18.04. Details on how to create a virtual machine to load Ubuntu 14.04 are described in this page.
Note
Processor SDK Installer is 64-bit, and installs only on 64-bit host machine. Support for 32-bit host is dropped as Linaro toolchain is available only for 64-bit machines