VXLIB_channelCombine_2to1_i8u_o8u


Detailed Description


Functions

VXLIB_STATUS VXLIB_channelCombine_2to1_i8u_o8u (const uint8_t src0[restrict], const VXLIB_bufParams2D_t *src0_addr, const uint8_t src1[restrict], const VXLIB_bufParams2D_t *src1_addr, uint8_t dst[restrict], const VXLIB_bufParams2D_t *dst_addr)
VXLIB_STATUS VXLIB_channelCombine_2to1_i8u_o8u_checkParams (const uint8_t src0[], const VXLIB_bufParams2D_t *src0_addr, const uint8_t src1[], const VXLIB_bufParams2D_t *src1_addr, const uint8_t dst[], const VXLIB_bufParams2D_t *dst_addr)


Function Documentation

VXLIB_STATUS VXLIB_channelCombine_2to1_i8u_o8u ( const uint8_t  src0[restrict],
const VXLIB_bufParams2D_t src0_addr,
const uint8_t  src1[restrict],
const VXLIB_bufParams2D_t src1_addr,
uint8_t  dst[restrict],
const VXLIB_bufParams2D_t dst_addr 
)

Description:
Implements the Channel Combine Kernel.
Method:
The 2 to 1 Channel Combine is implemented using the following equation:

    dst(x + 0) = src0(x)
    dst(x + 1) = src1(x)

   

Parameters:
[in] src0[] Pointer to array containing first input image (UQ8.0)
[in] src0_addr[] Pointer to structure containing dimensional information of src0
[in] src1[] Pointer to array containing second input image (UQ8.0)
[in] src1_addr[] Pointer to structure containing dimensional information of src1
[out] dst[] Pointer to array containing output image (UQ8.0)
[in] dst_addr[] Pointer to structure containing dimensional information of dst
Assumptions:
  • I/O buffer pointers are assumed to be not aliased.
Performance Considerations:
  • For best performance, the following parameter settings are recommended:
    • Set output stride equal to input stride * 2
    • Align all pointers to 8 byte boundaries
    • Set all stride values to a multiple of 8
    • Set all width values to a multiple of 8

VXLIB_STATUS VXLIB_channelCombine_2to1_i8u_o8u_checkParams ( const uint8_t  src0[],
const VXLIB_bufParams2D_t src0_addr,
const uint8_t  src1[],
const VXLIB_bufParams2D_t src1_addr,
const uint8_t  dst[],
const VXLIB_bufParams2D_t dst_addr 
)

Description:
Checks the parameters for programming errors for the VXLIB_channelCombine_2to1_i8u_o8u function.
Method:
The following checks are made:
  • There shall be no NULL pointers
  • The dst image can be VXLIB_UINT8 or VXLIB_UINT16
    • If VXLIB_UINT8:
      • The dim_x of the dst image shall be 2 * dim_x of src images
    • If VXLIB_UINT16:
      • The dim_x of the dst image shall be equal to the dim_x of src images
  • The stride_y of the dst image shall be equal to or greater than src image dim_x * 2
  • Both src images shall have the same x and y dimensions
  • The stride_y of the src images shall be equal to or greater than dim_x
Parameters:
[in] src0[] Pointer to array containing first input image (UQ8.0)
[in] src0_addr[] Pointer to structure containing dimensional information of src0
[in] src1[] Pointer to array containing second input image (UQ8.0)
[in] src1_addr[] Pointer to structure containing dimensional information of src1
[out] dst[] Pointer to array containing output image (UQ8.0)
[in] dst_addr[] Pointer to structure containing dimensional information of dst


Copyright 2020, Texas Instruments Incorporated